world leader in high performance signal processing
This version (12 Apr 2013 16:02) was approved by LucianS.The Previously approved version (29 Mar 2013 10:58) is available.Diff

ADXRS453 Pmod Xilinx FPGA Reference Design

Introduction

The ADXRS453 is an angular rate sensor (gyroscope) intended for industrial, instrumentation, and stabilization applications in high vibration environments. An advanced, differential, quad sensor design rejects the influence of linear acceleration, enabling the ADXRS453 to offer high accuracy rate sensing in harsh envi-ronments where shock and vibration are present. This reference design allows full programming of the device, and also includes monitoring rotation angles on Z-Axis and printing them on the UART.

Two reference designs are available for this part:

  • A design which demonstrates how to acquire data and display it using Digilent PmodGYRO2 and PmodACL. Data acquired from PmodGYRO2 is displayed in Degrees per Second, and data acquired from PmodACL is displayed in g. Data is formatted in 4 columns.

ADXRS453 Pmod Reference Design

Quick Start Guide

The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT).

Required Hardware

Required Software

  • Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack).
  • A UART terminal (Tera Term/Hyperterminal), Baud rate 115200 for the Avnet LX-9 Microboard or 9600 for the Digilent Nexys™3 Board.

Running Demo (SDK) Program

If you are not familiar with LX9 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm for details.
If you are not familiar with Nexys™3 and/or Xilix tools, please visit
http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3 for details.

Extract the project from the archive file (ADXRS453_<board_name>.zip) to the location you desire.

Avnet LX9 MicroBoard Setup

To begin, connect the PmodGYRO2 to J5 connector of LX9 board, pins 7 to 12 (see image below). You can use an extension cable for ease of use. Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector.

PmodGYRO2 and LX-9

Digilent Nexys™3 Spartan-6 FPGA Board

To begin, connect the PmodGYRO2 to JA connector of Nexys™3 board, pins JA1 to JA6 (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART).

PmodGYRO2 and Nexys™3

FPGA Configuration

Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Start a UART terminal (set to appropiate baud rate) and then program the device using the bit file provided in the project *.zip archive, located in the “sw” folder (../adxrs453/sw/ADXRS453.bit).

Programming FPGA in IMPACT

If programming was successful, you should be seeing messages appear on the terminal window as shown in the figure below. After programming the ADXRS453 device, the program will automatically send the recommended initialization sequence. Once complete, it will start to print current angles/second rotation on Z-Axis on the UART.

UART messeges

Information displayed in the Terminal Screen is in Degrees/Second, representing the rotation described by the Pmod around the marked Axis in the past second. If you rotate the Pmod slowly, you will see a smaller value (e.g. 30 Degrees/Second), while rotating the Pmod at a higher speed will result in a higher value (e.g. 300 Degrees/Second). Afterwards the device will auto calibrate according to its new position, thus displaying a value close to 0 Degrees/Second.

Using the reference design

Functional Description

The reference design is a simple SPI interface for the ADXRS453. The software programs the device and monitors vibrations or rotations. The information is displayed on UART.

The hardware SPI access allows reading or writing of any ADXRS453 registers via the address, write and read data registers.


Connecting the PmodGYRO2 to the boards using an extension cable provides ease of use.
UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard or 9600 Baud Rate for the Digilent Nexys™3 Board.

Downloads

ADXRS453 Pmod and ADXL345 Pmod Reference Design

Quick Start Guide

The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system.

Required Hardware

Required Software

  • Xilinx 13.2 Design Suite (contains ISE, XPS, SDK and ChipScope Pro).
  • A UART terminal (Tera Term/Hyperterminal), Baud rate 57600.

Running Demo (SDK) Program


If you are not familiar with LX9 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm for details.

To begin, connect the PmodGYRO2 to J5 connector of LX9 board, pins 7 to 12. You must use an extension cable or the Pmod-TPH (Digilent). Afterwards connect PmodACL to connector J4 of the LX9 Board (see image below).

Connecting Pmods to LX-9 MicroBoard

Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Program the FPGA using the download.bit file provided in the project *.zip archive, located in the ”sw” folder (../adxrs453_adxl345/sw/download.bit).

Programming FPGA in IMPACT

Start a Hyperterminal program (Tera Term, puTTy, etc.), select the proper COM Port (look for the COM Port named Silicon Labs CP210x USB to UART Bridge in Windows Device Manager). Select 57600 Baud Rate and Odd Parity. You should start seeing messeges in the Terminal Window, displayed on 4 columns, representing the rotation of the board in Degrees per Second, and the acceleration in g on each axis.

Messeges displayed in the terminal window

On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.

  • Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH.
  • Connecting the PmodACL to the board with an extension cable provides ease of use.
  • UART must be set to 57600 baudrate.

Downloads

11 Apr 2012 10:45 · Alexandru Tofan

More information