This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:pmod:adxl345 [30 Oct 2013 09:56] – [Preparing the SD Card] Alexandru.Tofan | resources:fpga:xilinx:pmod:adxl345 [03 Sep 2014 18:48] – [Preparing the SD Card] Lars-Peter Clausen | ||
---|---|---|---|
Line 162: | Line 162: | ||
* Configure the kernel to include the driver for the ADXL345: [[http:// | * Configure the kernel to include the driver for the ADXL345: [[http:// | ||
* Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step and the kernel configuration above | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step and the kernel configuration above | ||
- | * [[http:// | + | * [[http:// |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. |