world leader in high performance signal processing
This version (12 Apr 2013 16:03) was approved by LucianS.The Previously approved version (29 Mar 2013 10:41) is available.Diff

ADP5589 Pmod Xilinx FPGA Reference Design

Introduction

The ADP5589 is a 19 I/O port expander with built-in keypad matrix decoder, programmable logic, reset generator and PWM generator. This reference design allows full programming of the device, and also includes Keypad Decoder Test Mode and Key Lock/Unlock Feature.

HW Platform(s):

System: Microblaze, AXI, UART

Quick Start Guide

The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT).

Required Hardware

Required Software

  • Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack).
  • A UART terminal (Tera Term/Hyperterminal), Baud rate 115200 for the Avnet LX-9 Microboard or 9600 for the Digilent Nexys™3 Board.

Running Demo (SDK) Program

If you are not familiar with LX9 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm for details.
If you are not familiar with Nexys™3 and/or Xilix tools, please visit
http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3 for details.

Extract the project from the archive file (ADP5589_<board_name>.zip) to the location you desire.

Avnet LX9 MicroBoard Setup

To begin, connect the PmodKYPD to J1 connector of PmodIOXP. After that, connect the PmodIOXP board to J4 connector of LX9 board, pins 3 to 6 (see image below). You must use the extension cable provided, otherwise the I2C Interface will not work. . Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector.

Connect PmodKYPD to PmodIOXP Connect PmodIOXP to LX-9

Digilent Nexys™3 Spartan-6 FPGA Board

To begin, connect the PmodKYPD to J1 connector of PmodIOXP. After that, connect the PmodIOXP board to JA connector of Nexys™3 board, pins JA3 to JA6 (see image below). You must use the extension cable provided, otherwise the I2C Interface will not work. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART).

Connect PmodKYPD to PmodIOXP Connect PmodIOXP to Nexys™3

FPGA Configuration

Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Start a UART terminal (set appropiate baud rate) and then program the device using the bit file provided in the project *.zip archive, located in the “sw” folder (../adp5589/sw/ADP5589.bit).

If programming was successful, you should be seeing messages appear on the terminal window as shown in figures below. After programming the ADP5589 device, the program will display initialization messages, and afterwards it will enter Key Decoder Test Mode. In this mode, you can press any key on the PmodKYPD, and it will be displayed on the UART along with the corresponding event (press/release). Pressing the [F] key will exit Key Decoder Test Mode. Next the program will Lock the keypad. Unlocking it requires the combination [1] [A].

Initialization Key Decode Test Key Lock/Unlock

Using the reference design

Functional Description

The reference design is a simple I2C interface for the ADP5589. The software programs the device, monitors and reports events, locks or unlocks the keypad. It can also be programmed to generate a PWM signal or implement simple digital logic. The information is displayed on a UART terminal.

The hardware I2C access allows reading or writing of any ADP5589 registers via the address, write and read data registers.

PmodIOXP must be connected to J4 using the extension cable provided.
When decoding the PmodKYPD pay attention to the fact that:

  • ROW1 to ROW4 are seen by the ADP5589 as C3 to C0.
  • COL4 to COL1 are seen by the ADP5589 as R3 to R0.

UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard or 9600 Baud Rate for the Digilent Nexys™3 Board.

Downloads

More information