This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:pmod:ad7780 [01 Oct 2013 08:57] – [FPGA Configuration for ZedBoard] Alexandru.Tofan | resources:fpga:xilinx:pmod:ad7780 [20 Nov 2013 14:57] – added custom hdl linux (in progress) Alexandru.Tofan | ||
---|---|---|---|
Line 141: | Line 141: | ||
* [[https:// | * [[https:// | ||
* [[https:// | * [[https:// | ||
- | * [[https:// | + | * [[https:// |
* [[https:// | * [[https:// | ||
* [[https:// | * [[https:// | ||
| | ||
</ | </ | ||
+ | |||
+ | ====== Linux Device Driver - Custom HDL PCore ====== | ||
+ | |||
+ | Connect PmodAD3 to the JD1 connector of the ZedBoard (upper row of pins). | ||
+ | |||
+ | ===== Preparing the SD Card ===== | ||
+ | |||
+ | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
+ | * Download the device tree: [[https:// | ||
+ | * Download the Xilinx XPS project: [[https:// | ||
+ | * Download the AD7780 IPcore: [[https:// | ||
+ | * Download the project libraries: [[https:// | ||
+ | * Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step | ||
+ | * [[http:// | ||
+ | |||
+ | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
+ | If everything is correct, the system should boot up. If you don't have an HDMI monitor, connect to the board via UART, Baud Rate 115200. | ||
+ | |||
+ | There are 2 ways to test the driver. | ||
+ | * Using the terminal window | ||
+ | * Using the ADI IIO Oscilloscope | ||
+ | |||
+ | ===== Using the terminal window ===== | ||
+ | |||
+ | Open a new terminal window by pressing **Ctrl+Alt+T**. | ||
+ | |||
+ | Navigate to the location of the device and identify it using the following commands: | ||
+ | < | ||
+ | cd / | ||
+ | ls | ||
+ | iio:device0 iio:device1 trigger0 | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | AD7780 | ||
+ | </ | ||
+ | |||
+ | If the **cat name** command doesn' | ||
+ | < | ||
+ | cd .. | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | </ | ||
+ | |||
+ | To see the list of options that the AD7780 driver provides, type: | ||
+ | < | ||
+ | ls | ||
+ | buffer | ||
+ | </ | ||
+ | |||
+ | To read the raw input voltage, type: | ||
+ | < | ||
+ | cd buffer | ||
+ | echo 40 > length | ||
+ | echo 1 > enable | ||
+ | hexdump -x / | ||
+ | 0000000 | ||
+ | 0000010 | ||
+ | </ | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== Using the ADI IIO Oscilloscope ===== | ||
+ | |||
+ | Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | ||
+ | * [[http:// | ||
+ | |||
+ | Launch the ADI IIO Oscilloscope. | ||
+ | |||
+ | Select **AD7780** from the **Device** drop-down menu. Set the desired number of samples in the **Sample Count** tab. Click the **Green Play Button** in order to start capturing and displaying data. Click **Stop** to stop the process. | ||
+ | |||
+ | {{: | ||
+ | |||
===== More information ===== | ===== More information ===== | ||
* [[ez> | * [[ez> | ||
* Example questions: {{rss> | * Example questions: {{rss> |