This is an old revision of the document!
The AD7156 delivers a complete signal processing solution for capacitive sensors, featuring an ultralow power converter with fast response time. The AD7156 uses an Analog Devices, Inc., capacitance-to-digital converter (CDC) technology, which combines features important for interfacing to real sensors, such as high input sensitivity and high tolerance of both input parasitic ground capacitance and leakage current. The integrated adaptive threshold algorithm compensates for any variations in the sensor capacitance due to environmental factors like humidity and temperature or due to changes in the dielectric material over time.
HW Platform(s):
The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT).
If you are not familiar with LX9 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards-and-kits/AES-S6MB-LX9.htm for details.
If you are not familiar with Nexys™3 and/or Xilix tools, please visit
http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,897&Prod=NEXYS3 for details.
If you are not familiar with ZedBoard and/or Xilix tools, please visit
http://www.em.avnet.com/en-us/design/drc/Pages/Zedboard.aspx for details.
Extract the project from the archive file (AD7156_<board_name>.zip) to the location you desire.
To begin, connect the PmodCDC1 to J5 connector of LX9 board (see image below). You can use an extension cable for ease of use. Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector.
Extract the project from the archive file (AD7156_<board_name>.zip) to the location you desire.
To begin, connect the PmodCDC1 to JA connector of NEXYS3 board (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART).
To begin, connect the PmodCDC1 to JC1 and JA1 connector of ZedBoard (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART).
Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Spartan 6 device (see screenshot below). Start a UART terminal (set to appropiate baud rate) and then program the device using the bit file provided in the project *.zip archive, located in the “sw” folder (../ad7156/sw/AD7156.bit).
Run the download.bat script from the “../bin” folder downloaded from the github (see the links in the download section of the wiki page). The script will automatically configure the ZYNQ SoC and download the *.elf file afterwards.
If the download script fails to run, modify the Xilinx Tools path in download.bat to match your Xilinx Installation path.
If programming was successful, the Main Menu will apear in your UART terminal, as seen in the picture below. There are 7 options. Pressing [d], [c], [a], [t], [r], [m], [s] or [q] key will allow you to select the desired option.
Select Channels for display allows selecting which channel(s) to display and measure.
Display Capacitance prints the selected Channel(s) measured capacitance.
Display Average Capacitance prints the selected Channel(s) measured average capacitance.
Set Threshold allows setting the threshold for each channel (feature available only in fixed threshold mode).
Set Sensitivity allows setting timeout for each channel.
Set Timeout prints Threshold mode and values for each channel.
Set Input Range allows setting the input range for each channel.
Threshold menu allows selecting between Fixed Threshold and Adaptive Threshold.
Display current settings prints Threshold mode, type and also the values for each channel.
Stop and return to menu will stop any ongoing action and will display the menu with all the available options.
The reference design is a SPI interface used to communicate with the device. The software programs the AD7156s internal registers, and afterwards reads desired data from the device and prints it via UART. Interrupts are used to turn on LEDs and start a timer (LEDs stay ON for 1 second).
When using the ZedBoard reference design in order to develop your own software, please make sure that the following options are set in “system_config.h”:
// Select between PS7 or AXI Interface #define USE_PS7 1 // SPI used in the design #define USE_SPI 0 // I2C used in the design #define USE_I2C 1 // Timer (+interrupts) used in the design #define USE_TIMER 1 // External interrupts used in the design #define USE_EXTERNAL 1 // GPIO used in the design #define USE_GPIO 1
Avnet LX-9 MicroBoard:
Digilent Nexys™3:
Avnet ZedBoard:
Connect PmodCDC1 to the JC1 connector of the ZedBoard (upper row of pins).
In order to prepare the SD Card for booting Linux on the ZedBoard:
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. If everything is correct, the system should boot up. If you don't have an HDMI monitor, connect to the board via UART, Baud Rate 115200.
There are 2 ways to test the driver.
Open a new terminal window by pressing Ctrl+Alt+T.
Navigate to the location of the device and identify it using the following commands:
cd /sys/bus/iio/devices/ ls iio:device0 iio:device1 cd iio\:device0 cat name ad7156
If the cat name command doesn't return ad7156, then change the number of the iio:device, and check again.
cd .. cd iio\:device1 cat name
To see the list of options that the AD7156 driver provides, type:
ls dev in_capacitance0_mean_raw in_capacitance1_mean_raw name subsystem events in_capacitance0_raw in_capacitance1_raw power uevent
To read the raw capacitance for channel 0, type:
cat in_capacitance0_raw 31152
To read the mean raw capacitance for channel 0, type:
cat in_capacitance0_mean_raw 38195
If you want to read the capacitance for another channel, replace in_capacitance0_raw with, for example, in_capacitance1_raw.
The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete.