This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:ad5628 [03 Aug 2012 10:43] – func descr Alexandru.Tofan | resources:fpga:xilinx:pmod:ad5628 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 6: | Line 6: | ||
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
- | * [[http:// | + | * [[http:// |
- | **System:** Microblaze, AXI, UART \\ | + | |
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
Line 15: | Line 15: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
+ | * [[http:// | ||
* [[http:// | * [[http:// | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). |
- | * A UART terminal (Tera Term/ | + | * A UART terminal (Tera Term/ |
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <note tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
- | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | + | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// |
- | </note> | + | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// |
- | + | ||
- | Extract the project from the archive file (AD5628_< | + | |
==== Avnet LX9 MicroBoard Setup ==== | ==== Avnet LX9 MicroBoard Setup ==== | ||
- | To begin, connect the PmodDA4 to J4 connector of LX9 board, pins 1 to 6 (see image below). You can use an extension cable for ease of use. Connect the USB cables | + | Extract the project from the archive file (AD5628_< |
+ | |||
+ | To begin, connect the PmodDA4 to J4 connector of LX9 board, pins 1 to 6 (see image below). You can use an extension cable for ease of use. Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector. | ||
{{: | {{: | ||
Line 41: | Line 42: | ||
==== Digilent Nexys™3 Spartan-6 FPGA Board ==== | ==== Digilent Nexys™3 Spartan-6 FPGA Board ==== | ||
- | To begin, connect the PmodDA4 to JA connector of Nexys™3 board, pins JA1 to JA6 (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board. | + | Extract the project from the archive file (AD5628_< |
+ | |||
+ | To begin, connect the PmodDA4 to JB connector of Nexys™3 board, pins JB1 to JB6 (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). | ||
{{: | {{: | ||
- | ==== FPGA Configuration ==== | + | ==== Avnet ZedBoard ==== |
+ | |||
+ | To begin, connect the PmodDA4 to JA1 connector of ZedBoard (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ==== FPGA Configuration | ||
Start IMPACT, and double click " | Start IMPACT, and double click " | ||
{{: | {{: | ||
+ | |||
+ | ==== FPGA Configuration for ZedBoard ==== | ||
+ | |||
+ | Run the **download.bat** script from the " | ||
+ | The script will automatically configure the ZYNQ SoC and download the *.elf file afterwards. | ||
+ | |||
+ | <WRAP center round tip 80%> | ||
+ | If the download script fails to run, modify the Xilinx Tools path in **download.bat** to match your Xilinx Installation path. | ||
+ | </ | ||
If programming was successful, the **Main Menu** will apear in your UART terminal, as seen in the picture below. | If programming was successful, the **Main Menu** will apear in your UART terminal, as seen in the picture below. | ||
- | The user has 2 options: | + | There are 3 options: |
- | * Press **[1]** to select **Fixed Value Mode**. | + | * Press **[f]** to select **Fixed Value Mode**. |
- | * Press **[2]** to select **Waveform Generation Mode**. | + | * Press **[w]** to select **Waveform Generation Mode**. |
+ | * Press **[p]** to select **Programmable Ramp Signal Generator**. | ||
- | {{: | + | {{: |
- | When entering **Fixed Value Mode**, | + | When entering **Fixed Value Mode**, |
- | {{: | + | {{: |
- | **Fixed Value Mode** allows | + | **Fixed Value Mode** allows |
{{: | {{: | ||
Line 68: | Line 87: | ||
Pressing the **[q]** key at any time exits the Fixed Value (or Waveform Generation) Mode and displays the **Main Menu** again. | Pressing the **[q]** key at any time exits the Fixed Value (or Waveform Generation) Mode and displays the **Main Menu** again. | ||
- | {{: | + | {{: |
- | When entering **Waveform Generation Mode**, | + | When entering **Waveform Generation Mode**, |
- | {{: | + | {{: |
- | **Waveform Generation Mode** allows | + | **Waveform Generation Mode** allows |
- | {{: | + | {{: |
+ | |||
+ | **Programmable Ramp Signal Generator** allows generating a programmable ramp signal. This mode can be used to test the PmodDA4 using a Digital Multimeter. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Enter time step** allows setting a time step between **100** and **5000** ms. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Enter increment size** allows selecting an increment size that suits your design. Values can vary from **0x000** to **0xFFF**. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Select DAC** allows selecting which DAC Output will be used for the Ramp Signal Generation. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Run Ramp Signal Generator** will start generating the desired output. | ||
+ | |||
+ | {{: | ||
Line 85: | Line 124: | ||
The reference design is a simple SPI interface used to communicate with the PmodDA4. The software programs the device sending 12-bit data values read from the keyboard input or from predefined look up tables. The user has the ability to select between two modes: a Fixed Value Mode or a Waveform Generation Mode. Communication between the user and the board is done via UART. | The reference design is a simple SPI interface used to communicate with the PmodDA4. The software programs the device sending 12-bit data values read from the keyboard input or from predefined look up tables. The user has the ability to select between two modes: a Fixed Value Mode or a Waveform Generation Mode. Communication between the user and the board is done via UART. | ||
- | <note important> | + | <WRAP round important |
+ | \\ | ||
* Connecting the PmodDA4 to the boards using an extension cable provides ease of use. | * Connecting the PmodDA4 to the boards using an extension cable provides ease of use. | ||
- | * UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard or 9600 Baud Rate for the Digilent Nexys™3 Board. | + | * UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard |
- | </note> | + | \\ |
+ | </WRAP> | ||
+ | <WRAP round important 80%> | ||
+ | When using the ZedBoard reference design in order to develop your own software, please make sure that the following options are set in " | ||
+ | |||
+ | <code c> | ||
+ | // Select between PS7 or AXI Interface | ||
+ | #define USE_PS7 1 | ||
+ | // SPI used in the design | ||
+ | #define USE_SPI 1 | ||
+ | // I2C used in the design | ||
+ | #define USE_I2C 0 | ||
+ | // Timer (+interrupts) used in the design | ||
+ | #define USE_TIMER 1 | ||
+ | // External interrupts used in the design | ||
+ | #define USE_EXTERNAL | ||
+ | // GPIO used in the design | ||
+ | #define USE_GPIO | ||
+ | </ | ||
+ | |||
+ | </ | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | {{: | ||
- | {{: | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | **Avnet LX-9 MicroBoard: **\\ | ||
+ | * {{: | ||
+ | |||
+ | **Digilent Nexys™3: | ||
+ | * {{: | ||
+ | |||
+ | **Avnet ZedBoard: | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | | ||
+ | </ | ||
+ | |||
+ | <wrap hide> | ||
+ | ====== Linux Device Driver ====== | ||
+ | |||
+ | Connect PmodDA4 to the JB1 connector of the ZedBoard (upper row of pins). | ||
+ | |||
+ | ===== Preparing the SD Card ===== | ||
+ | |||
+ | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
+ | * Download the device tree: [[https:// | ||
+ | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | ||
+ | * [[/ | ||
+ | |||
+ | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
+ | If everything is correct, the system should boot up. If you don't have an HDMI monitor, connect to the board via UART, Baud Rate 115200. | ||
+ | |||
+ | There are 2 ways to test the driver. | ||
+ | * Using the terminal window | ||
+ | * Using a serial terminal | ||
+ | |||
+ | ===== Using the terminal window ===== | ||
+ | |||
+ | Open a new terminal window by pressing **Ctrl+Alt+T**. | ||
+ | |||
+ | Navigate to the location of the device and identify it using the following commands: | ||
+ | < | ||
+ | cd / | ||
+ | ls | ||
+ | iio:device0 iio:device1 trigger0 | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | ad5628-1 | ||
+ | </ | ||
+ | |||
+ | If the **cat name** command doesn' | ||
+ | < | ||
+ | cd .. | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | </ | ||
+ | |||
+ | To see the list of options that the AD5628 driver provides, type: | ||
+ | < | ||
+ | ls | ||
+ | dev out_voltage4_powerdown_mode | ||
+ | name | ||
+ | out_voltage0_powerdown | ||
+ | out_voltage0_powerdown_mode | ||
+ | out_voltage0_raw | ||
+ | out_voltage0_scale | ||
+ | out_voltage1_powerdown | ||
+ | out_voltage1_powerdown_mode | ||
+ | out_voltage1_raw | ||
+ | out_voltage1_scale | ||
+ | out_voltage2_powerdown | ||
+ | out_voltage2_powerdown_mode | ||
+ | out_voltage2_raw | ||
+ | out_voltage2_scale | ||
+ | out_voltage3_powerdown | ||
+ | out_voltage3_powerdown_mode | ||
+ | out_voltage3_raw | ||
+ | out_voltage3_scale | ||
+ | out_voltage4_powerdown | ||
+ | </ | ||
+ | |||
+ | To set the raw output voltage for channel A, type: | ||
+ | < | ||
+ | echo 1200 > out_voltage0_raw | ||
+ | </ | ||
+ | |||
+ | To check that the raw output voltage has been set, you can type: | ||
+ | < | ||
+ | cat out_voltage0_raw | ||
+ | 1200 | ||
+ | </ | ||
+ | |||
+ | If you want to set the voltage for another channel, replace **out_voltage0_raw** with, for example, **out_voltage1_raw**. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete. | ||
+ | {{: | ||
+ | </ | ||
===== More information ===== | ===== More information ===== | ||
* [[ez> | * [[ez> | ||
* Example questions: {{rss> | * Example questions: {{rss> |