This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:ad5541a [20 Nov 2015 13:45] – hide linux, it is not supported at the moment Lars-Peter Clausen | resources:fpga:xilinx:pmod:ad5541a [25 Jan 2021 21:48] (current) – Moved PmodDA3 files to legacy, fixed links Adrian Costina | ||
---|---|---|---|
Line 6: | Line 6: | ||
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 16: | Line 16: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 29: | Line 29: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | ||
If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | ||
Line 154: | Line 154: | ||
**Avnet ZedBoard: | **Avnet ZedBoard: | ||
* [[https:// | * [[https:// | ||
- | * [[https:// | + | * [[https:// |
- | * [[https:// | + | * [[https:// |
- | * [[https:// | + | * [[https:// |
</ | </ | ||
<wrap hide> | <wrap hide> | ||
Line 166: | Line 166: | ||
In order to prepare the SD Card for booting Linux on the ZedBoard: | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
- | * Download the device tree: [[https:// | + | * Download the device tree: [[https:// |
* Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | ||
- | * [[http:// | + | * [[/ |
Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. |