This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:fpga:xilinx:kc705:adv7511 [10 Nov 2014 14:52] – [Supported Carriers] Lucian Sin | resources:fpga:xilinx:kc705:adv7511 [15 Apr 2015 14:22] – Vivado Updates Dragos Bogdan | ||
---|---|---|---|
Line 25: | Line 25: | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * Xilinx | + | * Xilinx |
- | * A UART terminal (Tera Term/ | + | * A UART terminal (Tera Term/ |
- | * For ISE, Baud rate 57600 for AC701/ | + | |
- | * For Vivado, Baud rate 115200 for AC701/ | + | |
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
Line 36: | Line 34: | ||
Run the **// | Run the **// | ||
- | **Note: | + | **Note: |
If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | ||
Line 163: | Line 161: | ||
The HDL Reference Designs and the no-OS Software can be downloaded from the Analog Devices Github.\\ | The HDL Reference Designs and the no-OS Software can be downloaded from the Analog Devices Github.\\ | ||
\\ | \\ | ||
- | <WRAP round important 80%> | ||
- | \\ | ||
- | The software project contains 2 components: the Reference Design files and the ADV7511 Transmitter Library. All the components have to be downloaded from the links below. | ||
- | </ | ||
**Evaluation Scripts:** | **Evaluation Scripts:** | ||
Line 205: | Line 199: | ||
* Questions? [[http:// | * Questions? [[http:// | ||
</ | </ | ||
- | ===== Tar file contents ===== | ||
- | |||
- | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http:// | ||
- | |||
- | | license.txt | ADI license & copyright information. | | ||
- | | system.mhs | ||
- | | system.xmp | ||
- | | data/ | UCF file and/or DDR MIG project files. | | ||
- | | docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). | | ||
- | | sw/ | Software (Xilinx SDK) & bit file(s). | | ||
- | | cf_lib/ | ||
- | |||
===== More information ===== | ===== More information ===== |