This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:kc705:adv7511 [19 Jun 2014 08:28] – [Software Setup for Vivado] Lucian Sin | resources:fpga:xilinx:kc705:adv7511 [24 Jul 2014 16:03] – added information about how to program a FPGA after an Engineer Zone discussion Lucian Sin | ||
---|---|---|---|
Line 156: | Line 156: | ||
* The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display the the result of the build. If the build is not done automatically select the // | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display the the result of the build. If the build is not done automatically select the // | ||
{{ : | {{ : | ||
- | * At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. | + | * At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. |
+ | {{ : | ||
+ | * Then choose this bitstream and press // | ||
+ | {{ : | ||
+ | * This window will appear next. | ||
+ | {{ : | ||
+ | * Afterwards a //Run Configuration// | ||
+ | {{ : | ||
* The no-OS drivers source code does the following actions: | * The no-OS drivers source code does the following actions: | ||
* Initializes the HDMI core; | * Initializes the HDMI core; |