This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:kc705:adv7511 [18 Jun 2014 10:36] – Added Software Setup for Vivado and links to HDL reference designs for Vivado for 6 boards(AC701,KC705,VC707,ZC702,ZC706,ZED) Lucian Sin | resources:fpga:xilinx:kc705:adv7511 [19 Jun 2014 08:28] – [Software Setup for Vivado] Lucian Sin | ||
---|---|---|---|
Line 154: | Line 154: | ||
* In the same window, go to // | * In the same window, go to // | ||
{{ : | {{ : | ||
- | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display the the result of the build. If the build is not done automatically select the //**Project?Build Automatically**// | + | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display the the result of the build. If the build is not done automatically select the //**Project->Build Automatically**// |
{{ : | {{ : | ||
* At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. | * At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. |