This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:fpga:xilinx:kc705:adv7511 [24 Jul 2014 16:03] – added information about how to program a FPGA after an Engineer Zone discussion Lucian Sin | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== ADV7511 Xilinx Evaluation Boards Reference Design ====== | ||
+ | |||
+ | ===== Introduction ===== | ||
+ | The [[adi> | ||
+ | |||
+ | ===== Supported Carriers ===== | ||
+ | |||
+ | ^ Board ^ XPS ^ Vivado | ||
+ | | [[xilinx> | ||
+ | | [[xilinx> | ||
+ | | [[xilinx> | ||
+ | | [[xilinx> | ||
+ | | [[xilinx> | ||
+ | | [[http:// | ||
+ | Board]] | **x** | **x** | | ||
+ | |||
+ | <WRAP round important 80%> | ||
+ | \\ | ||
+ | The XPS projects remain on this website only for legacy purposes. The support for them has been discontinued. | ||
+ | </ | ||
+ | |||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | |||
+ | * AC701/ | ||
+ | * HDMI Monitor. | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | |||
+ | * Xilinx ISE 14.6 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | ||
+ | * A UART terminal (Tera Term/ | ||
+ | * For ISE, Baud rate 57600 for AC701/ | ||
+ | * For Vivado, Baud rate 115200 for AC701/ | ||
+ | |||
+ | ==== Running Demo (SDK) Program ==== | ||
+ | |||
+ | To begin, connect an HDMI cable between the board HDMI out and the HDMI monitor. After the hardware setup, turn the power on to the board. | ||
+ | |||
+ | Run the **// | ||
+ | |||
+ | **Note:** The // | ||
+ | |||
+ | If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The reference design contains an example of how to: | ||
+ | * Initialize the ADV7511 High-Definition Multimedia Interface (HDMI®) transmitter. | ||
+ | * Check current AVR operating mode and depending on this result set the AV mute state. | ||
+ | * Display an image and play a sound. | ||
+ | |||
+ | ===== Using the reference design ===== | ||
+ | |||
+ | ==== Functional description ==== | ||
+ | |||
+ | |{{.: | ||
+ | |||
+ | The reference design consists of two independent pcore modules. | ||
+ | |||
+ | The video part consists of a Xilinx VDMA interface and the ADV7511 video interface. The ADV7511 interface consists of a 16bit YCbCr 422 with separate synchorinzation signals. The VDMA streams frame data to this core. The internal buffers of this pcore are small (1k) and do NOT buffer any frames as such. Additional resources may cause loss of synchronization due to DDR bandwidth requirements. The video core is capable of supporting any formats through a set of parameter registers (given below). The pixel clock is generated internal to the device and must be configured for the correct pixel frequency. It also allows a programmable color pattern for debug purposes. A zero to one transition on the enable bits trigger the corresponding action for HDMI enable and color pattern enable. | ||
+ | |||
+ | The reference design defaults to the 1080p video mode. Users may change the video settings by programming the following registers. The core requires a corresponding pixel clock to generate the video. This clock must be generated externally. | ||
+ | |||
+ | **HSYNC count**: is the total horizontal pixel clocks of the video, for 1080p this is 2200.\\ | ||
+ | **HSYNC width**: is the pulse width in pixel clocks, for 1080p this is 44.\\ | ||
+ | **HSYNC DE Minimum**: is the number of pixel clocks for the start of active video and is the sum of horizontal sync width and back porch, | ||
+ | **HSYNC DE Maximum**: is the number of pixel clocks for the end of active video and is the sum of horizontal sync width, back porch and the active video count, | ||
+ | \\ | ||
+ | **VSYNC count**: is the total vertical pixel clocks of the video, for 1080p this is 1125.\\ | ||
+ | **VSYNC width**: is the pulse width in pixel clocks, for 1080p this is 5.\\ | ||
+ | **VSYNC DE Minimum**: is the number of pixel clocks for the start of active video and is the sum of vertical sync width and back porch, | ||
+ | **VSYNC DE Maximum**: is the number of pixel clocks for the end of active video and is the sum of vertical sync width, back porch and the active video count, | ||
+ | \\ | ||
+ | Note that the pixel frequency for 1080p is 148.5MHz. | ||
+ | |||
+ | The reference design reads 24bits of RGB data from DDR and performs color space conversion (RGB to YCbCr) and down sampling (444 to 422). If bypassed, the lower 16bits of DDR data is passed to the HDMI interface as it is. | ||
+ | |||
+ | A color pattern register provides a quick check of any RGB values on the monitor. If enabled, the register data is used as the pixel data for the entire frame. | ||
+ | |||
+ | The audio part consists of a Xilinx DMA interface and the ADV7511 spdif audio interface. The audio clock is derived from the bus clock. A programmable register (see below) controls the division factor. The audio data is read from the DDR as two 16bit words for the left and right channels. It is then transmitted on the SPDIF frame. The sample frequency and format may be controlled using the registers below. The reference design defaults to 48KHz. | ||
+ | |||
+ | ==== Registers ==== | ||
+ | |||
+ | Please refer to the regmap.txt file inside the pcores. | ||
+ | |||
+ | ==== Audio Registers (axi_spdif_tx) ==== | ||
+ | |||
+ | ^ QW Address< | ||
+ | | 0x00 | 23:20| 0 | mode | Sample format 0 to 8 (0-16bit, 8-24bit). | | ||
+ | | | 15:8 | 0 | ratio | Clock divider for the transmit frequency = bus_clock/ | ||
+ | | | 1 | 0 | txdata | ||
+ | | | 0 | 0 | txenable | ||
+ | | 0x01 | 7:6 | 0 | frequency | ||
+ | | | 3 | 0 | gstat | Generation status original/ | ||
+ | | | 2 | 0 | pre-emphasis | ||
+ | | | 1 | 0 | copy | Copy permitted (0x1) or inhibited (0x0) (RO). | | ||
+ | | | 0 | 0 | audio | Data format is non-audio (0x1) or audio (0x0) (RO). | | ||
+ | | 1. For AXI-Lite byte addresses, multiply by 4. ||||| | ||
+ | |||
+ | ===== Using the Software Reference Design ===== | ||
+ | |||
+ | The Software Reference Design uses the **ADV7511 Transmitter Library** which is a collection of APIs that provide a consistent interface to ADV7511. The library is a software layer that sits between the application and the TX hardware and it is intended to serve two purposes: | ||
+ | * Provide the application with a set of APIs that can be used to configure HDMI TX hardware without the need for low-level register access. This makes the application portable across different revisions of the hardware and even across different hardware modules. | ||
+ | * Provide basic services to aid the application in controlling the TX module, such as interrupt service routine, HDCP high-level control and status information. | ||
+ | |||
+ | The documentation for the library' | ||
+ | |||
+ | The project contains 2 components: the Reference Design files and the ADV7511 Transmitter Library. All the components have to be downloaded from the links provided in the **Downloads** section. | ||
+ | |||
+ | ==== Software Setup for ISE Design Suite ==== | ||
+ | The **HDL Reference Design** for each supported Xilinx FPGA board contains a folder called // | ||
+ | These are the steps that need to be followed to recreate the software project: | ||
+ | * Copy the // | ||
+ | * Copy the library file to the // | ||
+ | {{ : | ||
+ | * Copy the library headers to the // | ||
+ | {{ : | ||
+ | * Copy the Reference Design files to the // | ||
+ | {{ : | ||
+ | * Open the Xilinx SDK. When the SDK starts it asks for a to provide a folder where to store the workspace. Any folder can be provided. | ||
+ | * In the SDK select the // | ||
+ | {{ : | ||
+ | * In the //Import// window select the // | ||
+ | {{ : | ||
+ | * In the //Import Projects// window select the // | ||
+ | {{ : | ||
+ | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the //Console// window will display the the result of the build. If the build is not done automatically select the // | ||
+ | {{ : | ||
+ | |||
+ | ==== Software Setup for Vivado ==== | ||
+ | |||
+ | Example for a ZC702 board: | ||
+ | * After [[http:// | ||
+ | * Open the Xilinx SDK for Vivado. When the SDK starts it asks to provide a folder where to store the workspace. Any folder can be provided. | ||
+ | * Go to // | ||
+ | {{ : | ||
+ | * Use a new hardware platform, so choose //**Create new**// in // | ||
+ | {{ : | ||
+ | * In //**Target Hardware Specification**// | ||
+ | {{ : | ||
+ | * Then give a name to the project and click // | ||
+ | {{ : | ||
+ | * In the next window choose //**Empty Application**// | ||
+ | {{ : | ||
+ | * Now the project without source code looks like this | ||
+ | {{ : | ||
+ | * Then the no-OS software for the used FPGA board must be added from Github. Also the library must be added (ZC library for a Zynq based platform or Microblaze library for AC701, | ||
+ | {{ : | ||
+ | * Afterwards click right on project name and go to // | ||
+ | {{ : | ||
+ | * In the window that appears, go to // | ||
+ | {{ : | ||
+ | * In the same window, go to // | ||
+ | {{ : | ||
+ | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display the the result of the build. If the build is not done automatically select the // | ||
+ | {{ : | ||
+ | * At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. You can program the FPGA by going to //**Xilinx Tools**//. | ||
+ | {{ : | ||
+ | * Then choose this bitstream and press // | ||
+ | {{ : | ||
+ | * This window will appear next. | ||
+ | {{ : | ||
+ | * Afterwards a //Run Configuration// | ||
+ | {{ : | ||
+ | |||
+ | * The no-OS drivers source code does the following actions: | ||
+ | * Initializes the HDMI core; | ||
+ | * Initializes the ADV7511 part; | ||
+ | * Transmits to a HDMI capable monitor an image whoose resolution can be changed by typing in the terminal a number from 0 to 6; | ||
+ | * Transmits to a HDMI capable monitor a sound. | ||
+ | * This is what is transmitted through UART: | ||
+ | {{ : | ||
+ | * The output of the example program can be viewed in the SDK console by enabling the //Connect STDIO Console// option and setting the baud rate of the UART port to 115200. | ||
+ | {{ : | ||
+ | |||
+ | As an alternative an UART terminal can be used to capture the output of the example program. The number of used UART port depends on the computer' | ||
+ | * Baud Rate: 115200bps | ||
+ | * Data: 8 bit | ||
+ | * Parity: None | ||
+ | * Stop bits: 1 bit | ||
+ | * Flow Control: none | ||
+ | |||
+ | |||
+ | ===== Downloads ===== | ||
+ | |||
+ | The HDL Reference Designs and the no-OS Software can be downloaded from the Analog Devices Github.\\ | ||
+ | \\ | ||
+ | <WRAP round important 80%> | ||
+ | \\ | ||
+ | The software project contains 2 components: the Reference Design files and the ADV7511 Transmitter Library. All the components have to be downloaded from the links below. | ||
+ | </ | ||
+ | |||
+ | **Evaluation Scripts:** | ||
+ | <WRAP round download 80%> | ||
+ | * **AC701 Evaluation Script: ** [[https:// | ||
+ | * **KC705 Evaluation Script: ** [[https:// | ||
+ | * **VC707 Evaluation Script: ** [[https:// | ||
+ | * **ZC702 Evaluation Script: ** [[https:// | ||
+ | * **ZC706 Evaluation Script: ** [[https:// | ||
+ | * **Zed Evaluation Script: ** [[https:// | ||
+ | </ | ||
+ | |||
+ | **HDL Reference Designs:** | ||
+ | <WRAP round download 80%> | ||
+ | * **AC701 HDL Reference Design for ISE: ** [[https:// | ||
+ | * **KC705 HDL Reference Design for ISE: ** [[https:// | ||
+ | * **VC707 HDL Reference Design for ISE: ** [[https:// | ||
+ | * **ZC702 HDL Reference Design for ISE: ** [[https:// | ||
+ | * **ZC706 HDL Reference Design for ISE: ** [[https:// | ||
+ | * **Zed HDL Reference Design for ISE: ** [[https:// | ||
+ | |||
+ | * **AC701 HDL Reference Design for Vivado: ** https:// | ||
+ | * **KC705 HDL Reference Design for Vivado: ** https:// | ||
+ | * **vC707 HDL Reference Design for Vivado: ** https:// | ||
+ | * **ZC702 HDL Reference Design for Vivado: ** https:// | ||
+ | * **ZC706 HDL Reference Design for Vivado: ** https:// | ||
+ | * **ZED HDL Reference Design for Vivado: ** https:// | ||
+ | </ | ||
+ | |||
+ | **no-OS Software:** | ||
+ | <WRAP round download 80%> | ||
+ | * **ADV7511 MicroBlaze Library: ** https:// | ||
+ | * **ADV7511 AC701 Reference Design: ** https:// | ||
+ | * **ADV7511 KC705 Reference Design: ** https:// | ||
+ | * **ADV7511 VC707 Reference Design: ** https:// | ||
+ | * **ADV7511 ZC Library: ** https:// | ||
+ | * **ADV7511 ZC702 Reference Design: ** https:// | ||
+ | * **ADV7511 ZC706 Reference Design: ** https:// | ||
+ | * **ADV7511 ZedBoard Library: ** https:// | ||
+ | * **ADV7511 ZedBoard Reference Design: ** https:// | ||
+ | </ | ||
+ | |||
+ | <WRAP round help 80%> | ||
+ | \\ | ||
+ | * Questions? [[http:// | ||
+ | </ | ||
+ | ===== Tar file contents ===== | ||
+ | |||
+ | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http:// | ||
+ | |||
+ | | license.txt | ADI license & copyright information. | | ||
+ | | system.mhs | ||
+ | | system.xmp | ||
+ | | data/ | UCF file and/or DDR MIG project files. | | ||
+ | | docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). | | ||
+ | | sw/ | Software (Xilinx SDK) & bit file(s). | | ||
+ | | cf_lib/ | ||
+ | |||
+ | |||
+ | ===== More information ===== | ||
+ | |||
+ | * [[ez> | ||
+ | * [[resources/ |