This is an old revision of the document!
The AD9122 is a dual 16-bit, high dynamic range, digital-to-analog converter (ADC) that provides a sample rate of 1200MSPS. This reference design includes two DDS generators that drives both channels of the device. The programming is done via the USB-SPI interface.
HW Platform(s): Virtex-6 ML605 (Xilinx), AD9122 Evaluation Board (ADI), DAC FMC Interposer Board (ADI)
System: Microblaze, AXI, UART
The bit file provided combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal, ADI DAC software and the programmer (IMPACT).
If you are not familiar with ML605 and/or Xilix tools, please visit
http://www.xilinx.com/products/boards/ml605/reference_designs.htm for details.
To begin make the following connections (see image below):
Setup the clock source to be 1GHz. After the hardware setup, turn the power on to the ML605 and the AD9122-M537x-EBZ boards.
Start ADI- AD9122 SPI program (see screenshot below)-
Start IMPACT, and initialze the JTAG chain. The program should recognize the Virtex 6 device (see screenshot below). Start a UART terminal (set to 57600 baud rate) and then program the device.
If programming was successful, you should be seeing messages appear on the terminal as shown in figure below.
After DDS is enabled, you should see the spectrum analyzer displaying the two tones (90MHz and 70MHz).
The reference design consists of two independent DDS modules and a lvds interface.
The DDS module consists of a Xilinx IP core and a DDR-DDS. Internally the DDS runs at fDAC/3 clock. The DDR-DDS allows any pattern to be generated in the memory to be driven to the DAC. The output samples are interleaved and driven by the lvds interface.
Please see the regmap.txt file in the pcore directory.
The following two files are missing from the tar file.
To use the reference design as it is, re-generate these two files (16bit full-range sine DDS).
The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to Xilinx EDK documentation for details.
license.txt | ADI license & copyright information. |
system.mhs | MHS file. |
system.xmp | XMP file (use this file to build the reference design). |
data/ | UCF file and/or DDR MIG project files. |
docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). |
sw/ | Software (Xilinx SDK) & bit file(s). |
cf_lib/edk/pcores/ | Reference design core file(s) (Xilinx EDK). |