This document presents the steps to setup an environment for using the EVAL-AD5668SDZ evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-AD5668SDZ Evaluation Board with the Xilinx KC705 board.
For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to use the part evaluation setup. This consists of:
The SDP-B controller board is part of Analog Devices System Demonstration Platform (SDP). It provides a high speed USB 2.0 connection from the PC to the component evaluation board. The PC runs the evaluation software. Each evaluation board, which is an SDP compatible daughter board, includes the necessary installation file required for performance testing.
Note: it is expected that the analog performance on the two platforms may differ.
Below is presented a picture of SDP-B Controller Board with the EVAL-AD5668SDZ Evaluation Board.
The EVAL-AD5668EBZ / AD5668SD_Z evaluation board is a member of a growing number of boards available for the SDP. Designed to help customers evaluate performance or quickly prototype new AD5668 circuits and reduce design time, the EVAL-AD5668EBZ / AD5668SD_Z evaluation board can operate from a single 2.7 V to 5.5 V supply. The part incorporates an internal 1.25 V or 2.5 V on-board reference to give an output voltage span of 2.5 V or 5 V, respectively. The on-board reference is off at power-up allowing for the use of an external reference; the REF195 is used on this evaluation board. The AD5668 must be written to after power-up to turn on the internal reference.
The AD5668 is a low power, octal, 16-bit, buffered voltage-output DAC. The device operates from a single 2.7 V to 5.5 V supply and is guaranteed monotonic by design. The AD5668 has an on-chip reference with an internal gain of 2. The AD5668-1 has an 1.25 V 5 ppm/°C reference, giving a full-scale output range of 2.5 V; the AD5668-2, -3 has a 2.5 V 5 ppm/°C reference, giving a full-scale output range of 5 V. The on-board reference is off at power-up, allowing the use of an external reference. The internal reference is enabled via a software write. The AD5668 utilizes a versatile 3-wire serial interface that operates at clock rates of up to 50 MHz and is compatible with standard SPI®, QSPI™, MICROWIRE™, and DSP interface standards. The on-chip precision output amplifier enables rail-to-rail output swing.
The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project.
Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.
To power on the EVAL-AD5668 evaluation board, you need to provide +5V supply voltage to J1 connector on the board (LK1 position=A, LK6 position=A).
The following commands were implemented in this version of EVAL-AD5668 reference project for Xilinx KC705 FPGA board.
Command | Description |
---|---|
help? | Displays all available commands. |
reset! | Makes a power-on reset. |
powerMode= | Selects a given power mode for selected DAC. Accepted values: channel: 0 .. 7 - selected DAC A .. H. power mode: 0 - normal operation. 1 - 1KOhm to GND. 2 - 100KOhms to GND. 3 - three-state. |
powerMode? | Displays the power mode for one selected DAC. Accepted values: channel: 0 .. 7 - selected DAC A .. H. |
intRef= | Turns on/off the internal reference. Accepted values: 0 - turns off the internal reference. 1 - turns on the internal reference. |
intRef? | Displays the status of the internal reference. |
loadN= | Loads selected DAC register with a given value. Accepted values: channel: 0 .. 7 - selected DAC A .. H. 15 - all DACs. value: 0 .. 65535 - value to be written in register. |
updateN | Updates the selected DAC with the last value written in register. Accepted values: channel: 0 .. 7 - selected DAC A .. H. 15 - all DACs. value: 0 .. 65535 - value to be written in register. |
loadNUpdateN | Loads and updates the selected DAC with a given value. Accepted values: channel: 0 .. 7 - selected DAC A .. H. 15 - all DACs. value: 0 .. 65535 - value to be written in register. |
loadNUpdateAll | Loads the selected DAC with a given value and updates all DACs. Accepted values: channel: 0 .. 7 - selected DAC A .. H. 15 - all DACs. value: 0 .. 65535 - value to be written in register. |
enLdacPin= | Enables/Disables the LDAC pin for selected DAC. Accepted values: channel: 0 .. 7 - selected DAC A .. H. value: 1 - disable LDAC pin. 0 - enable LDAC pin. |
enLdacPin? | Displays the status(enabled or disabled) of the LDAC pin for a selected DAC. Accepted values: channel: 0 .. 7 - selected DAC A .. H. |
clrCode= | Loads Clear Code Register with specific clear code. Accepted values: 0 - clears code to zero scale when CLR pin goes from high to low. 1 - clears code to midscale when CLR pin goes from high to low. 2 - clears code to full scale when CLR pin goes from high to low. 3 - no operation. |
clrCode? | Displays the active clear code. |
ldacPin= | Sets the output value of LDAC pin. Accepted values: 0 - sets LDAC pin low.(default) 1 - sets LDAC pin high. |
ldacPin? | Displays the value of LDAC pin. |
clrPin= | Sets the output value of CLR pin. Accepted values: 0 - sets CLR pin low. 1 - sets CLR pin high.(default) |
clrPin? | Displays the value of CLR pin. |
Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA.
The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral.
The hardware platform for each reference projects with FMC-SDP interposer and KC705 evaluation board is common. The next steps should be followed to recreate the software project of the reference design: