Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
resources:fpga:xilinx:interposer:ad5542a [11 Sep 2013 10:52] – changed source code (without using Micrium uC-Probe), added Sofware Setup, remove programming with Impact Lucian Sinresources:fpga:xilinx:interposer:ad5542a [01 Oct 2013 14:23] – remove reference_design_files.zip, changed driver and commands, changed the links to Github for driver and commands Lucian Sin
Line 50: Line 50:
 <WRAP round download 80%> <WRAP round download 80%>
 \\ \\
-  * {{:resources:fpga:xilinx:interposer:cf_ad5542a_kc705.zip|Reference Design Files}} +  * **AD5542A Driver:** https://github.com/analogdevicesinc/no-OS/tree/master/device_drivers/AD5446 
-  * **AD5542A Driver:** https://github.com/analogdevicesinc/no-OS/tree/master/device_drivers/AD5542A +  * **AD5542A Commands:** https://github.com/analogdevicesinc/no-OS/tree/master/device_commands/AD5446
-  * **AD5542A Commands:** https://github.com/analogdevicesinc/no-OS/tree/master/device_commands/AD5542A+
   * **Xilinx Boards Common Drivers:** https://github.com/analogdevicesinc/no-OS/tree/master/platform_drivers/Xilinx/SDP_Common   * **Xilinx Boards Common Drivers:** https://github.com/analogdevicesinc/no-OS/tree/master/platform_drivers/Xilinx/SDP_Common
   * **EDK KC705 Reference project:** https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_sdp_kc705   * **EDK KC705 Reference project:** https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_sdp_kc705
Line 71: Line 70:
 <WRAP round important 80%> <WRAP round important 80%>
 \\ \\
-To power on the EVAL-AD5542A evaluation board, you need to provide external +5V and -5V supply voltage.+To power on the EVAL-AD5542A evaluation board, you need to provide external +5V and -5V supply voltage to J1 connector on the board (LK8 position=B, LK9 position=A, LK7 position=A, LK3 position=B, LK2 position=A).
 </WRAP> </WRAP>
- 
-===== Quick start evaluation ===== 
-For a quick start evaluation, run the **download.bat** script located in the **SDK/SDK_Workspace/bin** folder provided within the Reference Design Files.  This script uses XMD to program the FPGA with the HDL Reference Design and download the Software Reference Design into the DDR. 
- 
-<WRAP round info 80%> 
-\\ 
-The **download.bat** script assumes that the Xilinx ISE Design Suite 14.6 is installed at this path: **C:/Xilinx/14.6**. If the installation path on your computer is different, please modify the script accordingly. 
-</WRAP> 
- 
-If programming was successful, you should be seeing the command messages appear on the terminal. 
  
 ===== Reference Project Overview ===== ===== Reference Project Overview =====
resources/fpga/xilinx/interposer/ad5542a.txt · Last modified: 09 Jan 2021 00:48 by Robin Getz