This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:fmc:ad9467 [12 Mar 2014 18:05] – [AD9467 Native FMC Card / Xilinx Reference Design] Cybel Ran | resources:fpga:xilinx:fmc:ad9467 [10 Apr 2014 10:50] – [Clock Selection] Istvan Csomortani | ||
---|---|---|---|
Line 34: | Line 34: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | To begin, connect the AD9467-FMC-EBZ board to the FMC-LPC connector of ML605 (see image below) or KC705 or Zed board. If using VC707 connect to the FMC1-HPC. Connect power and two USB cables from the PC to the //JTAG// and //UART// USB connectors on the edge of the ML605. **The demo program uses the on board AD9517-4 to generate the input clock for the AD9467 A/D converter. ** The provided | + | To begin, connect the AD9467-FMC-EBZ board to the FMC-LPC connector of ML605 (see image below) or KC705 or Zed board. If using VC707 connect to the FMC1-HPC. Connect power and two USB cables from the PC to the //JTAG// and //UART// USB connectors on the edge of the ML605. ** The demo program uses the default |
{{: | {{: | ||
Line 86: | Line 86: | ||
The board provides three (some modification maybe necessary) possible clock path for clocking the AD9467. | The board provides three (some modification maybe necessary) possible clock path for clocking the AD9467. | ||
- | * Active | + | * External passive clock (default): A SMA connector is provided for an external clock source. |
- | * Optional external passive clock: A SMA connector is provided for an external clock source. | + | * Optional active |
* Optional oscillator: The connector P200 must be set to OSC-ON position. This can be enabled through the passive or active (AD9517) path. | * Optional oscillator: The connector P200 must be set to OSC-ON position. This can be enabled through the passive or active (AD9517) path. | ||