This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:fpga:xilinx:fmc:ad-fmcjesdadc1-ebz [29 Apr 2014 20:12] – [Running Demo (SDK) Program] rejeesh kutty | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== ADI AD-FMCJESDADC1-EBZ Boards & Xilinx Reference Design ====== | ||
+ | |||
+ | ===== Introduction ===== | ||
+ | <WRAP important> | ||
+ | |||
+ | The [[/ | ||
+ | |||
+ | <WRAP tip>This board is similar to the [[http:// | ||
+ | |||
+ | Also included in this wiki is a dual AD-FMCJESDADC1-EBZ on [[xilinx> | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | The boards also feature the [[adi> | ||
+ | |||
+ | It also features an external trigger input for customized sampling control. The card is mechanically and electrically compliant to the FMC standard (ANSI/VITA 57.1). | ||
+ | |||
+ | The reference design includes the device data capture via the JESD204B serial interface and the SPI interface. The samples are written to the external DDR-DRAM. It allows programming the device and monitoring it's internal registers via SPI. | ||
+ | |||
+ | ===== Supported Devices ===== | ||
+ | |||
+ | * [[adi> | ||
+ | |||
+ | ===== Supported Carriers ===== | ||
+ | |||
+ | * [[xilinx> | ||
+ | * [[xilinx> | ||
+ | * [[xilinx> | ||
+ | |||
+ | ===== Quick Start Guide ===== | ||
+ | |||
+ | The reference design zip file contains a bit file combined with a SDK elf file for a quick demonstration of the programming, | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | |||
+ | * ML605, KC705 or VC707 board | ||
+ | * AD-FMCJESDADC1-EBZ | ||
+ | * Signal generators (for ADC inputs) | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | |||
+ | * Xilinx ISE (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | ||
+ | * A UART terminal (Tera Term/ | ||
+ | |||
+ | ==== Bit file ==== | ||
+ | |||
+ | * Download the gzip file and extract the **sw/ | ||
+ | |||
+ | ==== Running Demo (SDK) Program ==== | ||
+ | |||
+ | Please Note: For Zynq devices, programming the bit file alone is not sufficient. You need to initialize PS7 and run the elf. Run the provided tcl script (sw/ | ||
+ | |||
+ | Example: xmd -tcl sw/ | ||
+ | |||
+ | |||
+ | To begin make the following connections (see image below): | ||
+ | |||
+ | * Connect the AD-FMCJESDADC1-EBZ board to the FMC-HPC connector of ML605/KC705 (FMC1-HPC if VC707) board. | ||
+ | * Connect power to ML605/ | ||
+ | * Connect two USB cables from the PC to the //JTAG// and //UART// USB connectors on ML605/ | ||
+ | * Connect signal generators to the A3, A2, A1 and/or A0 connectors. | ||
+ | |||
+ | The quick start bit file configures the AD9517 to generate 250MHz clock to AD9250. It runs both the ADCs through all test modes and verifies the captured data accordingly. After the hardware setup, turn the power on.. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Start IMPACT, and initialze the JTAG chain. The program should recognize the 7 series device. Start a UART terminal (set to 57600 baud rate) and then program the device. If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. After programming the devices, the program checks data capture on various test modes. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | After patterns and prbs sequences are verified, if no errors are present, you may use the chipscope busplot to see the captured signal (see below). A chipscope project file is available inside the sw directory. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== Using the reference design ===== | ||
+ | |||
+ | The reference design is built on a microblaze based system parameterized for linux. A functional block diagram of the design is given below. The reference design contains both ADC and DAC pcores. If you are using the AD-FMCJESDADC1-EBZ, | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The reference design consists of two identical instances of pcores for the DAC. On the ADC side, it consists of a single JESD core (using Xilinx IP) and two identical instances of AD9250 pcores. | ||
+ | |||
+ | The AD9129 core consists of three functional modules, the DAC interface, a DDS (using Xilinx IP) and a VDMA interface. The frequency of DDS may be set via the programming interface. Alternatively a custom data sequence may be used via the VDMA interface. | ||
+ | |||
+ | The AD9250 core consists of three functional modules, the ADC interface, a PN9/PN23 monitor and a DMA interface. | ||
+ | |||
+ | All the pcores have an AXI lite interface that allows control and monitoring of data generation and/or capture. | ||
+ | |||
+ | The reference design also includes HDMI cores for GTX eye scan. | ||
+ | |||
+ | ==== Registers ==== | ||
+ | |||
+ | Please refer to the regmap.txt file in the pcores directory. | ||
+ | |||
+ | ==== Changing ADC Sample Rates ==== | ||
+ | |||
+ | The ADC sampling rate can vary from 40MHz to 250MHz. However, there are limitations imposed by the FPGA that may lower this range. In some cases, you may have to regenerate the cores for a different range. The reference design uses GTX (channel PLL) primitives and Xilinx' | ||
+ | |||
+ | As of this writing, the GTX specification & switching characteristics may be found at: | ||
+ | |||
+ | [[http:// | ||
+ | [[http:// | ||
+ | |||
+ | The key switching characteristics are- | ||
+ | |||
+ | The reference clock has a range of 60MHz to 670MHz (700MHz). This limits the minimum sampling clock to 60MHz. Though it is NOT recommended, | ||
+ | |||
+ | The line rate however, varies based on speed grade, package type and the use of CPLL vs QPLL. The CPLL supports rates between 0.5Gbps to 6.6Gbps (the core may have to be changed for rates less than 3.2Gbps (sampling rate 160MHz) - and the IP may not support all the combinations). Again, it is possible to run the device on a single lane at a higher rate (rather than 2 lanes each at a lower rate) to circumvent some of the troubles of line rate dependency on parametrization, | ||
+ | |||
+ | You must carefully evaluate these specifications against your requirements to run the design at a specific sampling frequency (or a range). As always, if you have any questions or run into any problems, | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ==== JESD Interface ==== | ||
+ | |||
+ | The default chipscope also captures the GTX/JESD core interface for a quick check on the transfer phases. There is a simple state machine within the pcore that walks through all the phases of the JESD specification. A sample screenshot is given below. | ||
+ | |||
+ | The default signals are: | ||
+ | |||
+ | | The following signals are per lane (GTX). Refer to Xilinx documentation on details of these signals. || | ||
+ | | rx_data | GTX receive data (32 bits). | | ||
+ | | rx_notintable | GTX receive data not in table (invalid 8B/10B). | | ||
+ | | rx_disperr | GTX receive disparity error. | | ||
+ | | rx_charisk | GTX receive data is a K character . | | ||
+ | | rx_fsm | The state machine (see the pcore module for details). | | ||
+ | | rx_sync_enb | SYNC enable (SYNC is driven by JESD core, but is enabled by the state machine). | | ||
+ | | rx_sysref_enb | SYSREF enable (SYSREF is driven by all lanes at the end of CGS). | | ||
+ | | rx_valid_k | If set, indicates a valid ' | ||
+ | | rx_cgs_k | If set, indicates CGS data on received data. | | ||
+ | | rx_ilas_r | If set, indicates ' | ||
+ | | rx_ilas_a | If set, indicates ' | ||
+ | | rx_ilas_q | If set, indicates ' | ||
+ | | rx_ilas_f | If set, indicates ' | ||
+ | | The following signals are top level signals (common to all lanes) || | ||
+ | | jesd204b_rxsync_s | The sync is generated by the IP core. | | ||
+ | | gtx_rst_s | The GTX reset (software controlled). | | ||
+ | | jesd204b_rst_s | The JESD core reset (software controlled AND GTX). | | ||
+ | | rxsync | JESD204b SYNC | | ||
+ | | rxsysref | JESD204b SYSREF | | ||
+ | |||
+ | After reset (0x0), the FSM is at state 0x1, where it waits for CGS (Code Group Synchronization). After it finds a certain number of consecutive K characters (this ensures that the CGS phase is stable and lanes are all up and running), it asserts SYSREF and also enables SYNC. At state 3, it waits for SYNC to be deasserted. Note that enabling SYNC only allows the Xilinx core to drive the SYNC and do NOT deassert SYNC. The SYNC is soon deasserted by the JESD core and the FSM moves to state 4. At state 4, it is assumed that it is correctly done by the Xilinx IP core. At any point, if SYNC is asserted by the core, the process starts over. | ||
+ | |||
+ | Here is the sample screen shot: | ||
+ | |||
+ | {{: | ||
+ | |||
+ | |||
+ | ===== FMC-176 Information ===== | ||
+ | |||
+ | The [[http:// | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | The following variations of this board are available. | ||
+ | |||
+ | ^ Part Number ^ ADC Channels | ||
+ | | [[http:// | ||
+ | | [[http:// | ||
+ | | [[adi> | ||
+ | |||
+ | |||
+ | This reference design may be used as it is for FMC-176 and it's variations by selecting the appropriate number of DAC channels. It is also easy to port the design for other boards by removing one or more corresponding pcores. Also some devices may not be accessible depending on whether one choose to use LPC or HPC. To fully support both the DACs of the FMC-176, a carrier must have a fully populated HPC connector. The KC705 do not have a fully populated HPC. | ||
+ | |||
+ | The reference design includes (if enabled) RF generation via DDS and the SPI interface for the DACs. At the prompt just enter the number of DAC channels you have in your hardware setup. As an example, if you are using FMC-176 with KC705, simply enter ' | ||
+ | |||
+ | The quick start bit file also configures the AD9517 to generate a 2.5GHz clock to AD9129. It then generates a 333MHz tone for the DAC. | ||
+ | |||
+ | The DAC spectrum for a 333MHz tone is shown below. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | <WRAP center round important 80%> | ||
+ | It is possible to use an adapter board such as FMC-700 with KC705 to access both the DACs on a FMC-176 board. However, the routing delays of FMC-LPC pins to the FMC-700 will cause timing errors on DAC1 and you may see parity errors on the UART terminal. | ||
+ | </ | ||
+ | |||
+ | |||
+ | ===== Dual AD-FMCJESDADC1-EBZ ===== | ||
+ | |||
+ | In the downloads section, you will also find a dual AD-FMCJESDADC1-EBZ reference design for VC707. This design supports two AD-FMCJESDADC1-EBZ (4 x AD9250 devices) on VC707 using both the FMC1 and FMC2 connectors. It does NOT support any variations that includes AD9129. | ||
+ | |||
+ | The procedure is the same. The setup, UART and chipscope plots are shown below. | ||
+ | |||
+ | |{{: | ||
+ | |{{: | ||
+ | |||
+ | |||
+ | ===== Downloads ===== | ||
+ | |||
+ | FPGA Referece Designs: | ||
+ | <WRAP round download 80%> | ||
+ | * ** ML605 ** {{: | ||
+ | * ** KC705 ** {{: | ||
+ | * ** VC707 ** {{: | ||
+ | * ** VC707 ** {{: | ||
+ | * ** ZC706 ** {{: | ||
+ | </ | ||
+ | |||
+ | Software Files: | ||
+ | <WRAP round download 80%> | ||
+ | * ** ML605 ** {{: | ||
+ | * ** KC705 ** {{: | ||
+ | * ** VC707 ** {{: | ||
+ | * ** VC707 ** {{: | ||
+ | * ** ZC706 ** {{: | ||
+ | </ | ||
+ | |||
+ | |||
+ | Only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[http:// | ||
+ | |||
+ | <WRAP round help 80%> | ||
+ | * Questions? [[http:// | ||
+ | </ | ||
+ | |||
+ | ===== Tar file contents ===== | ||
+ | |||
+ | The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to [[http:// | ||
+ | |||
+ | | license.txt | ADI license & copyright information. | | ||
+ | | system.mhs | ||
+ | | system.xmp | ||
+ | | data/ | UCF file and/or DDR MIG project files. | | ||
+ | | docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). | | ||
+ | | sw/ | Software (Xilinx SDK) & bit file(s). | | ||
+ | | cf_lib/ | ||
+ | |||
+ | |||
+ | ===== More information ===== | ||
+ | |||
+ | * [[http:// | ||
+ | * [[ez> |