This is an old revision of the document!
The util_axis_fifo_asym IP core is a simple FIFO (First Input First Output) with AXI streaming interfaces, supporting synchronous and asynchronous operation modes with an asymmetric data width on its salve and master interface. It can be used to mitigate data width differences or transfer an AXI stream to a different clock domain.
The FIFO is based on the util_axis_fifo, using it as its atomic building block.
The configuration of the atomic util_axis_fifo blocks are calculated as follows:
// atomic parameters - NOTE: depth is always defined by the slave attributes localparam A_WIDTH = (RATIO_TYPE) ? M_DATA_WIDTH : S_DATA_WIDTH; localparam A_ADDRESS = (RATIO_TYPE) ? S_ADDRESS_WIDTH : (S_ADDRESS_WIDTH-$clog2(RATIO)); localparam A_ALMOST_FULL_THRESHOLD = (RATIO_TYPE) ? ALMOST_FULL_THRESHOLD : (ALMOST_FULL_THRESHOLD/RATIO); localparam A_ALMOST_EMPTY_THRESHOLD = (RATIO_TYPE) ? (ALMOST_EMPTY_THRESHOLD/RATIO) : ALMOST_EMPTY_THRESHOLD;
The depth of the FIFO is defined by the following equation, which is a function of the S_ADDRESS_WIDTH and S_DATA_WIDTH parameters:
FIFO depth in bytes = S_DATA_WIDTH/8 * 2 ^ S_ADDRESS_WIDTH
The FIFO has three different status indicator ports on both side, which provides information about the state of the FIFO for both the source and destination logic:
Name | Description | Default Value |
---|---|---|
DATA_WIDTH | Data width of AXI streaming interface | 64 |
ADDRESS_WIDTH | Width of the address, defines the depth of the FIFO | 5 |
ASYNC_CLK | Clocking mode, if set the FIFO operates on asynchronous mode | 1 |
M_AXIS_REGISTERED | Add and additional register stage to the AXI stream master interface | 1 |
ALMOST_EMPTY_THRESHOLD | Defines the offset (in data beats) between the almost empty and empty assertion | 16 |
ALMOST_FULL_THRESHOLD | Defines the offset (in data beats) between the almost full and full assertion | 16 |
Interface/Pin | Type | Description | |
---|---|---|---|
Slave AXI Stream interface | |||
s_axis_aclk | input | Slave AXI stream clock signal | |
s_axis_aresetn | input | Slave AXI stream reset signal (active low) | |
s_axis_ready | output | Slave AXI stream ready | |
s_axis_valid | input | Slave AXI stream valid | |
s_axis_data | input[DATA_WIDTH-1:0] | Slave AXI stream ready | |
s_axis_tlast | input | Slave AXI stream TLAST signal, for packet boundary | |
s_axis_room | output[ADDRESS_WIDTH-1:0] | Indicates how much space (in data beats) is in the FIFO | |
s_axis_almost_empty | output | If set the FIFO is almost empty | |
s_axis_empty | output | If set the FIFO is empty | |
Master AXI Stream interface | |||
m_axis_aclk | input | Master AXI stream clock signal | |
m_axis_aresetn | input | Master AXI stream reset signal (active low) | |
m_axis_ready | input | Master AXI stream ready | |
m_axis_valid | output | Master AXI stream valid | |
m_axis_data | output[DATA_WIDTH-1:0] | Master AXI stream ready | |
m_axis_tlast | output | Master AXI stream TLAST signal, for packet boundary | |
m_axis_level | output[ADDRESS_WIDTH-1:0] | Indicates how much data is in the FIFO | |
m_axis_almost_full | output | If set the FIFO is almost full | |
m_axis_full | output | If set the FIFO is full |
This core does not have a register map.