This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:fpga:altera:ced1z:ad7689 [05 Nov 2012 21:20] – [Software Tools] Andrei Cozma | resources:fpga:altera:ced1z:ad7689 [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 188: | Line 188: | ||
* 6. After the programming ends, power off the CED1Z and reprogramm it using program_fpga.bat as described above. | * 6. After the programming ends, power off the CED1Z and reprogramm it using program_fpga.bat as described above. | ||
- | <note> This is a one time operation, as the programming is done on a non volatile memory on the Evaluation Board. In order to restore the original firmware on the Evaluation Board, at step 4 use the configuration file from the CD at Evaluation Board FPGA code/uMUX FPGA CED 2-2/ | + | <WRAP round help> This is a one time operation, as the programming is done on a non volatile memory on the Evaluation Board. In order to restore the original firmware on the Evaluation Board, at step 4 use the configuration file from the CD at Evaluation Board FPGA code/uMUX FPGA CED 2-2/ |
In order to acquire data, follow the instructions in the // | In order to acquire data, follow the instructions in the // | ||
Line 203: | Line 203: | ||
* 3. data_capture8chan.bat, | * 3. data_capture8chan.bat, | ||
- | <note>When changing between the data capture scripts the system must be reinitialized by reprogramming the FPGA.</note> | + | <WRAP round help>When changing between the data capture scripts the system must be reinitialized by reprogramming the FPGA.</WRAP> |
If the resulting csv file is opened with Microsoft Excel, the data will be displayed on a single column for the first script or on 8 columns for the second and third scripts. Each column represents a channel. If the AD7689 is configured to acquire less than 8 channels the remaining channels will have a constant value. For example, in the below picture, the AD7689 was configure to acquire data on 4 differential channels, a sine signal was applied on the first channel and the rest were left floating. In this case, the first column can be plotted as a sine wave, the next 3 have some noise on them, and the last 4 have a constant value of 0. | If the resulting csv file is opened with Microsoft Excel, the data will be displayed on a single column for the first script or on 8 columns for the second and third scripts. Each column represents a channel. If the AD7689 is configured to acquire less than 8 channels the remaining channels will have a constant value. For example, in the below picture, the AD7689 was configure to acquire data on 4 differential channels, a sine signal was applied on the first channel and the rest were left floating. In this case, the first column can be plotted as a sine wave, the next 3 have some noise on them, and the last 4 have a constant value of 0. |