This document presents the steps to setup an environment for using the EVAL-AD7606EDZ / EVAL-AD7606-6EDZ / EVAL-AD7606-4EDZ evaluation board together with the EVAL-CED Converter Evaluation and Development (CED) Board and the Nios II Embedded Development Suite (EDS). Below is presented a picture of the EVAL-AD7606 Evaluation Board with the CED1 board.
The CED1Z board is intended for use in evaluation, demonstration and development of systems using Analog Devices precision converters. It provides the necessary communications between the converter and the PC, programming or controlling the device, transmitting or receiving data over a USB link.
The AD7606 / AD7606-6 / AD7606-4 are 16-bit, 8/6/4 channel, simultaneous sampling Analog-to-Digital Data Acquisition systems (DAS). The parts contain analog input clamp protection, 2nd order anti-alias filter, track and hold amplifier, 16-bit charge redistribution successive approximation ADC, flexible digital filter, 2.5V reference and reference buffer and high speed serial and parallel interfaces. The AD7606, AD7606-6, AD7606-4 operate from a single 5V supply and can accommodate ± 10V and ±5V true bipolar input signals while sampling at throughput rates up to 200 kSPS for all channels. The input clamp protection circuitry can tolerate voltages up to ±16.5V. The AD7606 has 1 MΩ analog input impedance regardless of sampling frequency. The single supply operation, on chip filtering and high input impedance eliminates the need for driver op-amps and external bipolar supplies. The AD7606 anti-alias filter has a 3 dB cut off frequency of 22 kHz and provides 40 dB anti-alias rejection when sampling at 200ksps. The flexible digital filter is pin driven, yields improvements in SNR, and reduces the 3 dB bandwidth.
The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project.
Below is presented the list of required hardware items:
Below is presented the list of required software tools:
The Quartus II design software and the Nios II EDS is available via the Altera Complete Design Suite DVD or by downloading from the web.
EVAL-AD7606EDZ Create a folder called “ADIEvalBoard” on your PC and extract the ad7606_evalboard.zip archive to this folder. Make sure that there are NO SPACES in the directory path. After extracting the archive the following folders should be present in the ADIEvalBoard folder: FPGA, Hdl, NiosCpu, Software and DataCapture .
| Folder | Description |
|---|---|
| FPGA | Contains all the files necessary to program the CED1Z board in order to evaluate the ADC. By executing the script program_fpga.bat the FPGA will be programmed with the evaluation project. New Nios2 applications can be created using the files from this folder. The ip subfolder contains the HDL core for connecting the evaluation board to the CED1Z board , the software drivers for HAL in /hdl/src/HAL and the AD7606 registers in /hdl/src/inc |
| Hdl | Contains the source files for the AD7606 HDL driver: - The doc subfolder contains a brief documentation for the core. - The src subfolder contains the HDL source files. - The tb folder contains the sources of the core's testbench |
| NiosCpu | Contains the CED1Z Quartus evaluation project source files . The ip subfolder contains the AD7606 QSYS component |
| Software | Contains the source files of the Nios2 SBT evaluation project |
| DataCapture | Contains the script files used for data acquisition |
The USB Blaster is used to program the FPGA on the CED1Z board and also for data exchange between the system and a PC. To install the driver plug the Terasic USB Blaster into one of the PCs USB ports. Your Windows PC will find the new hardware and try to install the driver.
Since Windows cannot locate the driver for the device the automatic installation will fail and the driver has to be installed manually. In the Device Manager right click on the USB-Blaster device and select Update Driver Software.
In the next dialog box select the option Browse my computer for driver software. A new dialog will open where it is possible to point to the driver’s location. Set the location to altera\11.0\quartus\drivers\usb-blaster and press Next.
If Windows presents you with a message that the drivers have not passed Windows Logo testing, please click “Install this driver software anyway”. Upon installation completion a message will be displayed to inform that the installation is finished.
The evaluation project contains all the source files needed to build a system that can be used to configure the AD7606 and capture data from it. The system consists of a Nios II softcore processor that is implemented in the FPGA found on the CED1Z board and a PC application. The softcore controls the communication with the Device Under Test (DUT) and the data capture process. The captured data is saved into the SRAM of the CED1Z board and aftwerwards it is read by the PC application and saved into a comma separated values (.csv) file that can be used for further data analysis.
The following components are implemented in the FPGA design:
| Name | Address | IRQ |
|---|---|---|
| CPU | 0x00000800 | - |
| PLL | 0x00000000 | - |
| ONCHIP_MEM | 0x00002000 | - |
| LEDS | 0x00000010 | - |
| SYSID | 0x00000020 | - |
| SRAM | 0x00200000 | - |
| TRISTATE_BRIDGE_0 | - | - |
| JTAG_UART_0 | 0x00000030 | 1 |
| SYS_TIMER | 0x00000040 | 2 |
| MM_CONSOLE_MASTER | - | - |
| PWR_DATA | 0x00000060 | - |
| I2C_INT | 0x00000080 | - |
| PWR_EN_CLK | 0x000000a0 | - |
| AD7606_0 | 0x000000c0 | - |
| Table 1 System components | ||
The Nios II processor contains a peripheral that implements the communication protocol with the DUT. The peripheral is divided into three logical modules: a module which implements the interface with the Avalon bus and the communication with the SRAM, a module which implements an Avalon master interface which is used to write data directly in the SRAM and a module which communicates with the AD7606.
Table 2 describes the port definitions of the Avalon peripheral:
| Port | Direction | Width | Description |
|---|---|---|---|
| Generic pins | |||
| CLK_I | IN | 1 | System clock. Designed with a 98MHz clock |
| RESET_I | IN | 1 | System reset |
| Avalon Slave Interface | |||
| AVALON_WRITEDATA_I | IN | 32 | Slave write data bus |
| AVALON_WRITE_I | IN | 1 | Slave write data request |
| AVALON_READ_I | IN | 1 | Slave read data request |
| AVALON_ADDRESS_I | IN | 3 | Slave address bus |
| AVALON_READDATA_O | OUT | 32 | Slave read data bus |
| Avalon Master Interface | |||
| AVALON_MASTER_WAITREQUEST | IN | 1 | Master wait request signal |
| AVALON_MASTER_ADDRESS_O | OUT | 32 | Master address bus |
| AVALON_MASTER_WRITE_O | OUT | 1 | Master write signal |
| AVALON_MASTER_BYTEENABLE_O | OUT | 2 | Master byte enable signals |
| AVALON_MASTER_WRITEDATA_O | OUT | 16 | Master write data bus |
| External connectors | |||
| ADC_DB_I | IN | 16 | ADC data bus used to read data from the AD7606 |
| ADC_BUSY_I | IN | 1 | ADC Busy Output. Logic output that indicates the status of the conversion. The BUSY output goes high following the falling edge of CONVST and stays high for the duration of the conversion. Once the conversion is complete and the result is available in the output register, the BUSY output goes low. The track-and-hold returns to track mode just prior to the falling edge of BUSY on the 13th rising edge of CLKIN |
| ADC_OS_O | OUT | 3 | Oversampling Mode Pins. These inputs are used to select the oversampling ratio |
| ADC_RANGE_O | OUT | 1 | Analog Input Range Selection. The polarity of this pin determines the input range of the analog input channels. If this pin is tied to a logic high, the analog input range is +-10V for all channels. If this pin is tied to a logic low, the analog input range is +-5V. A logic change has immediate effect. |
| ADC_CS_N_O | OUT | 1 | ADC Chip Select. Active low logic input used in conjunction with RD to read conversion data. |
| ADC_RD_N_O | OUT | 1 | ADC Read pin. Active low logic input used in conjunction with CS to access the conversion result. The conversion result is placed on the data bus following the falling edge of RD read while CS is low. |
| ADC_RESET_O | OUT | 1 | Reset pin. When set to logic high, the rising edge of RESET resets the AD7606. |
| ADC_STDBY_O | OUT | 1 | Standby Mode pin. This pin is used to place the AD7606 into one of the two power-down modes: standby mode or shutdown mode. The power-down mode entered depends on the state of the RANGE pin. |
| ADC_CONVST_N_O | OUT | 1 | ADC conversion Start Input. A falling edge on CONVST is used to initiate a conversion. The track-and-hold goes from track mode to hold mode on the falling edge of CONVST and the conversion process is initiated at this point. Following power-down, when operating in auto-shutdown or auto-standby modes, a rising edge on CONVST is used to power up the device. |
| Table 2 Port description | |||
Table 3 describes the registers of the Avalon peripheral:
| Name | Offset | Width | Access | Description |
|---|---|---|---|---|
| CONTROL_REGISTER | 0 | 32 | RW | Bit 0 is used to start data acquisition Bit 1 is used to initiate software reset of the core Bit 2 is used to configure the Avalon write master core to write data to the same location Bit 3 is used to write data to the AD7606 evaluation board |
| ACQ_COUNT_REGISTER | 1 | 32 | RW | Register used to configure the number of samples to be acquired when acquisition is started |
| BASE_REGISTER | 2 | 32 | RW | Register used to configure the base address of the memory location where the acquired data is to be written |
| STATUS | 3 | 32 | R | Bit 0 is used to signal that the acquisition is complete Bit 1 is used to signal that the internal memory buffer has been overflown Bit 2 is used to signal that the user has performed a write of a read only register register |
| DUT_WRITE_REGISTER | 4 | 32 | W | Register used to configure the driver submodule |
| Table 3 Register description | ||||
The follwing figure presents the timing diagram for the read operations from the AD7606 driver.
This module is the actual driver of the AD7606 data acquisition system.
| Port | Direction | Width | Description |
|---|---|---|---|
| General Connectors | |||
| FPGA_CLK_I | IN | 1 | 48 MHz clock |
| ADC_CLK_I | IN | 1 | 20 MHz clock |
| RESET_I | IN | 1 | Module reset |
| CED1Z_interface connectors | |||
| WR_DATA_N_I | IN | 1 | Signal used to write data in the driver’s internal registers |
| DATA_I | IN | 16 | Data bus, used configure the driver |
| DATA_O | OUT | 16 | Parallel bus to transfer the data to the upper module |
| DATA_RD_READY_O | OUT | 1 | Signals that at port DATA_O there is new data available |
| DATA_WR_READY_O | OUT | 1 | Signals that the write from upper module has been performed |
| SYNC_O | OUT | 1 | Signals that the next data transfer will correspond to channel 1 |
| AD7606 connectors | |||
| ADC_DB_I | IN | 16 | ADC data bus used to read data from the AD7606 |
| ADC_BUSY_I | IN | 1 | ADC Busy Output. Logic output that indicates the status of the conversion. The BUSY output goes high following the falling edge of CONVST and stays high for the duration of the conversion. Once the conversion is complete and the result is available in the output register, the BUSY output goes low. The track-and-hold returns to track mode just prior to the falling edge of BUSY on the 13th rising edge of CLKIN |
| ADC_OS_O | OUT | 3 | Oversampling Mode Pins. These inputs are used to select the oversampling ratio |
| ADC_RANGE_O | OUT | 1 | Analog Input Range Selection. The polarity of this pin determines the input range of the analog input channels. If this pin is tied to a logic high, the analog input range is +-10V for all channels. If this pin is tied to a logic low, the analog input range is +-5V. A logic change has immediate effect. |
| ADC_CS_N_O | OUT | 1 | ADC Chip Select. Active low logic input used in conjunction with RD to read conversion data. |
| ADC_RD_N_O | OUT | 1 | ADC Read pin. Active low logic input used in conjunction with CS to access the conversion result. The conversion result is placed on the data bus following the falling edge of RD read while CS is low. |
| ADC_RESET_O | OUT | 1 | Reset pin. When set to logic high, the rising edge of RESET resets the AD7606. |
| ADC_STDBY_O | OUT | 1 | Standby Mode pin. This pin is used to place the AD7606 into one of the two power-down modes: standby mode or shutdown mode. The power-down mode entered depends on the state of the RANGE pin. |
| ADC_CONVST_N_O | OUT | 1 | ADC conversion Start Input. A falling edge on CONVST is used to initiate a conversion. The track-and-hold goes from track mode to hold mode on the falling edge of CONVST and the conversion process is initiated at this point. Following power-down, when operating in auto-shutdown or auto-standby modes, a rising edge on CONVST is used to power up the device. |
| Table 4 Port description for the AD7606 module | |||
The next sections of this document present all the steps needed to create a fully functional project that can be used for evaluating the operation of the ADI platform. It is possible to skip these steps and load in the FPGA an image that contains a fully functional system that can be used for platform evalution. The first step of the quick evaluation process is to program the FPGA with the image provided in the lab files. Before the image can be loaded the Quartus II Web Edition tool or the Quartus II Programmer must be installed on your computer. To load the FPGA image you must first make sure that the USB cable is not connected to the CED1Z board. Connect the USB Blaster to the J6 connector of the CED1Z and power the board. Run the program_fpga.bat batch file located in the ADIEvalBoard/FPGA folder.
In order to acquire data, follow the instructions in the Evaluation Project Data Acquisition section.
This section presents the steps for developing a software application that will run on the CED1Z system and will be used for controlling and monitoring the operation of the ADI evaluation board.
Launch the Nios II SBT from the Start → All Programs → Altera → Nios II EDS 11.0 → Nios II 11.0 Software Build Tools for Eclipse (SBT).
NOTE: Windows 7 users will need to right-click and select Run as administrator. Another method is to right-click and select Properties and click on the Compatibility tab and select the Run This Program As An Administrator checkbox, which will make this a permanent change.
The tool will create two new software project directories. Each Nios II application has 2 project directories in the Eclipse workspace.
Since you chose the blank project template, there are no source files in the application project directory at this time. The BSP contains a directory of software drivers as well as a system.h header file, system initialization source code and other software infrastructure.
The software project provided in this lab does not make use of an operating system. All stdout, stdin and stderr messages will be directed to the jtag_uart.
The memory used by the design is should be changed from OnChip ram to SRAM for the .text region.
In addition to the board support package settings configured using the BSP Editor, there are other compilation settings managed by the Eclipse environment such as compiler flags and optimization level.
In Windows Explorer locate the project directory which contains a directory called Software. In Windows Explorer select all the files and directories from the Software folder and drag and drop them into the Eclipse software project ADIEvalBoard.
Just as you configured the optimization level for the BSP project, you should set the optimization level for the application software project ADIEvalBoard as well.
Application code can be conveniently organized in a directory structure. This section shows how to define these paths in the makefile.
These 2 steps will compile and build the associated board support package, then the actual application software project itself. The result of the compilation process will be an Executable and Linked Format (.elf) file for the application, the ADIEvalBoard.elf file.
In case an error appears at compile time with a description like : section .rodata loaded at [00400164,00400477] overlaps section .text loaded at [00400164,004054d7] the enable_alt_load_copy_exceptions option must be unchecked from BSP Editor → Main → Settings → Advanced→ hal.linker
The CED1Z hardware is designed with a System ID peripheral. This peripheral is assigned a unique value based on when the hardware design was last modified in the SOPC Builder tool. SOPC Builder also places this information in the .sopcinfo hardware description file. The BSP is built based on the information in the .sopcinfo file.
To run the software project on the Nios II processor:
The code size and start address might be different than the ones displayed in the above screenshot.
After the FPGA is correctly programmed the data acquisition process can start by executing the data_capture.bat script. The data_capture.tcl file can be modified to acquire a variable number of channels, to change the oversampling signals and the range signal. If the number of channels is larger than the number of channels available on the part, the additional channels will be taken from channel 1. (e.g for AD7606-4, channel 5 will have the same data as channel 1, channel 6 will have the same data as channel 2 etc).
The configuration from data_capture.tcl is performed the first time the script is executed. If changes are performed after that, the system must be reinitialized by reprogramming the FPGA.
If the resulting csv file is opened with Microsoft Excel, the data will be displayed on a different number of columns, each column corresponding to a channel.