world leader in high performance signal processing

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

resources:fpga:altera:bemicro:cn0203 [28 May 2012 16:15]
ACozma [Software Tools]
resources:fpga:altera:bemicro:cn0203 [15 Feb 2013 16:04] (current)
AdrianC Updated uC/Probe related links
Line 3: Line 3:
 ===== Supported Devices ===== ===== Supported Devices =====
  
-  * [[adi>AD5660-1]]+  * [[adi>AD5660|AD5660-1]]
   * [[adi>AD5750-1]]   * [[adi>AD5750-1]]
 +===== Reference Circuits =====
  
-===== Evaluation Boards ===== +  * [[adi>CN0203]]
- +
-  * [[adi>EVAL-CN0203-SDPZ ]] +
 ====== Overview ====== ====== Overview ======
  
-This lab presents the steps to setup an environment for using the **[[adi>EVAL-CN0203-SDPZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/page/products/tools/probe|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-CN0203-SDPZ Evaluation Board with the BeMicro SDK Platform.+This lab presents the steps to setup an environment for using the **[[adi>EVAL-CN0203-SDPZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-CN0203-SDPZ Evaluation Board with the BeMicro SDK Platform.
  
 {{ :resources:fpga:altera:bemicro:cn0203_bemicro.jpg?400 }} {{ :resources:fpga:altera:bemicro:cn0203_bemicro.jpg?400 }}
  
-For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to Analog Devices [[/resources/eval/sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: +{{page>common_sdp}}
-  * a controller board, like the **[[resources/eval/sdp/sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** +
-  * an compatible Analog Devices SDP [[adi>sdp#exallist|product evaluation board]] +
-  * corresponding PC software +
-The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software.  Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ.+
  
 Below is presented a picture of **SDP-B** Controller Board with the **EVAL-CN0203-SDPZ** Evaluation Board. Below is presented a picture of **SDP-B** Controller Board with the **EVAL-CN0203-SDPZ** Evaluation Board.
Line 55: Line 49:
   * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]]   * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]]
   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]
-  * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]]+  * [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]]
  
 ====== Getting Started ====== ====== Getting Started ======
Line 76: Line 70:
   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0
   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0
-  * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool+  * [[http://micrium.com/tools/ucprobe/trial/|uC-Probe]] run-time monitoring tool, version 2.5
  
 The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web.  The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. 
  
-The **Micrium uC/Probe Trial** version is available via download from the web at [[http://micrium.com/download/Micrium-uC-Probe-Setup-Trial.exe]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list.+The **Micrium uC/Probe Trial** version 2.5 is available via download from the web at [[http://micrium.com/tools/ucprobe/trial/]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list.
  
 ===== Downloads ===== ===== Downloads =====
Line 168: Line 162:
  
 {{page>troubleshooting}} {{page>troubleshooting}}
-