Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Last revisionBoth sides next revision
resources:fpga:altera:bemicro:ad7657-1 [15 Oct 2012 17:04] – created Adrian Costinaresources:fpga:altera:bemicro:ad7657-1 [03 Jan 2013 20:42] – external edit
Line 175: Line 175:
 After the FPGA is correctly programmed the data acquisition process can start by executing the data_capture.bat script. The data_capture.tcl file can be modified to acquire a variable number of channels. After the FPGA is correctly programmed the data acquisition process can start by executing the data_capture.bat script. The data_capture.tcl file can be modified to acquire a variable number of channels.
  
-<note>The configuration from data_capture.tcl is performed the first time the script is executed. If changes are performed after that, the system must be reinitialized by reprogramming the FPGA.</note>+<WRAP round help>The configuration from data_capture.tcl is performed the first time the script is executed. If changes are performed after that, the system must be reinitialized by reprogramming the FPGA.</WRAP>
  
 {{ :resources:fpga:altera:bemicro:cmd_interface.png?500 |Demonstration Project Command Interface}} {{ :resources:fpga:altera:bemicro:cmd_interface.png?500 |Demonstration Project Command Interface}}
resources/fpga/altera/bemicro/ad7657-1.txt · Last modified: 26 Jan 2021 01:22 by Robin Getz