This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:altera:bemicro:ad7176_2 [10 Dec 2012 15:36] – Under Construction Alexandru.Tofan | resources:fpga:altera:bemicro:ad7176_2 [26 Jan 2021 01:21] (current) – update arrow links after their web site update Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ~~UNDERCONSTRUCTION~~under construction | ||
- | |||
====== BeMicro FPGA Project for AD7176-2 with Nios driver ====== | ====== BeMicro FPGA Project for AD7176-2 with Nios driver ====== | ||
Line 13: | Line 11: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This lab presents the steps to setup an environment for using the **[[adi> | + | This lab presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 30: | Line 28: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | * [[http://www.arrownac.com/solutions/ | + | * [[https://www.intel.com/content/ |
* [[http:// | * [[http:// | ||
Line 41: | Line 39: | ||
Below is presented the list of required hardware items: | Below is presented the list of required hardware items: | ||
- | * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board | + | * Arrow Electronics [[https://www.intel.com/content/www/ |
- | * [[http:// | + | * [[adi> |
* **EVAL-AD7176-2SDZ** evaluation board | * **EVAL-AD7176-2SDZ** evaluation board | ||
* Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | ||
Line 57: | Line 55: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{{{: | + | * {{{{: |
===== Extract the Lab Files ===== | ===== Extract the Lab Files ===== | ||
Line 110: | Line 108: | ||
After the FPGA is correctly programmed the data acquisition process can start by executing the data_capture.bat script. The data_capture.tcl file can be modified to acquire a variable number of channels. | After the FPGA is correctly programmed the data acquisition process can start by executing the data_capture.bat script. The data_capture.tcl file can be modified to acquire a variable number of channels. | ||
- | <note>The configuration from data_capture.tcl is performed the first time the script is executed. If changes are performed after that, the system must be reinitialized by reprogramming the FPGA.</note> | + | <WRAP round help>The configuration from data_capture.tcl is performed the first time the script is executed. If changes are performed after that, the system must be reinitialized by reprogramming the FPGA.</WRAP> |
{{ : | {{ : |