This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:altera:bemicro:ad7091r [04 Sep 2012 13:13] – Updated reference to SDP system Adrian Costina | resources:fpga:altera:bemicro:ad7091r [26 Jan 2021 01:21] (current) – update arrow links after their web site update Robin Getz | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
- | * [[adi> | + | * [[adi> |
====== Overview ====== | ====== Overview ====== | ||
- | This lab presents the steps to setup an environment for using the **[[adi> | + | This lab presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, | + | {{page> |
- | *1. A controller board like the SDP-B ( EVAL-SDP-CS1Z) | + | |
- | *2. The component SDP compatible product evaluation board | + | |
- | *3. Corresponding PC software ( shipped with the product evaluation board) | + | |
- | The SDP-B controller board is part of Analog Devices System Demonstration Platform (SDP). It provides a high speed USB 2.0 connection from the PC to the component evaluation board. The PC runs the evaluation software. Each evaluation board, which is an SDP compatible daughter board, includes the necessary installation file required for performance testing. | + | |
- | + | ||
- | // | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7091RSDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD7091RSDZ** Evaluation Board. | ||
Line 27: | Line 21: | ||
{{ : | {{ : | ||
- | The **EVAL-AD7091SDZ** evaluation board is a member of a growing number of boards available for the **SDP**. | + | The **EVAL-AD7091SDZ** evaluation board is a member of a growing number of boards available for the **SDP**. |
The [[adi> | The [[adi> | ||
Line 33: | Line 27: | ||
===== More information ===== | ===== More information ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * **EVAL-AD7091RSDZ** evaluation board user guide (Available on CD) |
- | * [[http://www.arrownac.com/solutions/ | + | * [[https://www.intel.com/content/ |
* [[http:// | * [[http:// | ||
Line 44: | Line 38: | ||
Below is presented the list of required hardware items: | Below is presented the list of required hardware items: | ||
- | * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board | + | * Arrow Electronics [[https://www.intel.com/content/www/ |
- | * [[http:// | + | * [[adi> |
* **EVAL-AD7091RSDZ** evaluation board | * **EVAL-AD7091RSDZ** evaluation board | ||
* Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | ||
Line 52: | Line 46: | ||
Below is presented the list of required software tools: | Below is presented the list of required software tools: | ||
- | * [[http:// | + | * [[http:// |
- | * [[https:// | + | * [[https:// |
The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. | The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. |