Wiki

This version (01 Dec 2017 21:25) was approved by Mark Looney.The Previously approved version (01 Dec 2017 20:55) is available.Diff

ADIS1644X/FLEX FLEXIBLE CONNECTOR WIKIGUIDE

GENERAL DESCRIPTION

The ADIS1644X/FLEX is a flexible connector that helps connect the ADIS16334, ADIS16445 and ADIS16448 IMUs to the EVAL-ADIS (J4) evaluation system. It also connects these same IMUs to the ADIS16IMU2/PCBZ or ADIS16IMU1/PCBZ breakout boards

SUMMARY

When used in conjunction with the ADIS16IMU2/PCBZ, the ADIS1644X/FLEX can connect the ADIS16334, ADIS16445 or ADIS16448 to the EVAL-ADIS or to an embedded processor system. Please see the following picture, which illustrates how each of these components fit together:

SETUP WITH ADIS1633X/44X IMUS

Connecting the IMU (ADIS16334, ADIS16445 or ADIS16448), ADIS1644X/FLEX and ADIS16IMU2 together is a very simple two-step process. Please note that the pin numbers markings on the ADIS1644X/FLEX were incorrect in early manufacturing lots. Please ignore the pin number markings on the ADIS1644X/FLEX and use the following instructions to guide the connection process.

Step 1: ADIS16xxx (IMU) to ADIS1644X/FLEX

The following diagram illustrates the two different connectors on ADIS1644X/FLEX, along with their connections:

The following diagram shows the IMU's interface connector, which the ADIS1644X/FLEX connects with:

The following table shows the correct insertion, along with the three most common incorrect ways to insert the flex onto the IMU's interface connector

TOP VIEW CONNECTOR VIEW

Step 2: ADIS1644X/FLEX to ADIS16IMU2/PCBZ

The ADIS1644X/FLEX has 20 pins, while J2 on the ADIS16IMU2/PCBZ has 24-pins. Connect the flex to pins 1 through 20 on J2. Pin numbers 1, 2, 23 and 24 are clearly identified on the silk screen, which is associated with J2 on the ADIS16IMU2/PCBZ. The following pictures illustrate the correct insertion alignment for this connection

Here is an example of what this will look like, after finishing these steps:

28 Mar 2015 01:55 · Mark Looney
resources/eval/user-guides/inertial-mems/imu/adis1644xflex.txt · Last modified: 01 Dec 2017 21:25 by Mark Looney