Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis16334-adisusb [18 Sep 2012 22:46] – [USB Driver Installation] Scott Hutchens | resources:eval:user-guides:inertial-mems:imu:adis16334-adisusb [09 Jan 2021 00:39] (current) – user interwiki links Robin Getz |
---|
====== ADIS16334 EVALUATION ON THE ADISUSB===== | ====== ADIS16334 EVALUATION ON THE ADISUSB===== |
===== OVERVIEW ===== | ===== OVERVIEW ===== |
| The [[adi>ADIS16334|ADIS16334]] is a low-profile, high-performance IMU that uses a serial peripheral interface for data communications. This interface enables direct connection with a large variety of embedded processor products. This electrical connection typically only requires 5 I/O lines for synchronous data collection, as shown in the following figure: |
''The [[adi>ADIS16334|ADIS16334]] is a low-profile, high-performance IMU that uses a serial peripheral interface for data communications. This interface enables direct connection with a large variety of embedded processor products. This electrical connection typically only requires 5 I/O lines for synchronous data collection, as show in the following figure:'' | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16334-uc-hook-up.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16334-uc-hook-up.png?400|}} |
| |
===== ADIS16334/PCB BREAKOUT BOARD ===== | ===== ADIS16334/PCB BREAKOUT BOARD ===== |
''For those who are on a tight timeline, connecting the [[adi>ADIS16334|ADIS16334]] to an embedded controller will provide the most flexibility in developing application firmware and will more closely reflect the final system design. The [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCBZ]] is the breakout board for the [[adi>ADIS16334|ADIS16334]] and may provide assistance in the process of hooking it up to an existing embedded processor system. For more information on the [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCBZ]] breakout boards, check out the following link: [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCB Breakout Board Web Page]].'' | For those who are on a tight timeline, connecting the [[adi>ADIS16334|ADIS16334]] to an embedded controller will provide the most flexibility in developing application firmware and will more closely reflect the final system design. The [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCBZ]] is the breakout board for the [[adi>ADIS16334|ADIS16334]] and may provide assistance in the process of hooking it up to an existing embedded processor system. |
===== ADISUSB: PC EVALUATION ===== | ===== ADISUSB: PC EVALUATION ===== |
| |
''For those who would prefer to perform PC-based evaluation of the [[adi>ADIS16334|ADIS16334]], before developing their own embedded system, the [[adi>ADISUSB|ADISUSB]] is the appropriate system to use. The remainder of this Wiki site will focus on PC-based evaluation with the [[adi>ADISUSB|ADISUSB]] system.'' | For those who would prefer to perform PC-based evaluation of the [[adi>ADIS16334|ADIS16334]], before developing their own embedded system, the [[adi>ADISUSB|ADISUSB]] is the appropriate system to use. The remainder of this Wiki site will focus on PC-based evaluation with the [[adi>ADISUSB|ADISUSB]] system. |
===== EQUIPMENT LIST ===== | ===== EQUIPMENT LIST ===== |
''[[adi>ADISUSB|ADISUSB]]'' | [[adi>ADISUSB|ADISUSB]] |
| |
''[[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCBZ]]'' | [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCBZ]] |
| |
===== SYSTEM REQUIREMENTS ===== | ===== SYSTEM REQUIREMENTS ===== |
''Windows XP, Vista, 7'' | Windows XP, Vista, 7 (32-bit systems only) |
| |
''.NET Framework 3.5'' | |
| |
''NOTE: Newer versions of the .NET framework do not currently support the IMU Evaluation software package.'' | |
| |
| NOTE: All the required files are contained in the .Cab file and deployed during software package install. |
===== PHYSICAL SETUP ===== | ===== PHYSICAL SETUP ===== |
''The [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCBZ]] includes one interface PCB, one flexible cable/connector and one [[adi>ADIS16334|ADIS16334AMLZ]] unit. Use the flexible cable/connector to install the [[adi>ADIS16334|ADIS16334]] onto the [[adi>ADISUSB|ADISUSB]], using the following five steps. Set interface PCB aside, as it is not used for connecting the [[adi>ADIS16334|ADIS16334AMLZ]] to the [[adi>ADISUSB|ADISUSB]].'' | The [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16334/products/EVAL-ADIS16334/eb.html|ADIS16334/PCBZ]] includes one interface PCB, one flexible cable/connector and one [[adi>ADIS16334|ADIS16334AMLZ]] unit. Use the flexible cable/connector to install the [[adi>ADIS16334|ADIS16334]] onto the [[adi>ADISUSB|ADISUSB]], using the following five steps. Set interface PCB aside, as it is not used for connecting the [[adi>ADIS16334|ADIS16334AMLZ]] to the [[adi>ADISUSB|ADISUSB]]. |
| |
''NOTE: Do not plug the [[adi>ADISUSB|ADISUSB]] into the USB cable at this stage of the setup. Wait until the software installation is complete.'' | **NOTE:** Do not plug the [[adi>ADISUSB|ADISUSB]] into the USB cable at this stage of the setup. Wait until the software installation is complete. |
| |
''NOTE: Some of the pictures in this section represent the [[adi>ADIS16448|ADIS16448]], not the [[adi>ADIS16334|ADIS16334]]. The packages associated with these two products are close enough to illustrate the key points associated with installing the [[adi>ADIS16334|ADIS16334]]. '' | **NOTE:** Some of the pictures in this section represent the [[adi>ADIS16448|ADIS16448]], not the [[adi>ADIS16334|ADIS16334]]. The packages associated with these two products are close enough to illustrate the key points associated with installing the [[adi>ADIS16334|ADIS16334]]. |
| |
=== Step #1 === | === Step #1 === |
''Install the flexible cable onto the [[adi>ADIS16334|ADIS16334AMLZ]]. The following pictures provide a visual reference for correct connection. '' | Install the flexible cable onto the [[adi>ADIS16334|ADIS16334AMLZ]]. The following pictures provide a visual reference for correct connection. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:448-eval-adis-step1-01.jpg?nolink&200|}} | {{:resources:eval:user-guides:inertial-mems:imu:448-eval-adis-step1-01.jpg?nolink&200|}} |
{{:resources:eval:user-guides:inertial-mems:imu:448-eval-adis-step1-02.jpg?nolink&400|}} | {{:resources:eval:user-guides:inertial-mems:imu:448-eval-adis-step1-02.jpg?nolink&400|}} |
| |
''WARNING: Make sure that the connector is in proper alignment before pressing it in. Misalignment can cause pin damage and exposure to harmful conditions. The following pictures provide visual examples of INCORRECT PIN ALIGNMENT. The most common alignment issues will cause the top view to look different than the third picture, shown directly above this paragraph.'' | **WARNING:** Make sure that the connector is in proper alignment before pressing it in. Misalignment can cause pin damage and exposure to harmful conditions. The following pictures provide visual examples of INCORRECT PIN ALIGNMENT. The most common alignment issues will cause the top view to look different than the third picture, shown directly above this paragraph. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:448-eval-adis-step1-04.jpg?nolink&200|}} | {{:resources:eval:user-guides:inertial-mems:imu:448-eval-adis-step1-04.jpg?nolink&200|}} |
| |
=== Step #2 === | === Step #2 === |
''Mounting to the system frame is accomplished by Drilling and tapping for M2 (drill size #52 1.6mm) or 2-56 (drill size #50 .070) holes in the [[adi>ADISUSB|ADISUSB]], according to the locations in the physical mounting diagram. The tap is the best way but an M2x0.4x10mm machine screw can be used for tapping the PCB material. The distance between these components is flexible but make sure that the hole-to-hole distance is within the 15 mm to 45 mm range shown in the diagram. The mounting location holes are marked as an example in the picture below (right). These locate holes position the [[adi>ADIS16334|ADIS16334AMLZ]] at the edge of the [[adi>ADISUSB|ADISUSB]] giving the interface flex more room.'' | Mounting to the system frame is accomplished by Drilling and tapping for M2 (drill size #52 1.6mm) or 2-56 (drill size #50 .070) holes in the [[adi>ADISUSB|ADISUSB]], according to the locations in the physical mounting diagram. The tap is the best way but an M2x0.4x10mm machine screw can be used for tapping the PCB material. The distance between these components is flexible but make sure that the hole-to-hole distance is within the 15 mm to 45 mm range shown in the diagram. The mounting location holes are marked as an example in the picture below (right). These locate holes position the [[adi>ADIS16334|ADIS16334AMLZ]] at the edge of the [[adi>ADISUSB|ADISUSB]] giving the interface flex more room. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-parts.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-parts.png?400 |}} |
| |
=== Step #3 === | === Step #3 === |
''The [[adi>ADIS16334|ADIS16334AMLZ]] and interface flex can now be connected to the [[adi>ADISUSB|ADISUSB]]. Make sure that Pin 1 on J2 (interface-flex) connects to Pin 20 on the [[adi>ADISUSB|ADISUSB]] J4 connector which, has 24 pins (leaving 4 empty holes at the top of the J4 connector opposite the J4 pin1 ★ designator). J4 has a Pin 1 indicator to help guide this connection. Making the J4 connection first then sliding the [[adi>ADIS16334|ADIS16334AMLZ]] body forward allowing the flex ribbon to fold under until the mounting holes line up.'' | The [[adi>ADIS16334|ADIS16334AMLZ]] and interface flex can now be connected to the [[adi>ADISUSB|ADISUSB]]. Make sure that Pin 1 on J2 (interface-flex) connects to Pin 20 on the [[adi>ADISUSB|ADISUSB]] J4 connector which, has 24 pins (leaving 4 empty holes at the top of the J4 connector opposite the J4 pin1 ★ designator). J4 has a Pin 1 indicator to help guide this connection. Making the J4 connection first then sliding the [[adi>ADIS16334|ADIS16334AMLZ]] body forward allowing the flex ribbon to fold under until the mounting holes line up. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-334-j4-connection.png?300 |}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-334-j4-connection.png?300 |}} |
| |
=== Step #4 === | === Step #4 === |
''Secure the [[adi>ADIS16334|ADIS16334AMLZ]] body, to a system frame using (4) M2x0.4x10mm machine screws (included with [[adi>ADISUSB|ADISUSB]]). Use a mounting torque of 25 inch-ounces for the M2 machine screws.'' | Secure the [[adi>ADIS16334|ADIS16334AMLZ]] body, to a system frame using (4) M2x0.4x10mm machine screws (included with [[adi>ADISUSB|ADISUSB]]). Use a mounting torque of 25 inch-ounces for the M2 machine screws. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-334-secured.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-334-secured.png?400 |}} |
| |
=== Step #5 === | === Step #5 === |
''The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). Change the JP1 jumper setting on the [[adi>ADISUSB|ADISUSB]]) to the **+5V** position (shown on the right) required for the [[adi>ADIS16334|ADIS16334AMLZ]].'' | The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). Change the JP1 jumper setting on the [[adi>ADISUSB|ADISUSB]]) to the **+5V** position (shown on the right) required for the [[adi>ADIS16334|ADIS16334AMLZ]]. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-3.3v-setting.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-3.3v-setting.png?400 |}} |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-5v-markedsetting.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-5v-markedsetting.png?400|}} |
| |
| **NOTE:** If JP1 is left on **+3.3V**, the gyroscope outputs will not respond and will appear to be saturated in one direction or the other. See the following picture for an example of this behavior. |
| |
''NOTE: If JP1 is left on **+3.3V**, the gyroscope outputs will not respond and will appear to be saturated in one direction or the other. See the following picture for an example of this behavior.'' | {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-error.png?800|}} |
| |
{{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-error.png?800 |}} | |
| |
| |
| |
| |
| |
| |
| |
| |
| |
===== IMU_6DOF Six Degrees of Freedom Demonstration SOFTWARE ===== | ===== IMU_6DOF Six Degrees of Freedom Demonstration SOFTWARE ===== |
'' [[adi>static/imported-files/eval_boards/IMU_6DOF_2.zip|Click here to download the IMU-6DOF Six Degrees of Freedom Software]] to a personal computer, which enables PC-based evaluation of the [[adi>ADIS16334|ADIS16334]] on an [[adi>ADISUSB|ADISUSB]] evaluation system. The download file will contain three separate files: The CAB file (IMU_6DOF.cab), the setup file (setup.exe) and the setup list. Copy these files to a convenient folder for running the application from.'' | [[adi>static/imported-files/eval_boards/IMU_6DOF_2.zip|Click here to download the IMU-6DOF Six Degrees of Freedom Software]] to a personal computer, which enables PC-based evaluation of the [[adi>ADIS16334|ADIS16334]] on an [[adi>ADISUSB|ADISUSB]] evaluation system. The download file will contain three separate files: The CAB file (IMU_6DOF.cab), the setup file (setup.exe) and the setup list. Copy these files to a convenient folder for running the application from. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-software-zip.png?500 |}} | |
| |
| |
| |
| |
| |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-software-zip.png?800|}} |
| |
| Navigate to the folder where the files were saved and double click the setup.exe file. The following pictures are a guide for the IMU_6DOF software install. The **Welcome** screen will appear click **OK** to continue. |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-v2welcome.png?600|}} |
| |
| Please choose a directory for the software application or use the default settings (recommended) and click the computer icon button to go to the next step. |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-v2install.png?600|}} |
| |
| Choose a program group or use the default settings (recommended) and click **Continue**. The last picture confirms completion click **OK** to finish. |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-v2programgroup.png?400|}} |
| {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-v2completed-install.png?400|}} |
| |
====USB Driver Installation==== | ====USB Driver Installation==== |
''The MCPDrivers.exe file contains USB drivers that are compatible with both 32-bit and 64-bit Windows systems. Double-click on the SDPDrivers.exe file and follow the prompts to install the USB driver files onto the PC. When the following window appears, click on **Next** and then click on **Continue Anyway** to continue with the installation.'' | The IMU_6DOF.cab file contains USB drivers that are compatible with both only 32-bit Windows systems. The drivers are unpacked the same time the software application is loaded by double clicking the setup.exe file. The first time the [[adi>ADISUSB|ADISUSB]] board is plugged into the computer (using the included USB mini cable) the hardware is recognized and loaded. The computer **Hardware Wizard** will find and install the drivers by following the steps below. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-foundnewhardware.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-foundnewhardware.png?400 |}} |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-hardware-install.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-hardware-install.png?400|}} |
| |
''The following pictures show the final steps for USB driver install. Click on **Next** then click **Finish** to complete the installation.'' | The following pictures show the final steps for USB driver install. Click on **Next** then click on **Finish** completing the installation. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-hardware-wizard.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-hardware-wizard.png?400 |}} |
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}} |
| |
| |
| |
| |
| <wrap alert> **WARNING:** For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. Please see page 8, on the **[[adi>static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps. </wrap> |
===== IMU_6DOF Six Degree of Freedom Demonstration SOFTWARE ===== | ===== IMU_6DOF Six Degree of Freedom Demonstration SOFTWARE ===== |
''After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the IMU_6DOF.exe file to launch the software application.'' | After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the IMU_6DOF.exe file to launch the software application. |
==== Main Window ==== | ==== Main Window ==== |
''Once the IMU_6DOF Six Degrees of Freedom Demonstration Software starts-up, the Main Window will appear and look like the following picture. The second picture provides color-coded boxes to support further discussion of each function in this screen.'' | Once the IMU_6DOF Six Degrees of Freedom Demonstration Software starts-up, the Main Window will appear and look like the following picture (which has highlights to support additional descriptions, see below the graphic). |
| |
{{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-v2main.jpg?800|}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-334-main-defined.png?800|}} |
{{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-v2main-functions.jpg?800|}} | |
| |
''The orange box identifies the drop-down menus, which provide a number of useful features. The **Devices** option provides a list of products. For [[adi>ADIS16334|ADIS16334]] Evaluation, click on **Devices** and then select **ADIS16334**. The green box shows the current device selection, which in this case, identifies the [[adi>ADIS16334|ADIS16334]] as the current selection.'' | The orange box identifies the drop-down menus, which provide a number of useful features. The **Devices** option provides a list of products for [[adi>ADIS16334|ADIS16334]] Evaluation, click on **Devices** and then select **[[adi>ADIS16334|ADIS16334]]**. The green box shows the current device selection, which in this case, identifies the [[adi>ADIS16334|ADIS16334]] as the current selection. |
| |
''The **Register Access** option provides a listing of user-configurable registers in the [[adi>ADIS16334|ADIS16334]] and also provides read/write access to each one of these registers.'' | The **Registers** option provides a listing of user-configurable registers in the [[adi>ADIS16334|ADIS16334]] and also provides read/write access to each one of these registers. |
| |
''The **Data Capture** option provides the core data collection function.'' | The **Datalog** option provides the core data collection function. |
| |
''The **Demos** option does not support the [[adi>ADIS16334|ADIS16334]].'' | The purple box identifies the output registers, which update, real-time, after pressing the **Read** button (see the red box for the location of the **Read** button). |
| |
''The **Tools** option provides some diagnostic tools for the USB interface.'' | |
| |
''The **About** option provides more detail software revision information.'' | |
| |
''The purple box identifies the output registers, which update, real-time, after pressing the **Read** button (see the red box for the location of the **Read** button).'' | |
| |
''The yellow box identifies the three waveform recorder windows. The top window contains the three gyroscope outputs. The bottom window contains the three accelerometer responses. Also, each waveform matches the color of its register (see register titles in the purple box).'' | |
| |
| The yellow box identifies the two waveform recorder windows. The top window contains the three gyroscope outputs. The bottom window contains the three accelerometer responses. Also, each waveform matches the color of its register (see register titles in the purple box). |
==== Register Access ==== | ==== Register Access ==== |
''The purpose of the **Register Access** window is to provide both read and write access to the user registers in the [[adi>ADIS16334|ADIS16334]]. The following picture shows the appearance of this window.'' | The purpose of the **Register Access** window is to provide both read and write access to the user registers in the [[adi>ADIS16334|ADIS16334]]. The following picture shows the appearance of this window. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-registers.jpg?600|}} | |
| |
''The color coded boxes illustrate the different functions that this window provides.'' | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-reg-defined.jpg?600|}} | |
| |
''The purple box identifies the register category. In addition to the Control/Status, this drop-down control offers access to **Output** and **Calibration** registers.'' | |
| |
''The red box identifies all of the registers that are in the current category. Click on the register name to select a register for individual read/write access.'' | |
| |
''The green box identifies the read/write control options for the current register selection. Use the hexadecimal format when writing commands to a particular register.'' | |
| |
''The **Update Registers in Category** button (orange box) triggers a read and display update of all registers in the current category (red box).'' | {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-334-reg.png?600|}} |
| |
''The yellow box identifies the area that provides single-bit command buttons, such as the ones provided by the GLOB_CMD register.'' | The color coded boxes illustrate the different functions that this window provides. |
| |
''The **Save Reg Settings to File** command saves all of the registers in the current category into a *.csv (common-delimited) file. The **Load Reg Settings from File** button reads the settings back into the software package and triggers a routine that updates all registers with the values from this file.'' | {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-334-reg-defined.png?600|}} |
| |
''APPLICATION TIP: The **Register Access** screen writes to user control registers, inside of the [[adi>ADIS16334|ADIS16334]], two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the **Write Register** button. When using an embedded processor to write to user control registers, inside of the [[adi>ADIS16334|ADIS16334]], each command (16-bits) writes to one byte at a time.'' | The purple box identifies the register category. In addition to the Control/Status, this drop-down control offers access to **Output** and **Calibration** registers. |
| |
| The red box identifies all of the registers that are in the current category. Click on the register name to select a register for individual read/write access. |
| |
| The green box identifies the read/write control options for the current register selection. Use the hexadecimal format when writing commands to a particular register. |
| |
| The yellow box updates all the registers in the current category. |
| |
| The **Update Flash** command saves writable user register data. |
| |
| APPLICATION TIP: The **Register Access** screen writes to user control registers, inside of the [[adi>ADIS16334|ADIS16334]], two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the **Write Register** button. When using an embedded processor to write to user control registers, inside of the [[adi>ADIS16334|ADIS16334]], each command (16-bits) writes to one byte at a time. |
| |
==== Data Capture Menu ==== | ==== Data Capture Menu ==== |
''The Data Capture function supports synchronous data acquisition, based on the data-ready signal from the [[adi>ADIS16334|ADIS16334]]. The following picture represents the Data Capture window, right after opening it from the **Main Window** and the second picture provides color-coded boxes, in order to support further discussion of each function that is associated with this screen.'' | ''The Data Capture function supports synchronous data acquisition, based on the data-ready signal from the [[adi>ADIS16334|ADIS16334]]. The following picture represents the Data Capture window, right after opening it from the **Main Window** and the second picture provides color-coded boxes, in order to support further discussion of each function that is associated with this screen.'' |
| |
{{:resources:eval:user-guides:inertial-mems:imu:334-imu-6dofdatacapture.jpg?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-334-datalog.png?400 |}} |
{{ :resources:eval:user-guides:inertial-mems:imu:334-imu-6dof-datacap-defined.jpg?400 |}} | {{:resources:eval:user-guides:inertial-mems:imu:imu_6dof-334-datalog-defined.png?400|}} |
| |
''The red box identifies all of the registers that are eligible for inclusion in the next acquisition process. Click on each box to include a register in the next data acquisition sequence. The box will have a check mark when it has been selected. '' | ''The red box identifies all of the registers that are eligible for inclusion in the next acquisition process. Click on each box to include a register in the next data acquisition sequence. The box will have a check mark when it has been selected. '' |
''The green box identifies the configuration box for the name and location of the data storage file.'' | ''The green box identifies the configuration box for the name and location of the data storage file.'' |
| |
''The yellow boxes identify a number of configuration options for the data acquisition process. The **Samples per File** is a user input for the total number of samples in a data record. Note that all selected registers will have this number of samples in the data record file, after the acquisition process completes. After each update to the **Record Length** box, the software calculates the displays the total **Capture Time**. The **Add Header** option allows the user to add or remove the header in the data storage file. The **Use Scaled Data** causes the software to convert the decimal, twos complement number into its representative value. For example, when enabling **Use Scaled Data,** the gyroscope outputs will be in units of degrees/second.'' | ''The yellow boxes identify a number of configuration options for the data acquisition process. The **Samples per File** is a user input for the total number of samples in a data record. Note that all selected registers will have this number of samples in the data record file, after the acquisition process completes. After each update to the **Record Length** box, the software calculates then displays the total **Capture Time**. The **Numeric Data Only..No File Header** option allows the user to add or remove the header in the data storage file. The **No Scale LSB's Only** causes the software to convert the decimal, twos complement number into its representative value. For example, when enabling **No Scale LSB's Only,** the gyroscope outputs will be in units of degrees/second.'' |
| |
==== EXAMPLE EXERCISES ==== | ==== EXAMPLE EXERCISES ==== |
''This section currently has no [[adi>ADIS16334|ADIS16334]]-specific content, but the | ''This section currently has no [[adi>ADIS16334|ADIS16334]]-specific content, but the |
[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with.'' | [[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with.'' |
| |