This version (17 Sep 2012 16:18) was approved by NevadaMark.The Previously approved version (01 Sep 2012 22:16) is available.
This is an old revision of the document!
The ADIS16305 is a low-profile, high-peformance IMU that uses a serial peripheral interface for data communications. This interface enables direct connection with a large variety of embedded processor products. This electrical connection typically only requires 5 I/O lines for sychronous data collection, as show in the following figure:
The ADIS16300 offers the same function, package, and interface as the ADIS16305, but it only calibrated at +25C. While the majority of the discussion in this Wiki will refer to the ADIS16305 specifically, all of this information also applies to the ADIS16300.
For those who are on a tight timeline, connecting the ADIS16305 to an embedded controller will provide the most flexibility in developing application firmware and will more closely reflect the final system design. The ADIS16305/PCBZ is the breakout board for the ADIS16305 and may provide assistance in the process of hooking it up to an existing embedded processor system. For more information on the ADIS16305/PCBZ breakout boards, check out the following links:
For those who would prefer to perform PC-based evaluation of the ADIS16305, before developing their own embedded system, the EVAL-ADIS is the appropriate system to use. The remainder of this Wiki site will focus on PC-based evaluation with the EVAL-ADIS system.
Windows XP, Vista, 7
.NET Framework 3.5
NOTE: Newer versions of the .NET framework do not currnently support the IMU Evaluation software pacakge.
The ADIS16305/PCBZ includes one interface PCB, one flexible cable/connector and one ADIS16305BMLZ unit. Use the flexible cable/connector to install the ADIS16305 onto the EVAL-ADIS, using the following five steps. Set interface PCB aside, as it is not used for connecting the ADIS16305BMLZ to the EVAL-ADIS.
NOTE: Do not plug the EVAL-ADIS into the USB cable at this stage of the setup. Wait until the software installation is complete.
NOTE: Most of the pictures in this section represent the ADIS16448, not the ADIS16305. The packages associated with these two products are close enough to illustrate the key points associated with installing the ADIS16305BMLZ on the EVAL-ADIS. The key differences to keep in mind when using these instrucitons are:
1. The ADIS16305BMLZ as two mounting holes (instead of two)
2. The ADIS16305BMLZ uses the B holes on the EVAL-ADIS for attachment.
Install the flexible cable onto the ADIS16305AMLZ. The following pictures provide a visual refernece for correct connection.
WARNING: Make sure that the connector is in proper alignment before pressing it in. Misalignment can cause pin damage and exposure to harmful conditions. The following pictures provide visual examples of INCORRECT PIN ALIGNMENT. The most common alignment issues will cause the top view to look different than the third picture, shown directly above this paragraph.
Connect the other end of the flexible cable to the EVAL-ADIS, using J4, pins 1-20. J4 has 24 pins, so make sure that the flexible cable connects only to pins 1-20 on J4.
Slide the ADIS16305BMLZ body towards J4, while tucking the excess flexing under the connector interface, as show in the following pictures.
Secure the ADIS16305BMLZ body, using (4) M2x0.4x10mm machine screws (included with EVAL-ADIS) and the “D” mounting holes (EVAL-ADIS labels for mounting holes).
Set JP1 (EVAL-ADIS) to +5V. The following picture shows JP1 in the +3.3V position
NOTE: If JP1 is left on +3.3V, the gyroscope outputs will not respond and will appear to be saturated in one direction or the other. See the following picture for an example of this behavior.
Click here to download the IMU Evaluation software to a personal computer, which enables PC-based evaluation of the ADIS16305 on an EVAL-ADIS evaluation system. The download file will contain three separate files: The USB driver (SDPDrivers.exe), the application file (IMUEvaluation.exe) and the revision table. Copy these files to a convenient folder for running the application from.
The SDPDrivers.exe file contains USB drivers that are compatible with both 32-bit and 64-bit Windows systems. Double-click on the SDPDrivers.exe file and follow the prompts to install the USB driver files onto the PC. When the following window appears, click on Next and then click on Install to continue with the installation.
The following pictures show the progress bar and the final confirmation window. Click on Finish to complete the installation.
After the USB driver installation is complete, connect the EVAL-ADIS USB connector to the PC, using the USB Mini cable, from the EVAL-ADIS kit. LED2 will illuminate as soon as this connection is made. This indicates that the EVAL-ADIS has power and is going through its start-up/initialization process. After the EVAL-ADIS completes its this process, LED1 will illuminate, indicating that it is time to launch the IMU Evaluation application. During the initialization process, several messages may appear on the screen. They are related to updating the EVAL-ADIS firmware and establishing communication between the PC and the EVAL-ADIS. Once LED1 lights up, double click on the IMU_Evaluation.exe file to launch the application.
Once the IMU Evaluation software starts-up, the Main Window will appear and look like the following picture. The second picture provides color-coded boxes to support further discussion of each function in this screen.
The orange box identifies the drop-down menus, which provide a number of useful features. The Devices option provides a list of products. For ADIS16305 Evaluation, click on Devices and then select ADIS16305. The green box shows the current device selection, which in this case, identifies the ADIS16305 as the current selection.
The Register Access option provides a listing of user-configurable registers in the ADIS16305 and also provides read/write access to each one of these registers.
The Data Capture option provides the core data collection function.
The Demos option does not support the ADIS16305.
The Tools option provides some diagnostic tools for the USB interface.
The About option provides more detail software revision information.
The purple box identifies the output registers, which update, real-time, after pressing the Read button (see the red box for the location of the Read button).
The yellow box identifies the three waveform recorder windows. The top window contains the three gyroscope outputs. The middle window contains the three accelerometer responses. The bottom window contains the three magnetometer responses. Also, each waveform matches the color of its register (see register titles in the purple box).
The purpose of the Register Access window is to provide both read and write access to the user registers in the ADIS16305. The following picture shows the appearance of this window.
The color coded boxes illustrate the different functions that this window provides.
The purple box identifies the register category. In addition to the Control/Status, this drop-down control offers access to Output and Calibration registers.
The red box identifies all of the registers that are in the current category. Click on the register name to select a register for individual read/write access.
The green box identifies the read/write control options for the current register selection. Use the hexadecimal format when writing commands to a particular register.
The Update Registers in Category button (orange box) triggers a read and display update of all registers in the current category (red box).
The yellow box identifies the area that provides single-bit command buttons, such as the ones provided by the GLOB_CMD register.
The Save Reg Settings to File command saves all of the registers in the current category into a *.csv (common-delimited) file. The Load Reg Settings from File button reads those settings back into the software package and triggers a routine that updates all registers with the values from this file.
APPLICATION TIP: The Register Acess screen writes to user control registers, inside of the ADIS16305, two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the Write Register button. When using an embedded processor to write to user control registers, inside of the ADIS16305, each command (16-bits) writes to one byte at a time.
The Data Capture function supports synchronous data acquisition, based on the data-ready signal from the ADIS16305. The following picture represents the Data Capture window, right after opening it from the Main Window and the second picture provides color-coded boxes, in order to support further discussion of each function that is associated with this screen.
The red box identifies all of the registers that are eligible for inclusion in the next acquistion process. Click on each box to include a register in the next data acquistion sequence. The box will have a check mark when it has been selected.
The green box identifies the configuration box for the name and location of the data storage file.
The yellow box identifies a number of configuration options for the data acquisition process. The Record Length is a user input for the total number of samples in a data record. Note that all selected registers will have this number of samples in the data record file, after the acuistion process completes. The Sample Rate represents the rate that the ADIS16305 updates its output register. This depends on the configuration in the SMPL_PRD{12:8] bits. For example, if SMPL_PRD = 0x0801, bits 12:8 represent a decimation setting of 8, which would result in an update rate of 102.5 SPS. After each update to the Record Length box, the software calculates the displays the total Capture Time. The Add Header option allows the user to add or remove the header in the data storage file. The Use Scaled Data causes the software to convert the decimal, twos omplement number into its representatiive value. For example, when enabling Use Scaled Data, the gyroscope outputs will be in units of degrees/second.
This section currently has no ADIS16305-specific content, but the
ADIS16448 Evaluation on the EVAL-ADIS Wiki Site has some good examples to start with.