Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis16228-eval-adis [28 Dec 2013 05:27] – [VIBRATION EVALUATION PROGRAM TUTORIALS] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16228-eval-adis [05 Feb 2021 12:45] (current) – Ioana Chelaru |
---|
For tips on interfacing to the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/EVAL-ADIS16228/eb.html|ADIS16228/PCBZ]] with a ribbon cable, check out the following Engineer Zone post: | For tips on interfacing to the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/EVAL-ADIS16228/eb.html|ADIS16228/PCBZ]] with a ribbon cable, check out the following Engineer Zone post: |
| |
[[ez>docs/DOC-2523| ADIS16228/PCBZ Breakout Board Cables (Engineer Zone FAQ)]] | [[ez>mems/w/documents/4496/faq-adis16228-pcbz-breakout-board-cables| ADIS16228/PCBZ Breakout Board Cables (Engineer Zone FAQ)]] |
| |
===== EVAL-ADIS: PC EVALUATION ===== | ===== EVAL-ADIS: PC EVALUATION ===== |
For those who would prefer to perform PC-based evaluation of the [[adi>ADIS16228|ADIS16228]], before developing their own embedded system, the [[adi>EVAL-ADIS|EVAL-ADIS]] is the appropriate system to use. The remainder of this Wiki site will focus on PC-based evaluation with the [[adi>EVAL-ADIS|EVAL-ADIS]] system. | For those who would prefer to perform PC-based evaluation of the [[adi>ADIS16228|ADIS16228]], before developing their own embedded system, the [[adi>EVAL-ADIS|EVAL-ADIS]] is the appropriate system to use. The remainder of this Wiki site will focus on PC-based evaluation with the [[adi>EVAL-ADIS|EVAL-ADIS]] system. |
| |
===== EQUIPMENT LIST ===== | ===== PART LIST FOR ORDERING ===== |
[[adi>EVAL-ADIS|EVAL-ADIS]] | [[adi>EVAL-ADIS|EVAL-ADIS]] |
| |
.NET Framework 3.5 | .NET Framework 3.5 |
| |
NOTE: Newer versions of the .NET framework do not currently support the IMU Evaluation software package. | NOTE: Newer versions of the .NET framework do not currently support the Vibration Evaluation Program. |
| |
===== PHYSICAL SETUP ===== | ===== PHYSICAL SETUP ===== |
The [[adi>en/mems-sensors/mems-accelerometers/adis162228/products/EVAL-ADIS16228/eb.html|ADIS16228/PCBZ]] provides the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/product.html|ADIS16228]] on a small printed circuit board (PCB) that simplifies the connection to an existing processor system. This PCB includes a silkscreen, for proper placement, and four mounting holes that have threads for M2 × 0.4 mm machine screws. The second set of mounting holes on the interface boards are in the four corners of the PCB and provide clearance for 4-40 machine screws. The third set of mounting holes provides a pattern that matches the EVAL-ADIS evaluation system, using M2 × 0.4mm × 4 mm machine screws. These boards are made of IS410 material and are 0.063 inches thick. J1 is a 16-pin connector, in a dual row, 2 mm geometry that enables simple connection to a 1 mm ribbon cable system. For example, use Molex P/N 87568-1663 for the mating connector and 3M P/N 3625/16 for the ribbon cable. For direct connection to the [[adi>EVAL-ADIS|EVAL-ADIS]] evaluation system, use these parts to make a 16-pin cable or remove pins 13, 14, 15 and 16. The LEDs (D1 and D2) are not populated, but the pads are available to install to provide a visual representation of the DIO1 and DIO2 signals. The pads accommodate Chicago Miniature Lighting Part No. CMD28-21VRC/TR8/T1, which works well when resistors R1 and R2 are approximately 400 Ω (0603 pad sizes).The mating connector for the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/product.html|ADIS16228]], J2, is AVX P/N 04-6288-015-000-846. The picture below provides a close-up view of this connector, which clamps down on the flex cable to press its metal pads onto the metal pads inside the mating connector. The schematic is for the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/EVAL-ADIS16228/eb.html|ADIS16228/PCBZ]] board. | The [[adi>ADIS16228|ADIS16228/PCBZ]] provides the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/product.html|ADIS16228]] on a small printed circuit board (PCB) that simplifies the connection to an existing processor system. This PCB includes a silkscreen, for proper placement, and four mounting holes that have threads for M2 × 0.4 mm machine screws. The second set of mounting holes on the interface boards are in the four corners of the PCB and provide clearance for 4-40 machine screws. The third set of mounting holes provides a pattern that matches the EVAL-ADIS evaluation system, using M2 × 0.4mm × 4 mm machine screws. These boards are made of IS410 material and are 0.063 inches thick. J1 is a 16-pin connector, in a dual row, 2 mm geometry that enables simple connection to a 1 mm ribbon cable system. For example, use Molex P/N 87568-1663 for the mating connector and 3M P/N 3625/16 for the ribbon cable. For direct connection to the [[adi>EVAL-ADIS|EVAL-ADIS]] evaluation system, use these parts to make a 16-pin cable or remove pins 13, 14, 15 and 16. The LEDs (D1 and D2) are not populated, but the pads are available to install to provide a visual representation of the DIO1 and DIO2 signals. The pads accommodate Chicago Miniature Lighting Part No. CMD28-21VRC/TR8/T1, which works well when resistors R1 and R2 are approximately 400 Ω (0603 pad sizes).The mating connector for the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/product.html|ADIS16228]], J2, is AVX P/N 04-6288-015-000-846. The picture below provides a close-up view of this connector, which clamps down on the flex cable to press its metal pads onto the metal pads inside the mating connector. The schematic is for the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/EVAL-ADIS16228/eb.html|ADIS16228/PCBZ]] board. |
| |
NOTE: Some of the illustrations show the [[adi>en/mems-sensors/mems-accelerometers/adis16210/products/EVAL-ADIS16210/eb.html|ADIS16210/PCBZ]] instead of the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/EVAL-ADIS16228/eb.html|ADIS16228/PCBZ]]. The package and setup process is identical for both of these products. | NOTE: Some of the illustrations show the [[adi>en/mems-sensors/mems-accelerometers/adis16210/products/EVAL-ADIS16210/eb.html|ADIS16210/PCBZ]] instead of the [[adi>en/mems-sensors/mems-accelerometers/adis16228/products/EVAL-ADIS16228/eb.html|ADIS16228/PCBZ]]. The package and setup process is identical for both of these products. |