Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [06 Sep 2013 17:54] – [Register Access] Scott Hutchens | resources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [09 Oct 2013 03:30] (current) – [Main Window] Mark Looney |
---|
| |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-holes-on-eval-adis.png?350|}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-holes-on-eval-adis.png?350|}} |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-on-eval-adis.png?470|}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265-eval-adis-data-rdy.png?500|}} |
| |
=== Step #3 === | === Step #3 === |
| |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265-main-low-voltage.png?600|}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265-main-low-voltage.png?600|}} |
====IMU EVALUATION SOFTWARE DOWNLOAD/GETTING STARTED==== | ====IMU EVALUATION SOFTWARE OVERVIEW==== |
| |
Visit the [[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software|IMU Evaluation Software Wiki Guide]] for software download, driver installation and basic, "getting started" instructions. | {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_overview&nofooter&noheader}} |
| |
QUICK TIP: Right click on this link and open this guide in a new Tab or Window, while keeping this Wiki Guide open. | ====USB Driver Installation==== |
| |
====IMU EVALUATION SOFTWARE FOR THE ADIS16265==== | {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#usb_driver_installation&nofooter&noheader}} |
After the USB driver installation is complete, connect the [[adi>EVAL-ADIS|EVAL-ADIS]] USB connector to the PC, using the USB Mini cable, from the [[adi>EVAL-ADIS|EVAL-ADIS]] kit. LED2 will illuminate as soon as this connection is made. This indicates that the [[adi>EVAL-ADIS|EVAL-ADIS]] has power and is going through its start-up/initialization process. After the [[adi>EVAL-ADIS|EVAL-ADIS]] completes its this process, LED1 will illuminate, indicating that it is time to launch the IMU Evaluation application. During the initialization process, several messages may appear on the screen. They are related to updating the EVAL-ADIS firmware and establishing communication between the PC and the [[adi>EVAL-ADIS|EVAL-ADIS]]. Once LED1 lights up, double click on the IMU_Evaluation.exe file to launch the application. | |
| |
| ====IMU EVALUATION SOFTWARE GETTING STARTED==== |
| |
| {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_starting_point&nofooter&noheader}} |
| |
| |
==== Main Window ==== | ====IMU EVALUATION SOFTWARE REVISION HISTORY==== |
Once the IMU Evaluation software starts-up, the Main Window will appear and look like the following picture. The second picture provides color-coded boxes to support further discussion of each function in this screen. | |
| |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265software-main.png?800|}} | {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#software_revision_history&nofooter&noheader}} |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265software-main-defined.png?800|}} | |
| |
The orange box identifies the drop-down menus, which provide a number of useful features. The **Devices** option provides a list of products. For [[adi>ADIS16265|ADIS16265]] Evaluation, click on **Devices** and then select **ADIS16265**. The green box shows the current device selection, which in this case, identifies the [[adi>ADIS16265|ADIS16265]] as the current selection. | |
| |
The **Register Access** option provides a listing of user-configurable registers in the [[adi>ADIS16265|ADIS16265]] and also provides read/write access to each one of these registers. | |
| |
The **Data Capture** option provides the core data collection function. | |
| |
The **Demos** option does not support the [[adi>ADIS16265|ADIS16265]]. | |
| |
The **Tools** option provides some diagnostic tools for the USB interface. | APPLICATION TIP: The **Register Access** screen writes to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the **Write Register** button. When using an embedded processor to write to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], each command (16-bits) writes to one byte at a time. |
| |
The **About** option provides more detail software revision information. | |
| |
The purple box identifies the output registers, which update, real-time, after pressing the **Read** button (see the red box for the location of the **Read** button). | |
| |
| |
The yellow box identifies the waveform recorder window. The window contains the gyroscope output (see register titles in the purple box). | |
| |
| ==== EXAMPLE EXERCISES ==== |
| This section currently has no [[adi>ADIS16265|ADIS16265]]-specific content, but the |
==== Register Access ==== | [[adi>resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. |
The purpose of the **Register Access** window is to provide both read and write access to the user registers in the [[adi>ADIS16265|ADIS16265]]. The following picture shows the appearance of this window. | |
| |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265-software-register.png?800|}} | |
| |
The color coded boxes illustrate the different functions that this window provides. | |
| |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265-software-register-defined.png?800|}} | |
| |
The purple box identifies the register category. In addition to the Control/Status, this drop-down control offers access to **Output** and **Calibration** registers. | |
| |
The red box identifies all of the registers that are in the current category. Click on the register name to select a register for individual read/write access. | |
| |
The green box identifies the read/write control options for the current register selection. Use the hexadecimal format when writing commands to a particular register. | |
| |
The yellow box updates all the registers in the current category. | |
| |
APPLICATION TIP: The **Register Access** screen writes to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the **Write Register** button. When using an embedded processor to write to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], each command (16-bits) writes to one byte at a time. | |
| |