Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [05 Sep 2013 17:36] – [IMU EVALUATION SOFTWARE FOR THE ADIS16265] Scott Hutchens | resources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [09 Oct 2013 03:30] (current) – [Main Window] Mark Looney |
---|
| |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-holes-on-eval-adis.png?350|}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-holes-on-eval-adis.png?350|}} |
{{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-on-eval-adis.png?450|}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265-eval-adis-data-rdy.png?500|}} |
| |
=== Step #3 === | === Step #3 === |
The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). That is the correct JP1 jumper setting on the [[adi>EVAL-ADIS|EVAL-ADIS]]) required for the [[adi>EVAL-ADIS16265|ADIS16265CCCZ]]. | The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). That is not the correct JP1 jumper setting on the [[adi>EVAL-ADIS|EVAL-ADIS]]) required for the [[adi>EVAL-ADIS16265|ADIS16265CCCZ]]and should be moved to the ***+5V*** position (right side). |
| |
{{:resources:eval:user-guides:inertial-mems:imu:eval-adis-3.3v.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:eval-adis-3.3v.png?350|}} |
| {{:resources:eval:user-guides:inertial-mems:gyroscopes:eval-adis-5v-setting.png?500|}} |
| |
<WRAP center round box 60%> | <WRAP center round box 60%> |
**NOTE:** If JP1 is left on **+5v** the software will look like the following picture. Move JP1 to the**+3.3V** setting to correct the problem. | **NOTE:** If JP1 is left on **+3.3v** position the software will look like the following picture. Move JP1 to the**+5V** setting to correct the problem. |
</WRAP> | </WRAP> |
| |
====IMU EVALUATION SOFTWARE DOWNLOAD/GETTING STARTED==== | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265-main-low-voltage.png?600|}} |
| ====IMU EVALUATION SOFTWARE OVERVIEW==== |
| |
Visit the [[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software|IMU Evaluation Software Wiki Guide]] for software download, driver installation and basic, "getting started" instructions. | {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_overview&nofooter&noheader}} |
| |
QUICK TIP: Right click on this link and open this guide in a new Tab or Window, while keeping this Wiki Guide open. | ====USB Driver Installation==== |
| |
====IMU EVALUATION SOFTWARE FOR THE ADIS16265==== | {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#usb_driver_installation&nofooter&noheader}} |
After the USB driver installation is complete, connect the [[adi>EVAL-ADIS|EVAL-ADIS]] USB connector to the PC, using the USB Mini cable, from the [[adi>EVAL-ADIS|EVAL-ADIS]] kit. LED2 will illuminate as soon as this connection is made. This indicates that the [[adi>EVAL-ADIS|EVAL-ADIS]] has power and is going through its start-up/initialization process. After the [[adi>EVAL-ADIS|EVAL-ADIS]] completes its this process, LED1 will illuminate, indicating that it is time to launch the IMU Evaluation application. During the initialization process, several messages may appear on the screen. They are related to updating the EVAL-ADIS firmware and establishing communication between the PC and the [[adi>EVAL-ADIS|EVAL-ADIS]]. Once LED1 lights up, double click on the IMU_Evaluation.exe file to launch the application. | |
| |
| ====IMU EVALUATION SOFTWARE GETTING STARTED==== |
| |
| {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_starting_point&nofooter&noheader}} |
| |
| |
| ====IMU EVALUATION SOFTWARE REVISION HISTORY==== |
| |
| {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#software_revision_history&nofooter&noheader}} |
| |
| |
| |
| |
| |
| |
| APPLICATION TIP: The **Register Access** screen writes to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the **Write Register** button. When using an embedded processor to write to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], each command (16-bits) writes to one byte at a time. |
| |
| |
| |
| |
| |
| ==== EXAMPLE EXERCISES ==== |
| This section currently has no [[adi>ADIS16265|ADIS16265]]-specific content, but the |
| [[adi>resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. |
| |