Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [30 Aug 2013 18:31] – [IMU EVALUATION SOFTWARE DOWNLOAD/GETTING STARTED] Mark Looneyresources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [09 Oct 2013 03:30] (current) – [Main Window] Mark Looney
Line 6: Line 6:
 The electrical connection typically only requires 5 I/O lines for synchronous data collection, as shown in the following figure: The electrical connection typically only requires 5 I/O lines for synchronous data collection, as shown in the following figure:
  
-{{:resources:eval:user-guides:inertial-mems:imu:16209_spi_conn.png?500|}}+{{:resources:eval:user-guides:inertial-mems:gyroscopes:265logic-lines_.png?500|}} 
  
 ===== ADIS16265/PCB BREAKOUT BOARD ===== ===== ADIS16265/PCB BREAKOUT BOARD =====
Line 24: Line 25:
  
 ===== PHYSICAL SETUP ===== ===== PHYSICAL SETUP =====
-The [[adi>ADIS16209|EVAL-ADIS16209]] provides the [[adi>ADIS16209|EVAL-ADIS16209]] function on a 1.2 inch × 1.3 inch printed circuit board (PCB), which simplifies the connection to an existing processor system. The four mounting holes accommodate either M2 (2mm) or Type 2-56 machine screws. These boards are made of IS410 +The [[adi>ADIS16265|ADIS16265]] provides the [[adi>ADIS16265|EVAL-ADIS16265]] function on a 1.2 inch × 1.3 inch printed circuit board (PCB), which simplifies the connection to an existing processor system. The four mounting holes accommodate either M2 (2mm) or Type 2-56 machine screws. These boards are made of IS410 
-material and are 0.063 inches thick. The second level assembly uses a SAC305-compatible solder composition (Pb-free), which has a pre-solder re-flow thickness of approximately 0.005 inches. The pad pattern on the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] matches that shown in below. J1 and J2 are dual-row, 2 mm (pitch) connectors that work with a number of ribbon cable systems, including 3M Part Number 152212-0100-GB (ribbon-crimp connector) and 3M Part Number 3625/12 (ribbon cable).+material and are 0.063 inches thick. The second level assembly uses a SAC305-compatible solder composition (Pb-free), which has a pre-solder re-flow thickness of approximately 0.005 inches. The pad pattern on the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] matches that shown in below. J1 and J2 are dual-row, 2 mm (pitch) connectors that work with a number of ribbon cable systems, including 3M Part Number 152212-0100-GB (ribbon-crimp connector) and 3M Part Number 3625/12 (ribbon cable).
  
 {{:resources:eval:user-guides:inertial-mems:imu:220-pcbz-dimensions.png?300 |}} {{:resources:eval:user-guides:inertial-mems:imu:220-pcbz-dimensions.png?300 |}}
Line 36: Line 37:
  
 === Step #1 === === Step #1 ===
-The connection to the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] is simple using J1 and a 16 pin cable included with the [[adi>EVAL-ADIS|EVAL-ADIS]].+The connection to the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] is simple using J1 and a 16 pin cable included with the [[adi>EVAL-ADIS|EVAL-ADIS]].
  
-{{:resources:eval:user-guides:inertial-mems:imu:209pcbz.png?400|}}+{{ :resources:eval:user-guides:inertial-mems:gyroscopes:265pcbz.png?600 |}}
  
-<WRAP center round alert 60%>+<WRAP center round alert 80%>
 **WARNING:** **WARNING:**
-Make sure that the connector cable going from J1 on the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] is properly aligned to the J1 connector on the [[adi>EVAL-ADIS|EVAL-ADIS]]. The 16 pin cable is included with the [[adi>EVAL-ADIS|EVAL-ADIS]] and proper mating has the last 4 cable connections open. The yellow wire from from J2-11 of the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] to the DIO1 test point on the [[adi>EVAL-ADIS|EVAL-ADIS]] is only required for synchronous data.</WRAP>+Make sure that the connector cable going from J1 on the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] is properly aligned to the J1 connector on the [[adi>EVAL-ADIS|EVAL-ADIS]]. The 16 pin cable is included with the [[adi>EVAL-ADIS|EVAL-ADIS]] and proper mating has the last 4 cable connections open. The Black wire from from J2-12 of the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] to the DIO1 test point on the [[adi>EVAL-ADIS|EVAL-ADIS]] is only required for synchronous data.</WRAP>
  
-{{:resources:eval:user-guides:inertial-mems:imu:209-cable-conn.png?400 |}} +{{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-on-eval-adis-j1conn.png?420|}} 
-{{:resources:eval:user-guides:inertial-mems:imu:209-data-ready-wire.png?400 |}}+{{:resources:eval:user-guides:inertial-mems:gyroscopes:265eval-adis-data-ready.png?400|}}
  
 === Step #2 === === Step #2 ===
-Mounting to the system frame is accomplished using 4 M2x.4x4mm machine screws included with the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]]. The mounting location holes are marked as an example in the picture below. Use the 4 A-location holes to secure the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] to the [[adi>EVAL-ADIS|EVAL-ADIS]].+Mounting to the system frame is accomplished using 4 M2x.4x4mm machine screws included with the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]]. The mounting location holes are marked as an example in the picture below. Use the 4 A-location holes to secure the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] to the [[adi>EVAL-ADIS|EVAL-ADIS]].
    
-{{:resources:eval:user-guides:inertial-mems:imu:209-eval-locate-holes.png?400 |}} +{{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-holes-on-eval-adis.png?350|}} 
-{{:resources:eval:user-guides:inertial-mems:imu:209pcbz-eval-adis.png?400|}}+{{:resources:eval:user-guides:inertial-mems:gyroscopes:265-eval-adis-data-rdy.png?500|}}
  
 === Step #3 === === Step #3 ===
-The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). That is the correct JP1 jumper setting on the [[adi>EVAL-ADIS|EVAL-ADIS]]) required for the [[adi>EVAL-ADIS16209|ADIS16209CCCZ]].+The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). That is not the correct JP1 jumper setting on the [[adi>EVAL-ADIS|EVAL-ADIS]]) required for the [[adi>EVAL-ADIS16265|ADIS16265CCCZ]]and should be moved to the ***+5V*** position (right side).
  
-{{:resources:eval:user-guides:inertial-mems:imu:eval-adis-3.3v.png?400|}}+{{:resources:eval:user-guides:inertial-mems:imu:eval-adis-3.3v.png?350|}} 
 +{{:resources:eval:user-guides:inertial-mems:gyroscopes:eval-adis-5v-setting.png?500|}}
  
 <WRAP center round box 60%> <WRAP center round box 60%>
-**NOTE:** If JP1 is left on **+5v** the software will look like the following picture. Move JP1 to the**+3.3V** setting to correct the problem.+**NOTE:** If JP1 is left on **+3.3v** position the software will look like the following picture. Move JP1 to the**+5V** setting to correct the problem.
 </WRAP> </WRAP>
  
-====IMU EVALUATION SOFTWARE DOWNLOAD/GETTING STARTED====+{{:resources:eval:user-guides:inertial-mems:gyroscopes:265-main-low-voltage.png?600|}} 
 +====IMU EVALUATION SOFTWARE OVERVIEW==== 
 + 
 +{{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_overview&nofooter&noheader}} 
 + 
 +====USB Driver Installation==== 
 + 
 +{{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#usb_driver_installation&nofooter&noheader}} 
 + 
 +====IMU EVALUATION SOFTWARE GETTING STARTED==== 
 + 
 +{{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_starting_point&nofooter&noheader}} 
 + 
 + 
 +====IMU EVALUATION SOFTWARE REVISION HISTORY==== 
 + 
 +{{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#software_revision_history&nofooter&noheader}} 
 +  
 + 
 + 
 + 
 + 
 + 
 +APPLICATION TIP: The **Register Access** screen writes to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the **Write Register** button. When using an embedded processor to write to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], each command (16-bits) writes to one byte at a time. 
  
-Visit the [[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software|IMU Evaluation Software Wiki Guide]] for software download, driver installation and basic, "getting started" instructions.  
  
-QUICK TIP: Right click on this link and open this guide in a new Tab or Window, while keeping this Wiki Guide open.  
  
-====IMU EVALUATION SOFTWARE FOR THE ADIS16265==== 
  
 +==== EXAMPLE EXERCISES ====
 +This section currently has no [[adi>ADIS16265|ADIS16265]]-specific content, but the
 +[[adi>resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with.
  
resources/eval/user-guides/inertial-mems/gyroscopes/adis16265-eval-adis.txt · Last modified: 09 Oct 2013 03:30 by Mark Looney