The EVAL-ADIN2111EBZ is a flexible platform enabling quick evaluation of the ADIN2111, robust, low power 10BASE-T1L 2-Port Ethernet switch. The evaluation board provides 2 10BASE-T1L channels with 10Mbit per second Single Pair Ethernet (SPE) connections reaching up to 1.7km of link distance. The ADIN2111 internal switch can be configured in store and forward mode between the two 10BASE-T1L channels and the SPI host. Cut through mode is also available between Port 1 and Port 2 and can be used without the need of the SPI host (unmanaged configuration).
The evaluation board offers two modes of operation for maximum flexibility: Connected to a PC via USB port, the full set of ADIN2111 register settings and features such as link quality monitoring and diagnostics can be accessed over the USB using the serial command interface implemented in the evaluation firmware.
Alternatively, the board can operate in cut-through mode between Port 1 and Port 2 (unmanaged configuration without firmware) where the EVAL-ADIN2111EBZ acts as a network switch forwarding packets between the 2x 10BASE-T1L ports. The 2x links are configured by setting the ADIN2111 hardware configuration pins jumper and switches. The 2x On-board Activity LEDs provide Link activity status indication for each port.
Custom firmware can also be developed and the ADIN2111 driver support package includes simple project examples to start a custom implementation.
The SPI interface provides access to the management registers required for the switch configuration, the 2 PHYs configuration and data exchange between SPI host and ports.
Figure 1.
The EVAL-ADIN2111EBZ can be powered from three different sources:
The power supply source can be configured using the P4 “BOARD POWER” link (3-positions: USB, EXT, GND).
Note that the two power supplies can be simultaneously enabled on P1 (2 jumpers inserted) as an internal common cathode diodes circuit selects the highest voltage source.
The selected input power source is converted by the step-down converter U501 (LT8619) to 3.3V
The link J2 is used to connect U2 output to the main 3.3V supply rail used on the board
The green “PWR” LED1 is ON when the 3.3V rail is present.
The board power consumption depends on the mode of operation, with the maximum of approximately 0.5W.
The 10BASE-T1L cable can be connected via pluggable screw-terminal block to connector P101. If more of the pluggable connectors are needed, for easy connecting / changing cables, additional connectors can be purchased from the vendor or distributors:
The demo board has two “Earth nodes”, one for each port. We call it “Earth node” here – though this node may or may not be electrically connected to Earth ground. In a real device this node would be typically connected to the device metal housing / chassis. Each Earth node can be connected as required in a wider demo system via “Earth” terminal of the power supply connector P1, or via exposed metal plating of 2 mounting holes in the left corners of the board. (The 3rd and 4th holes on the right do not have metal plating, and also no Earth connection.)
The shield of the 10BASE-T1L cables can be disconnected from this Earth node, connected directly, or connected via a 4x 1nF capacitors array for Port 1 (C85,C86,C87,C88) and Port 2 (C89,C92,C93,C95). The required connection is selected using jumper J101 (Port 1) and P22 (Port 2).
(!) Note: The EVAL-ADIN2111EBZ has been designed only as an Evaluation board. It has NOT been designed, and it has NOT been tested for electrical safety. Any equipment, device, wire, or cable connected to this demo must be already protected and safe to touch without danger of electric shock.
The EVAL-ADIN2111EBZ board is provided with links (jumper) and DIP switches that can be used to set the ADIN2111 configuration. The Table 1,2 and 3 describe the links and switches functions.
Table 1. Board Link Configuration
Link Ref. | Default Position | Description |
---|---|---|
J101 | Earth | CH1 Shield shorted either directly to Earth, or via 4nF cap |
P22 | Earth | CH2 Shield shorted either directly to Earth, or via 4nF cap |
P4 | EXT | USB – Connects 5V USB supply to the input of the LT8619 EXT - Connects externally supplied power from P1 or P2 to the input of LT8619 |
P10 | Burst | FORCED CURRENT – (H) Force Continuous mode of operation of LT8619 PULSE SKIP (o/c) - Pulse-Skipping mode of operation of LT8619 BURST (L) – Burst mode of operation of LT8619 |
J2 | Inserted | This link supplies 3.3V rail to circuitry on the board, beyond the LT8619 |
P11 | 3V3 | STM32 supply voltage – choice of 3.3V or 1.8V |
P13 | 3V3 | AVDD_H supply voltage – 3.3V (1.8V to be supported in final product) |
P14 | 3V3 | AVDD_L supply voltage – choice of 3.3V or 1.8V |
P15 | 3V3 | VDDIO supply voltage – choice of 3.3V or 1.8V |
DLDO_1V1_A | DLDO_1V1 | DVDD_A supply voltage – choice of EXT 1V1 rail or internally generated DLDO_1V1 |
DLDO_1V1_B | DLDO_1V1 | DVDD_B supply voltage – choice of EXT 1V1 rail or internally generated DLDO_1P1 |
P19 | Not Inserted | Option to short AVDD_H to AVDD_L |
P20 | Not Inserted | Option to short AVDD_L to VDDIO |
P8 | LES_RST | Option to hold STM32 in reset (GND RESET) or short it to the S5 push-button reset (LES_RST) |
P25 | RESET_N | Option to hold LES in reset (GND RESET) or short it to the RESET_N signal |
Table 2. ADIN2111 SPI Configuration , Schematics Ref. S1
Switch Position | Switch Name | Default Position | Description |
---|---|---|---|
1 | SPI_CFG1 | ON | SPI configuration 1 OFF: Generic SPI ON: Open Alliance SPI |
2 | SPI_CFG0 | OFF | SPI configuration 0 OFF: SPI CRC/Protection enabled. ON: SPI CRC/Protection disabled |
Table 3. ADIN2111 Transmit Level Configuration , Schematics Ref. S2
Switch Position | Switch Name | Default Position | Description |
---|---|---|---|
1 | P2_TX2P4_EN_N | OFF | Port 2 Transmit 2.4V disable OFF: TX level 2.4V p-p or 1.0V p-p ON: TX level 1.0V p-p only |
2 | P1_TX2P4_EN_N | OFF | Port 1 Transmit 2.4V disable OFF: TX level 2.4V p-p or 1.0V p-p ON: TX level 1.0V p-p only |
Table 4. ADIN2111 Software Power Down After Reset Configuration , Schematics Ref. S3
Switch Position | Switch Name | Default Position | Description |
---|---|---|---|
1 | P2_SWPD_EN_N | OFF | Port 2 Software Power Down After Reset OFF: Disabled ON: Enabled |
2 | P1_SWPD_EN_N | OFF | Port 1 Software Power Down After Reset OFF: Disabled ON: Enabled |
Table 3. Board LED indicators
Name (silkscreen) | Colour | Schematics Ref. | Description |
---|---|---|---|
PWR | GREEN | LED1 | * OFF: 3.3V board power supply not available ON: 3.3V board power supply available |
DEBUG | BLUE | DS5 | Firmware heart beat * OFF: No firmware activity, reset or reprogram the board * Blinking: firmware running |
MOD | RED GREEN | D10 | Microcontroller Mode LED Modes 6,14 - TCP/IP stack enabled with fixed IP: * GREEN LED always ON * RED LED not used |
Modes 7,15 - TCP/IP stack enabled with fixed DHCP * GREEN ON: IP assigned * GREEN blinking: waiting for IP assignment from DHCP server * RED LED not used |
|||
Modes 8,9 - Frame Generator/Frame Checker * GREEN OFF: No activity * GREEN ON: 10,000 packets transmitted and received with no error (err) or mismatched number of packets received (diff) * RED LED not used |
|||
NET | RED GREEN | D11 | Error LED |
All modes * RED OFF No issue * RED ON Potential SPI communication error with ADIN2111 (see terminal message). Check power and SPI configuration on S1 * GREEN LED not used |
|||
Modes 8,9 Only: Frame Generator/Frame Checker * RED OFF: No transmission error (err) or mismatch in number of packets received (diff) * RED ON: Transmission error (err) or mismatch in number of packets received (diff) |
|||
ACTIVITY_P2_LED0 | GREEN | DS1 | PORT 2 Link Activity LED * ON or blinking: Link activity * OFF: No link activity |
ACTIVITY_P1_LED0 | GREEN | DS6 | PORT 2 Link Activity LED * ON or blinking: Link activity * OFF: No link activity |
The EVAL-ADIN2111EBZ can be used in various modes of operations implemented in the uC firmware. Up to 16 modes of operations can be selected by setting the 4 positions of the slide switch S4. The selected configuration is latched after the board is powered up or reset.
Therefore, to change the mode of operation, the board must be reset by pressing “RESET” button S5 or by applying power cycle after changing the position of the slide switch S4. The available modes of operation are described in Table 4 below.
Table 4. Firmware Modes of Operation, Schematics Ref. S4
CFG [3:0]i | Mode No. | Operating Modeii | Description |
---|---|---|---|
0000 | 15 | TCP/IP Stack & Web Server, DHCP client, MAC Addr1 | In this mode, the TCP/IP stack can be managed via UART using dynamic IP address allocation. The media converter board is then used to convert 10BASE-T1L to 10BASE-T ethernet, for which common web browsers can be used to access the associated information. MAC address 1 is used. |
0001 | 14 | TCP/IP Stack & Web Server, Fixed IP, MAC Addr1 | This is a similar mode to the previous one except fixed IP address allocation is used. MAC address 1 is used. |
0010 | 13 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
0011 | 12 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
0100 | 11 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
0101 | 10 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
0110 | 9 | PHY2 Frame Generator Checker / PHY1 MAC Remote Loopback MSE reading enabled | PHY2 is set in Frame Generator/Checker Mode PHY1 is set in MAC Interface Remote loopback mode MSE readings are shown on UART. Link LED is also enabled. |
0111 | 8 | PHY1 Frame Generator Checker / PHY2 MAC Remote Loopback MSE reading enabled | PHY1 is set in Frame Generator/Checker Mode PHY2 is set in MAC Interface Remote loopback mode MSE readings are shown on UART. Link LED is also enabled. |
1000 | 7 | TCP/IP Stack & Web Server, DHCP client, MAC Addr2 | The use of this mode is depicted in Figure 11. In this mode, the TCP/IP stack can be managed via UART using dynamic IP address allocation. The media converter board is then used to convert 10BASE-T1L to 10BASE-T ethernet, for which common web browsers can be used to access the associated information. MAC address 2 is used. |
1001 | 6 | TCP/IP Stack & Web Server, Fixed IP, MAC Addr2 | This is a similar mode to the previous one except fixed IP address allocation is used. MAC address 2 is used. |
1010 | 5 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
1011 | 4 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
1100 | 3 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
1101 | 2 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
1110 | 1 | RESERVED | The uC makes no autonomous attempt to interact with the ADIN2111 |
1111 | 0 | Reset ADIN2111 | Keep the ADIN2111 in reset mode |
I Switch in ON position = signal logic 0 for microcontroller (shorted to ground).
Switch in OFF position = signal logic 1 (pulled up by a resistor)
II RESERVED means the microcontroller and command line interface is active (serial port).
The EVAL-ADIN2111EBZ can be used as a stand-alone board, with the firmware already pre-programmed in the microcontroller flash memory.
The mode of operation can be set using the S4 Configuration DIP switch and the link status is indicated by LEDs.
There is no software required for this stand-alone use case.
The EVAL-ADIN2111EBZ can also be interfaced with a host computer via the USB port. The full set of ADIN2111 PHY and MAC registers and features such as link quality monitoring can be accessed via the command line interface.
Note that the default firmware is configured with the SPI interface set to OPEN Alliance SPI with Protection enabled. The ADIN2111 hardware configurations pins must be set accordingly using the DIP switch S1 (see table 2 for reference).
The EVAL-ADIN2111EBZ has an onboard USB-UART converter (FTDI FT232R).
Ensure that the appropriate Virtual Com Port driver is installed on the host platform before connecting the EVAL-ADIN2111EBZ to the host computer via the USB cable.
The drivers are available from FTDI, at the time of writing this document at https://ftdichip.com/drivers/vcp-drivers/
When the EVAL-ADIN2111EBZ is connected to the host, it will become available in the host system as a USB Com Port, and will be assigned a com port number. The number will depend on the system settings, on com port devices previously connected and assigned in the system, and on the FTDI driver settings.
The EVAL-ADIN2111EBZ microcontroller communicates over a standard UART interface, with the following settings:
The protocol is based on ASCII text commands and messages. Each message sent from the firmware to the host is finished by both <CR> and <LF> characters. For the commands received from host the firmware expects <CR>, <LF> or <CR> + <LF>.
(For information: <CR> .. “carriage return”, ASCII code 0x0D, <LF> .. “line feed”, ASCII code 0x0A )
The EVAL-ADIN2111EBZ firmware works with the common serial terminals. It has been tested on Windows platform with PuTTY, RealTerm, Termite and Hyperterminal. (The examples in this document were captured using Compuphase Termite).
When the EVAL-ADIN2111EBZ is correctly connected via the USB Virtual COM Port using the terminal software, the firmware sends an initial welcome message as displayed below.
Note that a hardware reset of the board (using S5 “RESET” button) or the 'info' command will also display the welcome message. This can be useful to check the ADIN2111 information and link status.
================================================
ANALOG DEVICES 10BASE-T1L Demo Serial Interface
================================================
© 2021 Analog Devices Inc. All rights reserved
================================================
Firmware ver.: 1.2.1
Board Name: EVAL-ADIN2111EBZ
Board revision: B
Board Serial Number: 12345
uC CFG3-2-1-0: ON-OFF-OFF-OFF (Mode 7)
Board Configuration:TCP/IP Stack+WebServer,DHCP,MAC Addr2
SPI Access to ADIN2111: Success
MAC address: 00:e0:22:fe:da:ca
IP Address: not assigned
CH1 Link status: Down
Master/Slave: Not run
Tx Level: Not run
CH2 Link status: Down
Master/Slave: Not run
Tx Level: Not run
================================================
Type '<?><new line>' for a list of commands
================================================
Command | Description | Use |
---|---|---|
macwrite | Write in MAC registers. <regAddress> and <Data> in hex | macwrite <RegAddress>,<Data><newLine> |
macread | Read MAC registers. <regAddress> in hex | macread <RegAddress><newLine> |
phywrite | Write in PHY registers. <PortNumber>, <regAddress> and <Data> in hex | phywrite <PortNumber>,<RegAddress>,<Data><newLine> |
phyread | Read in PHY registers. <PortNumber> and <regAddress> in hex | phyread <PortNumber>,<RegAddress>,<Data><newLine> |
machwreset | ADIN2111 Hardware Reset | machwreset<newLine> |
macswreset | ADIN2111 Software Reset Similar to hardware reset without the power up sequence | macswreset<newLine> |
changemac | Change MAC address. Applies after 'savetoflash' and reset. All digits in hex | changemac <xx>:<xx>:<xx>:<xx>:<xx>:<xx><newLine> |
changeip | Change IP address. Applies after 'savetoflash' and reset. <xxx> digits in dec | changeip <xxx>.<xxx>.<xxx>.<xxx><newLine> |
changegw | Change gateway, all numbers in dec. Applies after 'savetoflash' and reset. <xxx> digits in dec | changegw <xxx>.<xxx>.<xxx>.<xxx><newLine> |
changenm | Change network mask,all numbers in dec. Applies after 'savetoflash' and reset. <xxx> digits in hex | changenm <xxx>.<xxx>.<xxx>.<xxx><newLine> |
changebrdname | Change board name. Applies after 'savetoflash' and reset. Warning: Predefined in factory. Lost if overwritten | changebrdname <custom text><newLine> |
changebrdrev | Change board revision Applies after 'savetoflash' and reset. Warning: Predefined in factory. Lost if overwritten | changebrdrev <custom text><newLine> |
changebrdsn | Change board serial number Applies after 'savetoflash' and reset. Warning: Predefined in factory. Lost if overwritten. Serial Number matches the label on the bottom of the board | changebrdsn <custom text><newLine><newLine> |
eraseflash | Erase the internal flash memory. Warning:resets the board parameters to default values Also erases board name,board serial number and board revision | eraseflash<newLine> |
savetoflash | Save configuration to flash. | savetoflash<newLine> |
reset | Microcontroller software reset. | reset<newLine> |
start | Start sending periodic diagnostics. Also provide statistics when used in Frame Generator\checker mode (9) | start<newLine> |
stop | Stop sending periodic diagnostics. | stop<newLine> |
clear | Clear/reset the diagnostics counters | clear<newLine> |
mode | Overwrite the board mode in software. After MCU reset or board reset, the mode is set to hardware configuration defined by the switch S303 | mode <number><newLine> |
modes | List the board modes available | modes<newLine> |
info | Display the board information (welcome message) | info<newLine> |
getbuildnb | Get the firmware build number | getbuildnb<newLine> |
? | Display the list of commands available | ?<newLine> |
The microcontroller (STM32L4S5QII3P) is programmed out-of-the box with the evaluation firmware. A binary image of the production firmware is also available to download from the ADIN2111 product webpage. The default behavior of the configuration switches based on the pre-loaded firmware is listed in Table 4. The revision of the programmed firmware can be checked using the serial terminal program and pressing the RESET button (S5) which will display the welcome message.
The ST-LINK JTAG programmer provides a robust solution for programming and debugging source code.
It is also faster to program the microcontroller using the JTAG interface.
Figure 4. STM32CubeProgrammer
The EVAL-ADIN2111EBZ firmware runs a webserver that can be used to access the Demo webpage to visualize the board information and link status for each port.
This feature demonstrates how the 10BASE-T1L Low Complexity Ethernet Switch can be connected to a 10BASE-T network and accessed using conventional HTTP requests.
A media converter board (e.g. EVAL-ADIN1100EBZ, see the user guide for more details) is required to interface the
EVAL-ADIN2111EBZ to a 10BASE-T network (using RJ45 cable).
A simple setup is shown below:
To run the webpage demo (DHCP, mode 7):
The webpage shows basic information about the board, the MSE and link parameters for each channel. The page is auto-refreshed every 5s. After a long period of time, if the page is hung a simple reset of the EVAL-ADIN2111EBZ will reload the page properly.
To run the frame generator/checker demo (mode 9 using Port 1):
start
OK
CH1 -37.2 dB,CH2 MSE n/a , Rx 0, Diff 0, Err 0
CH1 -37.2 dB,CH2 MSE n/a , Rx 0, Diff 0, Err 0
CH1 -37.2 dB,CH2 MSE n/a , Rx 0, Diff 0, Err 0
CH1 -37.2 dB,CH2 MSE n/a , Rx 0, Diff 0, Err 0
CH1 -37.2 dB,CH2 MSE n/a , Rx 0, Diff 0, Err 0
stop
OK
As a general recommendation, check the jumper configuration and make sure they are all in default state as a starting point. Exception applies to the power selection on P4 that can be configured based on the required power source.
Legal Terms and Conditions
By using the evaluation board discussed herein (together with any tools, components documentation or support materials, the “Evaluation Board”), you are agreeing to be bound by the terms and conditions set forth below (“Agreement”) unless you have purchased the Evaluation Board, in which case the Analog Devices Standard Terms and Conditions of Sale shall govern. Do not use the Evaluation Board until you have read and agreed to the Agreement. Your use of the Evaluation Board shall signify your acceptance of the Agreement. This Agreement is made by and between you (“Customer”) and Analog Devices, Inc. (“ADI”), with its principal place of business at One Technology Way, Norwood, MA 02062, USA. Subject to the terms and conditions of the Agreement, ADI hereby grants to Customer a free, limited, personal, temporary, non-exclusive, non-sublicensable, non-transferable license to use the Evaluation Board FOR EVALUATION PURPOSES ONLY. Customer understands and agrees that the Evaluation Board is provided for the sole and exclusive purpose referenced above, and agrees not to use the Evaluation Board for any other purpose. Furthermore, the license granted is expressly made subject to the following additional limitations: Customer shall not (i) rent, lease, display, sell, transfer, assign, sublicense, or distribute the Evaluation Board; and (ii) permit any Third Party to access the Evaluation Board. As used herein, the term “Third Party” includes any entity other than ADI, Customer, their employees, affiliates and in-house consultants. The Evaluation Board is NOT sold to Customer; all rights not expressly granted herein, including ownership of the Evaluation Board, are reserved by ADI. CONFIDENTIALITY. This Agreement and the Evaluation Board shall all be considered the confidential and proprietary information of ADI. Customer may not disclose or transfer any portion of the Evaluation Board to any other party for any reason. Upon discontinuation of use of the Evaluation Board or termination of this Agreement, Customer agrees to promptly return the Evaluation Board to ADI. ADDITIONAL RESTRICTIONS. Customer may not disassemble, decompile or reverse engineer chips on the Evaluation Board. Customer shall inform ADI of any occurred damages or any modifications or alterations it makes to the Evaluation Board, including but not limited to soldering or any other activity that affects the material content of the Evaluation Board. Modifications to the Evaluation Board must comply with applicable law, including but not limited to the RoHS Directive. TERMINATION. ADI may terminate this Agreement at any time upon giving written notice to Customer. Customer agrees to return to ADI the Evaluation Board at that time. LIMITATION OF LIABILITY. THE EVALUATION BOARD PROVIDED HEREUNDER IS PROVIDED “AS IS” AND ADI MAKES NO WARRANTIES OR REPRESENTATIONS OF ANY KIND WITH RESPECT TO IT. ADI SPECIFICALLY DISCLAIMS ANY REPRESENTATIONS, ENDORSEMENTS, GUARANTEES, OR WARRANTIES, EXPRESS OR IMPLIED, RELATED TO THE EVALUATION BOARD INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTY OF MERCHANTABILITY, TITLE, FITNESS FOR A PARTICULAR PURPOSE OR NONINFRINGEMENT OF INTELLECTUAL PROPERTY RIGHTS. IN NO EVENT WILL ADI AND ITS LICENSORS BE LIABLE FOR ANY INCIDENTAL, SPECIAL, INDIRECT, OR CONSEQUENTIAL DAMAGES RESULTING FROM CUSTOMER’S POSSESSION OR USE OF THE EVALUATION BOARD, INCLUDING BUT NOT LIMITED TO LOST PROFITS, DELAY COSTS, LABOR COSTS OR LOSS OF GOODWILL. ADI’S TOTAL LIABILITY FROM ANY AND ALL CAUSES SHALL BE LIMITED TO THE AMOUNT OF ONE HUNDRED US DOLLARS ($100.00). EXPORT. Customer agrees that it will not directly or indirectly export the Evaluation Board to another country, and that it will comply with all applicable United States federal laws and regulations relating to exports. GOVERNING LAW. This Agreement shall be governed by and construed in accordance with the substantive laws of the Commonwealth of Massachusetts (excluding conflict of law rules). Any legal action regarding this Agreement will be heard in the state or federal courts having jurisdiction in Suffolk County, Massachusetts, and Customer hereby submits to the personal jurisdiction and venue of such courts. The United Nations Convention on Contracts for the International Sale of Goods shall not apply to this Agreement and is expressly disclaimed.
©2021 Analog Devices, Inc. All rights reserved. Trademarks and registered trademarks are the property of their respective owners.