This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ev-gear-expander1z [20 Dec 2017 13:23] – Rajalakshmi Jayaraman | resources:eval:user-guides:ev-gear-expander1z [28 Jan 2021 17:36] (current) – Fixed bad link for digikey Ioana Chelaru | ||
---|---|---|---|
Line 35: | Line 35: | ||
=====COG connectors===== | =====COG connectors===== | ||
- | The COG connectors C1 and C2 interface the EV-GEAR-EXPANDER1Z board with MCU Cog. The connector carries all the GPIO signals from the MCU Cog board. The pinout details are given in the [[resources: | + | The COG connectors C1 and C2 interface the EV-GEAR-EXPANDER1Z board with MCU Cog. The connector carries all the GPIO signals from the MCU Cog board. The pinout details are given in the [[resources: |
- | <note warning> | + | <note warning> |
+ | |||
+ | Improper connector mating can also result in the loss of connectivity between MCU COG and EV-GEAR-EXPANDER1Z, | ||
+ | **</ | ||
=====Gear connectors===== | =====Gear connectors===== | ||
The connectors D1 and D2 can be used to connect a Gear. Gear is an addon application board which can be a custom build to serve the required application. | The connectors D1 and D2 can be used to connect a Gear. Gear is an addon application board which can be a custom build to serve the required application. | ||
- | <note important> | + | <note important> |
=====Arduino Uno headers===== | =====Arduino Uno headers===== | ||
The headers A1, A2, A3, A4 and A5 support the shields that are Arduino Uno compatible. The following table captures the signals connected to the headers | The headers A1, A2, A3, A4 and A5 support the shields that are Arduino Uno compatible. The following table captures the signals connected to the headers | ||
Line 56: | Line 59: | ||
|::: | |::: | ||
|::: | |::: | ||
- | |:::|A3|1|FT_EXT_VDD_OUT| | + | |:::|A3|1|NC| |
- | |:::|:::|2|TT_EXT_RESET_IN| | + | |:::|:::|2|FT_EXT_VDD_OUT| |
- | |:::|:::|3|FT_EXT_VDD_OUT| | + | |:::|:::|3|TT_EXT_RESET_IN| |
- | |:::|:::|4|FT_EXT_SUPPLY_OUT| | + | |:::|:::|4|FT_EXT_VDD_OUT| |
- | |:::|:::|5|GND| | + | |:::|:::|5|FT_EXT_SUPPLY_OUT| |
|::: | |::: | ||
- | |:::|:::|7|N.C| | + | |:::|:::|7|GND| |
|::: | |::: | ||
|::: | |::: |