This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0337 [01 Oct 2014 21:24] – changed fig.1 Christo Hrisulev | resources:eval:user-guides:circuits-from-the-lab:cn0337 [29 Jul 2021 07:28] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0337 Software User Guide ====== | ====== CN0337 Software User Guide ====== | ||
===== Overview===== | ===== Overview===== | ||
- | [[http:// | + | [[ADI>CN0337]] provides robust and complete solution for Temperature to digital conversion with isolation, for measurements where, standard RTD sensors are used. The design solution is optimized for high precision and low cost measurement, |
- | The circuit shown in Figure 1 incorporates [[http:// | + | The circuit shown in Figure 1 incorporates [[adi>AD8608ARZ|AD8608ARZ]] OpAmp, [[adi>AD7091RBRMZ|AD7091RBRMZ]] 12-bit successive approximation (SAR) ADC, and [[adi>ADuM5401ARWZ|ADuM5401ARWZ]] isolator to create a standard Temperature measurement system. |
The circuit has 12 pin PMOD connector on board, which could be used for connection to a customer microprocessor or FPGA. | The circuit has 12 pin PMOD connector on board, which could be used for connection to a customer microprocessor or FPGA. | ||
- | This [[http:// | + | This [[adi>CN0337|CN0337]] circuit note discusses the design steps needed to optimize the circuit shown in Figure 1 for a specific temperature range including component selection considerations. |
- | The performance of the circuit could be demonstrated with the use of Analog Devices SDP controller [[http:// | + | The performance of the circuit could be demonstrated with the use of Analog Devices SDP controller [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and SDP-to-PMOD Interposer Board [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]], |
- | This user guide will discuss how to use the evaluation software to collect data from the EVAL-CN0337-PMDZ Evaluation Board [[http:// | + | This user guide will discuss how to use the evaluation software to collect data from the EVAL-CN0337-PMDZ Evaluation Board [[adi>CN0337|CN0337]] |
{{: | {{: | ||
- | + | Figure 1. Resistance Deviation to Digital Conversion with Isolation Using Pt100 RTD Sensor (All Connections and Decoupling Not Shown) | |
- | + | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>CN0337|EVAL-CN0337-PMDZ]] Evaluation Board (**CN-0337 Board**) |
- | * [[http:// | + | * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V Power Supply)** or equivalent |
- | * [[http:// | + | * [[adi>SDP-PMD-IB1Z]] SDP-to-PMOD interposer board |
* Resistance Decade (to simulate the input resistance of the RTD element), e.g. IET RS-200 Labs Resistance Substituter Decade Box. (If no calibration procedure is performed, the temperature can be measured using real sensor) | * Resistance Decade (to simulate the input resistance of the RTD element), e.g. IET RS-200 Labs Resistance Substituter Decade Box. (If no calibration procedure is performed, the temperature can be measured using real sensor) | ||
* [[ftp:// | * [[ftp:// | ||
Line 30: | Line 28: | ||
* USB type A to USB type mini-B cable | * USB type A to USB type mini-B cable | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The [[http:// | + | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>EVAL-CN0337-PMDZ|EVAL-CN0337-PMDZ]] **(CN0337 Board)** via the DC barrel jack. |
- | * The [[http:// | + | * The [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector A. |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
- | * The [[http:// | + | * The [[adi>CN0337|EVAL-CN0337-SDPZ]] **(CN0337)** connects to the [[adi>EVAL-PMD-IB1Z|EVAL-PMD-IB1Z]] **(Interposer board)** via the 12-Pin header PMOD connector |
- | * The **(Pt/100 Resistance Decade )** connects to the [[http:// | + | * The **(Pt/100 Resistance Decade )** connects to the [[adi>CN0337|EVAL-CN0337-SDPZ]] **(CN0337 Board)** via the terminal block **J2** |
{{: | {{: | ||
Line 54: | Line 52: | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
- | - Connect the [[http:// | + | - Connect the [[adi>EVAL-CFTL-6V-PWRZ|+6V DC Power Supply]] **(Wallwart)** to the barrel jack **J1** of the [[adi>SDP-PMD-IB1Z|Interposer Board ]] **(Interposer Board )** as depicted below.\\ \\ <WRAP left round tip 50%> |
- | - Connect the 120-pin connector on the [[http:// | + | - Connect the 120-pin connector on the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** to the 120-pin connector marked **“CON A”** on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{: |
- | - Connect the USB cable supplied with [[http:// | + | - Connect the USB cable supplied with [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** to the USB port on the PC and the SDP Board \\ \\ {{: |
- | - Connect the [[http:// | + | - Connect the [[adi>EVAL-CN0337-PMDZ|EVAL-CN0337-PMDZ]] **(CN0337 Board)** to the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** via the 12 pin header PMOD connector. \\ \\ {{: |
- Connect the input current source (Current calibrator) to J2 Terminal Block. The polarity is shown on the picture below \\ {{: | - Connect the input current source (Current calibrator) to J2 Terminal Block. The polarity is shown on the picture below \\ {{: | ||
Line 129: | Line 127: | ||
- Open with Notepad or similar. The saved data shows the ADC Codes (decimal) | - Open with Notepad or similar. The saved data shows the ADC Codes (decimal) | ||
<WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</ | <WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</ | ||
+ | \\ \\ \\ \\ \\ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |