Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0336 [30 Sep 2013 15:06] – changes Christo Hrisulev | resources:eval:user-guides:circuits-from-the-lab:cn0336 [01 Oct 2013 21:58] – complete Christo Hrisulev |
---|
* USB type A to USB type mini-B cable | * USB type A to USB type mini-B cable |
===== General Setup ===== | ===== General Setup ===== |
* The [[http://www.analog.com/EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[http://www.analog.com/EVAL-CN0288-SDPZ|EVAL-CN0288-SDPZ]] **(CN-0288 Board)** via the DC barrel jack. | * The [[http://www.analog.com/EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[http://www.analog.com/EVAL-CN0336-PMDZ|EVAL-CN0336-PMDZ]] **(CN0336 Board)** via the DC barrel jack. |
* The [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector A. | * The [[http://www.analog.com/SDP-PMD-IB1Z|SDP-PMD-IB1Z]] **(Interposer Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector A. |
* The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
==== Establishing a USB Connection Link ==== | ==== Establishing a USB Connection Link ==== |
- Follow the instructions to properly install the software and connect the hardware as described in the previous sections. | - Follow the instructions to properly install the software and connect the hardware as described in the previous sections. |
- Open the file named **CN0366.exe** in the installation directory.\\ \\ <WRAP left info round box 60%>**NOTE:** If the software was installed to the default location it will be found at \\ **C:\Program Files\Analog Devices\CN0366\CN0366.exe**</WRAP>\\ \\ \\ \\ \\ \\ | - Open the file named **CN0336.exe** in the installation directory.\\ \\ <WRAP left info round box 60%>**NOTE:** If the software was installed to the default location it will be found at \\ **C:\Program Files\Analog Devices\CN0336\CN03366.exe**</WRAP>\\ \\ \\ \\ \\ \\ |
- Click the **Connect/Reconnect Button**. A window with a progress bar will load.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0336:usb-connection.png?nolink|}}\\ \\ | - Click the **Connect/Reconnect Button**. A window with a progress bar will load.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0336:usb-connection.png?nolink|}}\\ \\ |
- Upon success, the **System Status String Indicator** will display __SDP Board Ready to Acquire Data__ | - Upon success, the **System Status String Indicator** will display __SDP Board Ready to Acquire Data__ |