This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0326 [16 Sep 2013 07:10] – CN0326 rev F erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0326 [05 May 2015 19:41] – formatting Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======CN-0326 Software User Guide====== | + | ====== CN-0326 Software User Guide ====== |
- | <fs medium> | + | ===== OVERVIEW |
Line 9: | Line 9: | ||
---- | ---- | ||
- | <fs medium> | + | ===== GENERAL SETUP ===== |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 22: | Line 22: | ||
---- | ---- | ||
- | <fs medium> | + | ===== MINIMUM PC/SYSTEM REQUIREMENTS |
* One PC with the following | * One PC with the following | ||
* Windows XP SP2, Windows Vista or Windows 7 Business/ | * Windows XP SP2, Windows Vista or Windows 7 Business/ | ||
Line 31: | Line 31: | ||
---- | ---- | ||
- | <fs medium> | + | ===== HOW TO INSTALL THE EVALUATION SOFTWARE |
- Extract the file **CN0326 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | - Extract the file **CN0326 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
- Click **Next** to view the installation review page\\ \\ {{: | - Click **Next** to view the installation review page\\ \\ {{: | ||
Line 37: | Line 37: | ||
- Upon completion of the installation of the **CN0326 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | - Upon completion of the installation of the **CN0326 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | ||
- Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | ||
- | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | + | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. |
---- | ---- | ||
- | <fs medium> | + | ===== STEP BY STEP INSTRUCTION FOR CONNECTING THE HARDWARE |
{{: | {{: | ||
Line 52: | Line 52: | ||
- Plug in the wall wart and connect it to connector J1 of the [[http:// | - Plug in the wall wart and connect it to connector J1 of the [[http:// | ||
- | |||
- | | ||
---- | ---- | ||
- | <fs medium> | + | ===== OPENING AND ENABLING THE EVALUATION SOFTWARE |
{{: | {{: | ||
Line 66: | Line 64: | ||
---- | ---- | ||
- | <fs medium> | + | ===== STEP BY STEP INSTRUCTION USING THE EVALUATION SOFTWARE |
{{: | {{: | ||
Line 100: | Line 98: | ||
---- | ---- | ||
- | <fs medium> | + | ===== CALIBRATION |
Pre-Calibration Note: | Pre-Calibration Note: |