The Triton Quad-Apollo System Development Platform contains four AD9084 software defined, direct X-Band Quad-MxFE, as well as associated RF front-ends, clocking, and power circuitry. The target application is phased array radars, electronic warfare, and ground-based SATCOM, specifically a 16 transmit/16 receive channel direct X-Band sampling phased array at L/S/C/X-Band (0.1 GHz to ~12GHz). The Rx & Tx RF front-end has drop-in configurations that allow for customized frequency ranges up to Ku-Band (12-18GHz), depending on the end user’s application.
The ADXBAND16EBZ System Development Platform highlights a complete system solution. It is intended as a testbed for demonstrating multi-chip synchronization as well as the implementation of system level calibrations, beamforming algorithms, and other signal processing algorithms. The system is designed to mate with a VCU118 Evaluation Board from Xilinx®, which features the Virtex® UltraScale+™ XCVU9P FPGA, with provided reference software, HDL code, and MATLAB system-level interfacing.
In addition to the ADXBAND16EBZ Digitizing Card, the kit also contains a 16Tx/16Rx Calibration Board that is used to develop system-level calibration algorithms, or otherwise more easily demonstrate power-up phase determinism in situations pertinent to their own use case. The Calibration Board also allows the user to demonstrate combined-channel dynamic range, spurious, and phase noise improvements and can also be controlled via MATLAB add-on when connected to the PMOD interface of the VCU118.
The system can be used to enable quick time-to-market development programs for applications like:
This user guide serves as the main source of information for system engineers and software developers using the ADXBAND16EBZ System Evaluation Board, which contains four AD9084 software defined, direct X-Band Sampling Phased Array Development Platform, as well as associated RF front-end, clocking, and power circuitry. The target application is phased array radars, electronic warfare, and ground-based SATCOM, specifically a 16 transmit/16 receive channel direct X-Band sampling phased array at L/S/C/X-Band (0.1 GHz to ~12GHz). The Rx RF front-end has by-pass configurations that allow for customized frequency ranges up to Ku-band, depending on the end user’s application.
The ADXBAND16EBZ System Evaluation Board highlights a complete system solution. It is intended as a testbed for demonstrating multi-chip synchronization as well as implementation of system level calibrations, beam forming algorithms, and other signal processing algorithms. The board is designed to mate with a VCU118 Evaluation Board from Xilinx®, which features the Virtex® UltraScale+™ XCVU9P FPGA, with provided reference software and HDL code.
ADXBAND16EBZ-CAL Digitizing Card Key Features:
• Provides both individual adjacent channel loopback and combined channel loopback options
• Combined Tx and Rx channels output via SMPM connectors
A 4-step process allows single clock synchronization across dozens of channels using a tree fan-out architecture for bi-directional SYSREF
Combining 16 Tx channels after phase alignment improves Power Magnitude ~23dBm with SFDR improving by ~18dB
Combining 16 Rx channels after phase alignment improves NSD performance ~12dB with SFDR improving by >11dB
For additional questions or support, please visit the Engineering Zone forum at adef.