analog@debian:~$ mkdir tools analog@debian:~$ cd tools analog@debian:~/tools$ wget https://armkeil.blob.core.windows.net/developer/Files/downloads/gnu-a/10.3-2021.07/binrel/gcc-arm-10.3-2021.07-x86_64-aarch64-none-linux-gnu.tar.xz analog@debian:~/tools$ tar xvf gcc-arm-10.3-2021.07-x86_64-aarch64-none-linux-gnu.tar.xz analog@debian:~/tools$ export CROSS_COMPILE=`pwd`/gcc-arm-10.3-2021.07-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- analog@debian:~/tools$ export ARCH=arm64 analog@debian:~/tools$ cd ~
analog@debian:~$ git clone -b agilex https://github.com/analogdevicesinc/linux analog@debian:~$ cd ./linux analog@debian:~/linux$ make adi_zynqmp_defconfig analog@debian:~/linux$ make Image analog@debian:~/linux$ make intel/socfpga_agilex_socdk_ad9081.dtb analog@debian:~/linux$ cp arch/arm64/boot/Image /media/analog/BOOT/ analog@debian:~/linux$ cp arch/arm64/boot/dts/intel/socfpga_agilex_socdk_ad9081.dtb /media/analog/BOOT/socfpga_agilex_socdk.dtb analog@debian:~/linux$ cd ~
analog@debian:~$ git clone -b QPDS24.1_REL_GSRD_PR https://github.com/altera-opensource/arm-trusted-firmware analog@debian:~$ cd ./arm-trusted-firmware analog@debian:~/arm-trusted-firmware$ make bl31 PLAT=agilex DEPRECATED=1 analog@debian:~/arm-trusted-firmware$ cd ~
analog@debian:~$ git clone -b QPDS24.1_REL_GSRD_PR https://github.com/altera-opensource/u-boot-socfpga analog@debian:~$ cd ./u-boot-socfpga analog@debian:~/u-boot-socfpga$ ln -sf ../arm-trusted-firmware/build/agilex/release/bl31.bin . analog@debian:~/u-boot-socfpga$ sed -i 's/earlycon panic=-1/earlycon panic=-1 console=ttyS0,115200 root=\/dev\/mmcblk0p2 rw rootwait/g' configs/socfpga_agilex_defconfig analog@debian:~/u-boot-socfpga$ sed -i '/^CONFIG_NAND_BOOT=y/d' configs/socfpga_agilex_defconfig analog@debian:~/u-boot-socfpga$ sed -i '/^CONFIG_SPL_NAND_SUPPORT=y/d' configs/socfpga_agilex_defconfig analog@debian:~/u-boot-socfpga$ sed -i '/^CONFIG_CMD_UBI=y/d' configs/socfpga_agilex_defconfig analog@debian:~/u-boot-socfpga$ echo 'CONFIG_USE_BOOTCOMMAND=y' >> configs/socfpga_agilex_defconfig analog@debian:~/u-boot-socfpga$ echo 'CONFIG_BOOTCOMMAND="load mmc 0:1 \${loadaddr} agilex.core.rbf; bridge disable; fpga load 0 \${loadaddr} \${filesize}; bridge enable; load mmc 0:1 ${kernel_addr_r} Image; load mmc 0:1 ${fdt_addr_r} socfpga_agilex_socdk.dtb; booti ${kernel_addr_r} - ${fdt_addr_r}"' >> configs/socfpga_agilex_defconfig analog@debian:~/u-boot-socfpga$ make socfpga_agilex_defconfig analog@debian:~/u-boot-socfpga$ make analog@debian:~/u-boot-socfpga$ cp u-boot.itb /media/analog/BOOT/ analog@debian:~/u-boot-socfpga$ cd ~
analog@debian:~$ git clone https://github.com/analogdevicesinc/hdl analog@debian:~$ cd hdl/projects/ad9081_fmca_ebz/fm87 analog@debian:~/hdl/projects/ad9081_fmca_ebz/fm87$ make Building ad9081_fmca_ebz_fm87 [/home/analog/hdl/projects/ad9081_fmca_ebz/fm87/ad9081_fmca_ebz_fm87_quartus.log] ... OK analog@debian:~/hdl/projects/ad9081_fmca_ebz/fm87$ quartus_pfg -c ad9081_fmca_ebz_fm87.sof ad9081_fmca_ebz_fm87.jic \ -o hps_path=../../../../u-boot-socfpga/spl/u-boot-spl-dtb.hex \ -o device=MT25QU02G \ -o flash_loader=AGIB027R31B1E1V \ -o mode=ASX4 \ -o hps=1 analog@debian:~/hdl/projects/ad9081_fmca_ebz/fm87$ cp ad9081_fmca_ebz_fm87.core.rbf /media/analog/BOOT/agilex.core.rbf
S9 4-bit DIP Switch
Switch Bit | 1 | 2 | 3 | 4 |
Name | MSEL0 | MSEL1 | MSEL2 | Not Used |
JTAG Mode | ON | ON | ON | OFF |
QSPI Mode | ON | OFF | OFF | OFF |
4-bit DIP Switch | 1 | 2 | 3 | 4 |
S4 | ON | ON | ON | ON |
S15 | ON | ON | ON | OFF |
S10 | ON | ON | ON | ON |
S23 | ON | ON | ON | ON |
S6 | OFF | OFF | OFF | OFF |
S1 | OFF | OFF | OFF | OFF |
S22 | OFF | ON | ON | ON |
S19 | OFF | OFF | ON | ON |
S20 | ON | ON | ON | ON |