Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:ad-fmcomms4-ebz [29 Apr 2014 21:47] – add char data Robin Getz | resources:eval:user-guides:ad-fmcomms4-ebz [03 Dec 2014 15:26] – fix picture Robin Getz |
---|
The AD-FMComms4-EBZ board is very similar to the [[AD-FMComms2-EBZ]] and [[AD-FMComms3-EBZ]] board with only one exception, rather than the [[adi>AD9361]] (which is 2 Rx, 2Tx), it uses the [[adi>AD9364]], a lower cost 1 Rx, 1 Tx device. The AD-FMComms4-EBZ includes both types of external baluns, one targetted for wider tuning range applications (Minicircuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]), and ones which provide optimized performance for 2.4GHz. | The AD-FMComms4-EBZ board is very similar to the [[AD-FMComms2-EBZ]] and [[AD-FMComms3-EBZ]] board with only one exception, rather than the [[adi>AD9361]] (which is 2 Rx, 2Tx), it uses the [[adi>AD9364]], a lower cost 1 Rx, 1 Tx device. The AD-FMComms4-EBZ includes both types of external baluns, one targetted for wider tuning range applications (Minicircuits [[http://www.minicircuits.com/pdfs/TCM1-63AX+.pdf|TCM1-63AX+]]), and ones which provide optimized performance for 2.4GHz. |
| |
{{ :resources:eval:user-guides:ad9361_top_layer.png?direct&400|}} | {{ http://www.analog.com/static/imported-files/images/evaluation_tools/AD-FMCOMMS4.jpg|}} |
Since much of the FMCOMMS2/3/4 share a common device/infrastructure, much of the documentation is the same. | Since much of the FMCOMMS2/3/4 share a common device/infrastructure, much of the documentation is the same. |
- [[.:ad-fmcomms2-ebz:introduction|Introduction]] | - [[.:ad-fmcomms2-ebz:introduction|Introduction]] |