This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:software:filters [01 Jan 2015 08:02] – add Fstop for 1.4 & 3 MHz Robin Getz | resources:eval:user-guides:ad-fmcomms2-ebz:software:filters [05 Jan 2015 18:07] – [Basic Functions] Robin Getz | ||
---|---|---|---|
Line 56: | Line 56: | ||
This table is stored in [[https:// | This table is stored in [[https:// | ||
- | ^ LTE Bandwidth Set ((Release-8)) ^ Occupied RF Bandwidth ^ Sample Rate ^ | + | ^ LTE Specification |
- | ^ | + | ^ LTE Bandwidth Set ((Release-8)) ^ Occupied RF Bandwidth ^ Sample Rate ^ |
- | | | + | ^ |
- | | | + | | |
- | | | + | | |
- | | 10 | | + | | |
- | | 15 | 13.5 | + | | 10 | |
- | | 20 | 18 | + | | 15 | 13.5 | 23.04 |
+ | | 20 | 18 | 30.72 | ||
- | The LTE Release-8 physical layer specification actually supports 105 different bandwidth options (not just the 6 shown above). Occupied RF Bandwidth from between 1.08MHz to 19.8MHz with 180kHz steps complies with the spec. | + | The LTE Release-8 physical layer specification actually supports 105 different bandwidth options (not just the 6 shown above). Occupied RF Bandwidth from between 1.08MHz to 19.8MHz with 180kHz steps complies with the spec, and while these filters can be designed (manually) they are not included as defaults. |
In addition, you can also save your favorite parameter settings in this list, such as " | In addition, you can also save your favorite parameter settings in this list, such as " |