This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms1-ebz:hardware:functional_overview [14 Dec 2012 17:36] – remove under construction Lars-Peter Clausen | resources:eval:user-guides:ad-fmcomms1-ebz:hardware:functional_overview [09 Feb 2021 16:06] (current) – add retired Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD-FMCOMMS1-EBZ Functional Overview ====== | ====== AD-FMCOMMS1-EBZ Functional Overview ====== | ||
+ | {{page>/ | ||
A functional block diagram of the system is given below. The system consists of four functional partitions - transmit path, receive path, clocking and power supply. | A functional block diagram of the system is given below. The system consists of four functional partitions - transmit path, receive path, clocking and power supply. | ||
Line 14: | Line 14: | ||
| [[adi> | | [[adi> | ||
- | In the transmit direction, the system converts complex I and Q signals to a corresponding RF signal. The [[adi> | + | In the transmit direction, the system converts complex I and Q signals to a corresponding RF signal. The [[adi> |
The reference design generates the signals for AD9122 either from an internal DDS or external memory (via VDMA). The internal DDS consists of four independent signal generators with programmable phase offset and frequency. These four signal generators are paired to create two tones that are interleaved and driven to the DAC. | The reference design generates the signals for AD9122 either from an internal DDS or external memory (via VDMA). The internal DDS consists of four independent signal generators with programmable phase offset and frequency. These four signal generators are paired to create two tones that are interleaved and driven to the DAC. | ||
Line 27: | Line 27: | ||
| [[adi> | | [[adi> | ||
- | In the receive direction, the system converts a RF signal into complex I and Q signals. The RF signal is demodulated by the [[adi> | + | In the receive direction, the system converts a RF signal into complex I and Q signals. The RF signal is demodulated by the direct-conversion |
- | The reference design transfers the received data to DDR via DMA. An optional off-line FFT core may be used to generate a spectrum plot. | + | {{: |
+ | The resulting I and Q baseband signals are filtered and then passed to the [[adi> | ||
+ | |||
+ | The reference design transfers the received data to DDR via DMA. An optional off-line FFT core may be used to generate a spectrum plot. | ||
===== Clocking ===== | ===== Clocking ===== | ||
Line 48: | Line 51: | ||
* This is cleaned up (from a jitter standpoint) and sent to the AD9523. | * This is cleaned up (from a jitter standpoint) and sent to the AD9523. | ||
* The AD9523 takes this, and creates: | * The AD9523 takes this, and creates: | ||
- | * 983.04 MHz for the DAC sample rate | + | * 491.52 MHz for the DAC sample rate |
* 245.76 MHz for the ADC sample rate | * 245.76 MHz for the ADC sample rate | ||
- | * 30.72 MHz for the reference clocks for the LO PLLs. | + | * 122.88 MHz for the reference clocks for the LO PLLs. |
These clocks can be changed, but the key thing to remember is that the AD9523 drives both the ADC and DAC. The AD9523 has two clock banks (see figure 1 in the datasheet), Bank 0: 0-3 & 10-13, and Bank 1: 4-9. The outputs on the different banks need to be integer mutliples of eachother. The best thing to do if you are interested in the details of this, is to get the [[adi> | These clocks can be changed, but the key thing to remember is that the AD9523 drives both the ADC and DAC. The AD9523 has two clock banks (see figure 1 in the datasheet), Bank 0: 0-3 & 10-13, and Bank 1: 4-9. The outputs on the different banks need to be integer mutliples of eachother. The best thing to do if you are interested in the details of this, is to get the [[adi> | ||
Line 64: | Line 67: | ||
| [[adi> | | [[adi> | ||
| [[adi> | | [[adi> | ||
- | | [[adi>ADP150/1]] | Ultra low noise, 150/200 mA LDO | | + | | [[adi>ADP151]] | Ultra low noise, 150/200 mA LDO | |
| [[adi> | | [[adi> | ||
Line 75: | Line 78: | ||
To increase receive sensitivity, | To increase receive sensitivity, | ||
- | {{ :resources:fpga:xilinx:fmc: | + | {{ :resources:eval:user-guides: |
- | {{navigation AD-FMCOMMS1-EBZ# | + | {{navigation AD-FMCOMMS1-EBZ# |