The AD-FMCMOTCON2-EBZ is a complete motor drive system on a FMC board. Information on the card, and how to use it, the design package that surrounds it, and the software which can make it work, can be found here.
The purpose of the AD-FMCMOTCON2-EBZ is to provide a complete motor drive system demonstrating efficient and high dynamic control of three phase PMSM, BLDC, induction and stepper motors up to 48V and 20A. Two motors can be driven at the same time, each motor having its separate power supply. The kit consists of two boards: a controller board and a drive board. The system incorporates high quality power supplies; reliable power, control, and feedback signals isolation; accurate measurement of motor current & voltage signals; high speed interfaces for control signals to allow fast controller response; industrial Ethernet high speed interfaces; single ended Hall, differential Hall, encoder and resolver interfaces; digital position sensors interface; flexible control with a FPGA/SoC interface.
The AD-DYNO2-EBZ dynamometer is provided as an extension of the drive system. This is a dynamically adjustable load system that can be used to test real-time motor control performance. It consists of two BLDC motors directly coupled through a rigid connection. One of the BLDC motors acts as a load and is controlled by the DYNO’s embedded control system while the second motor is driven by the AD-FMCMOTCON2-EBZ FMC board. The load can be driven also by the AD-FMCMOTCON2-EBZ to implement dynamic load profiles.
This platform is intended to be used as a prototyping system to verify the hardware and the control algorithms before moving to the production stage. It helps reduce the time needed to move a motor control system from concept to production. Example reference designs showing how to use the platform with Xilinx® FPGAs or SoCs and high performance control algorithms from Mathworks® and Qdesys® are provided together with the hardware.