Analog Devices uses six designations to inform our customers where a semiconductor product is in its life cycle. From emerging innovations to products which have been in production for twenty years, we understand that insight into life cycle status is important. Device life cycles are tracked on their individual product pages on analog.com, and should always be consulted before making any design decisions.
This particular articl/edocument/design has been retired or deprecated, which means it is no longer maintained or actively updated, even though the devices themselves may be Recommended for New Designs or in Production. This page is here for historical/reference purposes only.
Power | |
---|---|
ADuM5000 | isoPower® integrated isolated dc-to-dc converter |
ADP3335 | HIGH ACCURACY ULTRALOW QUIESCENT CURRENT, 500 mA, ANYCAP® LOW DROPOUT |
Isolation | |
ADUM3223 | 3 KV RMS ISOLATED PRECISION HALF-BRIDGE DRIVER, 4 A OUTPUT |
The system is equipped with an LCD which displays information about the state of the load such and together with the 3 push buttons placed below it can be used to display and configure different system parameters. The +/- buttons are used to navigate through the system's menu and to change different system parameters, while the Enter button is used to confirm parameter changes or to enter / exit the menu screens.
In order interface the Dyno with the Analog Discovery™ USB Oscilloscope:
Two software packages are available for interfacing with Analog Discovery™:
The signals available to the Analog Discovery™ are:
Dyno Signal | Analog Discovery channel | Description |
---|---|---|
I_A | Scope Channel 1 Positive | Phase A motor current (185mv/A) |
I_B | Scope Channel 2 Positive | Phase B motor current (185mv/A) |
PWM1 | Digital Channel 0 | Phase A PWM (3.3V levels) |
PWM2 | Digital Channel 2 | Phase B PWM (3.3V levels) |
PWM3 | Digital Channel 2 | Phase C PWM (3.3V levels) |
The system needs a 5V 500mA power supply. The power connector is a 2.1 X 5.5MM jack with the center pin positive(+)
AD-DYNO1-EBZ