The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the AD-FMCDAQ2-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.
The AD-FMCDAQ2-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:
The supported OS are:
Board | HDL | Linux Software | No-OS Software |
---|---|---|---|
Arria10 SoC Dev Kit | YES | NO | YES |
Arria10 GX FPGA Dev Kit | NO (only until hdl_2021_r1 branch) | NO | YES |
KC705 | YES | YES | YES |
KCU105 | YES | YES | YES |
VC707 | NO (only until hdl_2018_r2 branch) | YES | YES |
ZC706 | YES | YES | YES |
ZCU102 | YES | YES | YES |