This is an old revision of the document!
SDP-S Getting Started
This chapter provides specific information to assist you with using the SDP board as part of your evaluation system.
Package Contents
Your EVAL-SDP-CS1Z board package contains the following items.
-
1m
USB Standard-A to mini-B cable
Contact the vendor where you purchased your SDP board or contact Analog Devices, Inc. if any item is missing.
PC Configuration
For correct operation of the SDP board, your computer must have the following minimum configuration
The SDP board evaluation system contains
ESD (electrostatic discharge) sensitive devices. Electrostatic charges readily accumulate on the human body and equipment and can discharge without detection. Permanent damage may occur on devices subjected to high-energy discharges. Proper
ESD precautions are recommended to avoid performance degradation or loss of functionality. Store unused SDP boards in the protective shipping package.
When removing the SDP board from the package, handle the board carefully to avoid the discharge of static electricity, which can damage some components.
USB Installation
Perform the following tasks to safely install the SDP board onto the computer.
There are two stages in the software application installation procedure. The first installs the application software. The second installs the .NET Framework 3.5 and the necessary drivers.
Run the application install provided. The first stage will install the Applications
GUI and necessary support files onto the computer
Immediately following the application install, the .NET Framework 3.5 and the driver package for the SDP board is installed. If the .NET Framework 3.5 is already pre-installed on the computer in question, this stage will be skipped and step two will consist of a driver package installation only
Connecting the SDP Board to the PC
Attach the SDP board to a
USB 2.0 port on the computer via the Standard-A to Mini-B cable provided.
Verifying Driver Installation
Before using the SDP board, verify the driver software has installed properly.
Open the Windows Device Manager and verify the SDP board appears under
ADI Development Tools as shown in figure GS1.
Figure GS1 : Device Manager showing correct SDP installation
Powering Up/Down the SDP
The following sections describe how to safely power up and down the SDP.
Powering Up the SDP Board
Connect the SDP board to the daughter evaluation board through the 120 pin mating connectors.
Power the daughter board
Connect the
USB port on the computer to the SDP board.
Powering Down the SDP Board
Power down the daughter evaluation board
Disconnect the
USB port on the computer from the SDP board
Disconnect the SDP board from the daughter evaluation board