This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:eval-ad9783 [15 Feb 2022 02:17] – [Software Needed:] Melissa Lorenz Lacanlale | resources:eval:dpg:eval-ad9783 [02 Apr 2023 08:55] (current) – John Marco Mina | ||
---|---|---|---|
Line 1: | Line 1: | ||
======EVALUATING THE AD9780/ | ======EVALUATING THE AD9780/ | ||
=====Preface===== | =====Preface===== | ||
- | This user guide describes both the hardware and software setup needed to acquire data capture from [[adi> | + | This user guide describes both the hardware and software setup needed to acquire data capture from [[adi> |
- | + | ||
- | This guide shows how AD9783-DPG2-EBZ works with SDP-H1 controller board developed by Analog Devices. Link to the old user guide document is provided for customers who still have DPG2 and DPG3 controller boards. | + | |
+ | This guide shows how AD9783-DPG2-EBZ works with ADS7-V2/ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
=====Typical Setup===== | =====Typical Setup===== | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | // | + | // |
+ | <WRAP centeralign> | ||
+ | //Figure 1b. EVAL-AD978x with ADS7-V2//</ | ||
<note tip>Tip: Click on any picture in this guide to open an enlarged version.</ | <note tip>Tip: Click on any picture in this guide to open an enlarged version.</ | ||
+ | |||
=====Helpful Files===== | =====Helpful Files===== | ||
* {{ : | * {{ : | ||
Line 20: | Line 26: | ||
=====Software Needed: | =====Software Needed: | ||
* [[: | * [[: | ||
- | * [[: | + | * [[: |
< | < | ||
- | |||
=====Hardware Needed: | =====Hardware Needed: | ||
* [[adi> | * [[adi> | ||
- | * [[: | + | * [[: |
- | * 12Vdc 1A Wall Adapter for SDP-H1 | + | * 5Vdc 1A Power supply for the evaluation board |
- | * 5Vdc 1A power supply | + | * [[adi> |
- | * [[adi> | + | |
* PC with ACE and DPG Lite Software Applications | * PC with ACE and DPG Lite Software Applications | ||
* High-Frequency Continuous Wave Generator (Clock Source) | * High-Frequency Continuous Wave Generator (Clock Source) | ||
* Signal/ | * Signal/ | ||
- | * (2) USB A to USB Mini Cables | ||
* (2) SMA Cables | * (2) SMA Cables | ||
+ | * (2) Banana Plug Cables | ||
+ | * The following are to be included if using SDP-H1 Evaluation Kit: | ||
+ | * 12Vdc 1A Wall Adapter | ||
+ | * (2) USB-A to USB-Mini Cable | ||
+ | * The following are to be included if using ADS7-V2 Evaluation Kit: | ||
+ | * 12Vdc Power Supply | ||
+ | * Power Cord | ||
+ | * USB-A to USB-B Cable | ||
=====Quick Start Guide===== | =====Quick Start Guide===== | ||
- | - Attach [[adi> | + | - Attach [[adi> |
- | - Connect SDP-H1 to PC via USB and to a 12V 1A power supply. | + | - Connect |
- | - Connect the evaluation board to PC via USB and to a 5Vdc 1A power supply on P5 and P6. Refer to Figure 1. | + | - Connect the evaluation board to PC via USB and to a **5Vdc 1A power supply** on **P5** and **P6**. Refer to Figures 1a and 1b. |
- | - Connect continuous wave generator for clock input to SMA J1 and DAC output from SMA J5 (IOUT1P) or SMA J9 (IOUT2P) to a signal/ | + | - Connect continuous wave generator for clock input to **SMA J1** and DAC output from **SMA J5 (IOUT1P)** or **SMA J9 (IOUT2P)** to a signal/ |
- | - Set clock input to 200MHz, 3dBm. | + | - Set clock input to **200MHz**, **3dBm**. |
- Open ACE. The board will be automatically recognized by the software. Click the plugin. Otherwise, install the [[adi> | - Open ACE. The board will be automatically recognized by the software. Click the plugin. Otherwise, install the [[adi> | ||
//Figure 2. AD9783 Plugin //</ | //Figure 2. AD9783 Plugin //</ | ||
Line 48: | Line 59: | ||
- The default values for the register is displayed and set. The values can be changed on the Chip View GUI, or on the **Memory Map** for registers not available in the GUI. For more info on the memory map, refer to [[adi> | - The default values for the register is displayed and set. The values can be changed on the Chip View GUI, or on the **Memory Map** for registers not available in the GUI. For more info on the memory map, refer to [[adi> | ||
//Figure 4. Apply Changes and Read All button | //Figure 4. Apply Changes and Read All button | ||
- | - Start DPG Downloader Lite. At the SDP-H1 | + | - Start DPG Downloader Lite. The controller board (SDP-H1/ADS7-V2), the device part number and clock frequency should be displayed. Refer to Figures 5a and 5b. {{ : |
- | // | + | - In DPG Downloader Lite, from the **Add Generator Waveforms** pulldown menu select **Single Tone** and apply the settings as shown in Figures 5a and 5b. Set the **Data Rate** to **200MHz** and **Desired Frequency** to **16MHz**. Set **DAC Resolution** to 16 for AD9783, 14 for AD9781, and 12 for AD9780. Uncheck the **Unsigned Data** box and Check the **Generate Complex Data (I & Q)**. |
- | - In DPG Downloader Lite, from the **Add Generator Waveforms** pulldown menu select **Single Tone** and apply the settings as shown in Figure 5. Set the **Data Rate** to 200MHz and Desired Frequency to 16MHz. Set **DAC Resolution** to 16 for AD9783, 14 for AD9781, and 12 for AD9780. Uncheck the **Unsigned Data** box and Check the **Generate Complex Data (I & Q)**. | + | |
- Select the I/Q tone from the **I/Q Data Vector** pulldown menu. | - Select the I/Q tone from the **I/Q Data Vector** pulldown menu. | ||
- Press the download arrow and then the play button. The spectrum similar to Figure 6 should appear in the signal/ | - Press the download arrow and then the play button. The spectrum similar to Figure 6 should appear in the signal/ | ||
Line 63: | Line 73: | ||
This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | ||
* Check the voltage rails of the evaluation board. P5 and P6 should be 5V; TP3, TP5, and TP7 should be 3.3V; TP9 and TP11 should be 1.8V. | * Check the voltage rails of the evaluation board. P5 and P6 should be 5V; TP3, TP5, and TP7 should be 3.3V; TP9 and TP11 should be 1.8V. | ||
- | * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | + | * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of the controller board (SDP-H1/ |
- | * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 | + | * Check if controller board (SDP-H1/ |
* Perform a chip reset by pressing S2 on the AD9783 evaluation board. | * Perform a chip reset by pressing S2 on the AD9783 evaluation board. | ||
- | * Power cycle both the SDP-H1 and the AD9783 evaluation board. | + | * Power cycle both the controller board (SDP-H1/ |
* Probe C18 and C19 to make sure a clock signal is being sent into the DAC. | * Probe C18 and C19 to make sure a clock signal is being sent into the DAC. | ||
* Check if XD1 is lit up on the evaluation board. Reconnect/ | * Check if XD1 is lit up on the evaluation board. Reconnect/ | ||
- | * Disconnect and reconnect the SDP-H1 and AD9783 evaluation board. Reopen ACE and DPG Lite software. | + | * Disconnect and reconnect the controller board (SDP-H1/ |