world leader in high performance signal processing
This version (15 Apr 2013 16:16) was approved by JasonC.The Previously approved version (20 Mar 2013 21:40) is available.Diff

High-Speed DAC Software Suite

The High-Speed DAC Software Suite contains a number of software applications that assist in evaluating an Analog Devices high-speed DAC. The suite contains software for communicating with a pattern generator from a variety of different applications, as well as communicating with the SPI port in parts on an evaluation board.

System Requirements

The DAC Software Suite requires the following minimum PC requirements. Some components of the suite may require additional resources.

  • Windows XP SP3 (32-bit), Windows Vista SP2 (32/64-bit), or Windows 7 SP1 (32/64-bit)
  • At least two available USB 2.0 ports
  • 128MB RAM
  • 1GB of free hard drive space

Prerequisites

The following items are required before the DAC Software Suite can be installed. If they are not present on your system before the DAC Software Suite Setup is run, setup will install them automatically:

  • Microsoft Windows Installer 3.1 or later
  • Microsoft .NET Framework version 3.5 SP1
  • National Instruments VISA Runtime Version 4.6.2 or later
  • National Instruments LabVIEW Runtime Version 7.1.1 (later versions are not compatible)
  • National Instruments LabVIEW Runtime Version 2009 SP1 (later versions are not compatible)

Supported Hardware

  • DPGI/O
  • All High-Speed DAC evaluation boards with USB

Downloading

The latest edition of the full DAC Software Suite can be downloaded here:

DAC Software Suite 1.2.153.0 Updated 3/20/2013

This update is strongly recommended over the previous 1.2.140.0 version. The previous version may show artificially poor DAC performance in some cases.

Installation

Administrator Privileges: Administrator privileges are required to install the DAC Software Suite.

Upgrading: Previous versions of the DAC Software Suite do not need to be un-installed before installing a newer version. The installer will automatically upgrade from any existing versions already installed.

Run the setup program. The following screen will be displayed after the installer loads:

Read the Analog Devices Software License Agreement. If you accept the terms of the agreement, click I Agree.

The installer can check online to ensure the version you are installing is the latest. You can choose not to allow the installer to check online.

The Choose Components page allows you to select which components of the DAC Software Suite you would like to install. The installer will automatically select the best option for your system. The prerequisites will only be selected if the installer determines they are not present on your system. The various software interfaces will only be selected if the corresponding software package is already installed. Therefore, install the DAC Software Suite after installing other software you would like to use with the DPG (for example, Visual Analog.)

Warning: If you have another vendor's VISA libraries installed (for example, the Agilent IO Libraries), you should not install the NI-VISA runtime from within the DAC Software Suite Setup. NI-VISA will need to be manually installed according to both National Instruments' and your 3rd party VISA library's instructions, before installing the DAC Software Suite. For more information on NI-VISA, see http://www.ni.com/visa

For most users, the default install location should be used. Some software interfaces may not function properly if the default directory is changed.

This screen allows you to change the location where shortcuts to various parts of the DAC Suite will be installed. Press Next to begin the installation.

During the installation, a progress bar will be displayed, with various status messages appearing above it. Depending on what prerequisites need to be installed, the process may take up to an hour or more. Additional installers may be displayed as part of the prerequisites install process. Proceed through those installers with the default options.

Near the end of the installation, you may receive warnings from Windows about the USB drivers. Select “Install this driver software anyway” if prompted.

The main software installation is now complete. Press Next to select which evaluation boards you will be using.

This screen lists the available evaluation boards. Select which boards you will be using and click Next. Additional boards may be added at any time in the future.

The installation is now complete.

DPGDownloader

DPGDownloader is an application created for quickly and easily interfacing with DPGs for creating, loading, and playing data vectors. For complete documentation, see the DPGDownloader page.

VisualAnalog™

For designers who are selecting or evaluating high speed ADCs, VisualAnalog™ is a software package that combines a powerful set of simulation and data analysis tools with a user-friendly graphical interface. An interface to DPGs allows for evaluation of DACs and mixed-signal converters in the software package. For more information, see the Visual Analog page.

To use VisualAnalog with a DPG, the DAC Software Suite must be installed after VisualAnalog is installed. If the DAC Software Suite was installed first, the installer should be run again to install the DPG interface into VisualAnalog.

Interfacing to 3rd Party Applications

Applications besides DPGDownloader and VisualAnalog can communicate directly with the DPGs. Interfacing with several popular applications is described below, followed by the general Programming Reference which is used with all applications.

See the Programming Reference for the methods and properties that are used with all applications.

Support

Please contact DPG Support with any additional questions regarding the DPG or DAC Software Suite.

1) The DPG1 is not supported by DPGDownloader, however the installer for the DPG1 software is included in the DAC Software Suite.