There are two evaluation boards available for the ADA2200:
The ADA2200-EVALZ is the simpler of the two evaluation boards. It facilitates signal connections to standard test equipment. The part can be reconfigured with the use of the on-board EEPROM.
Figure 1. ADA2200-EVALZ Evaluation Board
User guide, documentation and purchasing information can be found under
The ADA2200SDP-EVALZ adds additional input and output signal conditioning circuitry on-board. It also adds an interface to the SDP board. This allows access to the ADA2200 configuration registers over the SPI port with the use of a PC resident GUI application.
Figure 2. ADA2200SDP-EVALZ Evaluation Board
The ADA2200SDP-EVALZ User guide can be downloaded from this link:
http://www.analog.com/media/en/technical-documentation/user-guides/ADA2200SDP-EVALZ_UG-787.pdf
The ACE software used to configure the ADA2200SDP-EVALZ eval board can be downloaded from this link:
Analysis | Control | Evaluation (ACE) Software
The evaluation board contains a reconstruction filter. To calculate new values for the filter, download the excel spreadsheet.